Run Matter-NCP demos on i.MX MPU platforms#
This document describes how to use the MATTER-NCP demos on the i.MX MPU platforms. It shows how to run MATTER-NCP demos on the i.MX MPU platform and how to do wifi-bt commissioning between chip-tool and chip-all-clusters-app-ncp apps.
Release version information#
To ensure proper functionality, the Matter‑NCP must be used with the ncp‑device. Therefore, the Matter‑NCP version released in this cycle is required to match the corresponding SDK release version. The SDK release link associated with this Matter‑NCP version is provided below. You may download the appropriate SDK source code from GitHub and use it to compile the ncp‑device.
MATTER-NCP RELEASE: 2026Q1 SDK RELEASE:26.03.00 Preview2 https://github.com/nxp-mcuxpresso/mcuxsdk-manifests
Hardware requirements#
Two i.MX 8M Mini EVK boards (one board acts as the Matter controller running chip-tool, and the other acts as the end device running the chip-all-clusters-app-ncp app).
The i.MX 8M Mini EVK, running the chip-all-clusters-app-ncp app, connects to the RD-RW612, forming the connection between the NCP host and the NCP device.
If you mean that the i.MX board is the NCP host and the RD-RW612 is the NCP device, the clearest version is:
The i.MX 8M Mini EVK, running the chip-all-clusters-app-ncp app, connects to the RD-RW612 as the NCP host, while the RD-RW612 acts as the NCP device.
RDRW612 A2 BGA board
The RDRW612 acts as ncp-device and ensures that the Bluetooth Low Energy antenna is connected to the RDRW612 board to prevent Bluetooth Low Energy disconnection during Bluetooth Low Energy pairing.
The four interfaces USB, UART, SPI, and SDIO are supported between all-clusters-app-ncp and ncp-device. Refer to NXP NCP Application Guide for RW612 with MPU Host to set up: https://www.nxp.com/webapp/Download?colCode=UM12095
Compilation of the ncp device
Refer to the user manual: https://www.nxp.com/webapp/Download?colCode=UM12095
Go to sdk-next/mcuxsdk/examples/ncp_examples/ncp_device/app_config.cmake, and change as below:
set(CONFIG_NCP_WIFI 1)
set(CONFIG_NCP_BLE 1)
set(CONFIG_NCP_OT 0)
Choose the interface that you want to verify.
set(CONFIG_NCP_UART 0)
set(CONFIG_NCP_SPI 0)
set(CONFIG_NCP_USB 1)
set(CONFIG_NCP_SDIO 0)
Close mDNS Go to sdk-next/mcuxsdk/examples/_boards/rdrw612bga/ncp_examples/ncp_device/app_config.h and change as below:
#define CONFIG_NCP_MDNS_ENABLE 0
Verification of ble-wifi commissioning#
Set up BT and connect to a Wi-Fi AP on controller device (DUT running chip-tool)
Step 1. Save your Wi-Fi SSID and Password to a file.
\( wpa_passphrase \){SSID} ${PASSWORD} > wifiap.conf
Step 2. Set up BT and connected to a Wi-Fi AP.
\(modprobe moal mod_para=nxp/wifi_mod_para.conf \)wpa_supplicant -d -B -i mlan0 -c ./wifiap.conf \(sleep 5 \)udhcpc -i mlan0 \(modprobe btnxpuart \)hciconfig hci0 up
Run the example application on the end device, the following example uses the USB interface.
$ export NCP_PORT=/dev/ttyUSB0, and for sdio: export NCP_PORT=/dev/mcu-sdio
$ ./chip-all-clusters-app-ncp-usb --wifi --ble-device 0
For other interfaces (SPI, SDIO, and UART):
$ ./chip-all-clusters-app-ncp-spi --wifi --ble-device 0
$ ./chip-all-clusters-app-ncp-sdio --wifi --ble-device 0
$ ./chip-all-clusters-app-ncp-uart --wifi --ble-device 0
Do commissioning and control the end devices on the controller device.
$ ./chip-tool pairing ble-wifi 8888 ${SSID} ${PASSWORD} 20202021 3840
Verify that the device (all-cluster-app) has obtained an IP address. If the IP is obtained, the device is successfully connected to the external AP.
[1748353915.770112][551:551] CHIP:DL: Got IP address on interface: ncp_wlan IP: 192.168.0.188
The controller and device establish IP communication using the CASE handshake. The following log indicates that commissioning was completed successfully.
CHIP:TOO: Device commissioning completed with success
Matter chip-tool control chip-all-clusters-app-ncp apps after successful Matter commissioning#
Read onoff status.
$ chip-tool onoff read on-off 8888 1
You can see this log in the chip-tool console log. OnOff reflects the onoff status. The value must be FALSE before enabling OnOff.
[2025-05-22 14:25:04.603] [1747865814.155617][647:649] CHIP:TOO: OnOff: FALSE
Toggle to enable onoff.
$ chip-tool onoff toggle 8888 1
Read onoff status again. $ chip-tool onoff read on-off 8888 1.
The chip-tool console displays this log. OnOff indicates the on/off status and must be TRUE after it is enabled.
[2025-05-22 14:25:04.603] [1747865814.155617][647:649] CHIP:TOO: OnOff: TRUE