NXP Matter Documentation

Release Notes v1.6.0.0.2#

Release highlights#

  • This release provides NXP downstream Matter 1.6 support for NXP MCUs for FreeRTOS and Zephyr.

FreeRTOS#

  • Provides support for the following NXP platforms: MCX W72, RW61x (RW612, RW610), i.MX RT1060 + radio coprocessors (K32W0 RCP, IW416, IW612, IW610).

  • Matter is a first-class MCUXpresso SDK Middleware component. MCUXpresso SDK entry point to get started with Matter development is the mcuxsdk-manifests-connectivity-addons repository.

  • Supports integration with MCUXpresso SDK 26.06.00 for FreeRTOS configurations on all platforms.

Zephyr#

  • Provides maintenance support for NXP platforms: RW61x (RW612, RW610).

  • Introduces experimental support for the MCX W72 platform.

  • Supports integration of the NXP Zephyr v4.4.1.1 SDK.

Version information#

The versions for Matter (connectedhomeip), OpenThread, MCUXpresso SDK with FreeRTOS, and Zephyr RTOS that are integrated by this release are summarized below:

Development tools#

Features and examples supported#

FreeRTOS configurations#

The release supports configurations for Matter over Wi-Fi, Matter over Thread, Matter over Ethernet, and Matter over Wi-Fi with Thread Border Router. Refer to the dedicated Matter example repository for a complete list of Matter examples supported on NXP platforms. Refer to the README file of each example for more detailed information.

Zephyr configurations#

Main changes compared to previous release (v1.6.0.0.1)#

FreeRTOS#

  • Targeting all NXP platforms supporting Matter:

    • Updated MCUXpresso SDK from v26.03.00 to v26.06.00

    • Updated OpenThread from ot-nxp release/v1.4.0.5_26.03 to release/v1.4.0.6_26.06

  • RW61x FreeRTOS:

    • Added Matter certification fixes on v1.6.0.0.1.

      • TC-G-2.3, TC-IDM-10.6, TC-IDM-13.1, TC-IDM-14.1, TC-DESC-2.3.

    • Fix OTBR secondary network commissioning failed when secondary network commissioning interface feature enabled.

Zephyr#

  • No changes compared to v1.6.0.0.1.

Memory footprint summary (Release mode)#

  • MCX W72 (App core)

Matter Example

Connectivity support

Build mode

Application Flash usage

Application RAM usage

Factory data section

NVM (internal flash area)

OS

Contact Sensor Low Power LIT with OTA requestor + FD

Matter over Thread MTD with SED

Release

687K

129K (inc 53K heap)

8K

48K

FreeRTOS

Lighting app with OTA requestor + FD

Matter over Thread FTD

Release

768K

137K (inc 53K heap)

8K

48K

FreeRTOS

Door Lock app with OTA requestor + FD

Matter over Thread MTD

Release

786K

130K (inc 53K heap)

8K

48K

FreeRTOS

Contact Sensor LIT LP with OTA requestor + FD (SE05x)

Matter over Thread MTD with SED

Release

755K

143K (inc 65K heap)

8K

48K

FreeRTOS

  • RW61X (FRDM)

Matter Example

Connectivity support

Build mode

Application Flash usage

Application RAM usage

Factory data section

NVM

OS

Thermostat app with OTA requestor + FD

Matter over Wi-Fi (with Bluetooth LE)

Release

1392 K

496 K (inc 126 K heap)

4 K

64K

FreeRTOS

Thermostat app with OTA requestor + FD

Matter over Wi-Fi with OTBR (with Bluetooth LE)

Release

1872K

811K (inc 250K heap)

4K

64K

FreeRTOS

Thermostat app with OTA requestor + FD

Matter over Thread

Release

1215K

448K (inc 126K heap)

4K

64K

FreeRTOS

Thermostat app with OTA requestor + FD

Matter over Ethernet

Release

804K

306K (inc 126K heap)

4K

64K

FreeRTOS

Thermostat app with FD (SE05x)

Matter over Wi-Fi (with Bluetooth LE)

Release

1424K

491K (inc 126K heap)

4K

64K

FreeRTOS

  • i.MX RT1060 + radio coprocessors

Matter Example

Connectivity support

Build mode

Radio coprocessor

Application Flash usage

Application RAM usage

Factory data section

NVM

OS

Thermostat app with FD

Matter over Thread

Release

K32W0

1067K

442K (inc 126K heap)

4K

128K

FreeRTOS

Thermostat app with FD

Matter over Wi-Fi (with Bluetooth LE)

Release

IW416

1355K

428K (inc 126K heap)

4K

128K

FreeRTOS

Thermostat app with OTA requestor + FD

Matter over Wi-Fi (with Bluetooth LE)

Release

IW610

1418K

438K (inc 126K heap)

4K

128K

FreeRTOS

Thermostat app with OTA requestor + FD

Matter over Thread

Release

IW610

1544K

458K (inc 126K heap)

4K

128K

FreeRTOS

Thermostat app with OTA requestor + FD

Matter over Wi-Fi with OTBR (with Bluetooth LE)

Release

IW610

1850K

759K (inc 250K heap)

4K

128K

FreeRTOS

Thermostat app with OTA requestor + FD

Matter over Wi-Fi (with Bluetooth LE)

Release

IW612

1913K

439K (inc 126K heap)

4K

128K

FreeRTOS

Thermostat app with OTA requestor + FD

Matter over Thread

Release

IW612

2039K

458K (inc 126K heap)

4K

128K

FreeRTOS

Thermostat app with OTA requestor + FD

Matter over Wi-Fi with OTBR (with Bluetooth LE)

Release

IW612

2349K

760K (inc 250K heap)

4K

128K

FreeRTOS

Thermostat app with OTA requestor + FD (SE05x)

Matter over Wi-Fi with OTBR (with Bluetooth LE)

Release

IW610

1921K

761K (inc 250K heap)

4K

128K

FreeRTOS