Known Issues imx_matter_2026_q2#
Known issues#
Due to a known issue in BlueZ, when performing ble-wifi pairing between two devices using the i.MX 8M Mini platform (as commissioner or commissionee), the other i.MX device must also run the current release image. Using an older i.MX Matter release image on the peer device can result in Bluetooth LE pairing failures.