# Introduction **MCUXpresso Secure Provisioning Tool \(SEC\)** is a GUI tool made to simplify the generation and provisioning of bootable executables on NXP MCU platforms. It is built upon the proven security enablement toolset provided by NXP and takes advantage of the breadth of programming interfaces provided by the BootROM. New users should find it easier to prepare, flash, and secure images, while experienced users rediscover features from the existing toolset \(sdphost, blhost, nxpimage, and so on\) under a friendlier GUI. Experienced users can further customize secure provisioning flows by modifying scripts generated by the tool. ```{eval-rst} .. figure:: _images/splash_screen.png :scale: 60% :align: center **MCUXpresso Secure Provisioning Tool** ```