# Generic workflows This section provides information on workflow for some typical use cases. These chapters are not specific for any processor. ## Debug authentication workflow This section describes the process of opening the debug port. This tool offers Debug Authentication Protocol \(DAP\) as a mechanism to authenticate the debugger \(an external entity\) for the field technician, which has the credentials approved by the product manufacturer \(OEM\) before granting the debug access to the device. For Debug Authentication \(DA\) to work, processor-specific fuses or PFR fields must be set. For more information see the device user manual, chapter Debug subsystems. ```{eval-rst} .. figure:: _images/Debug_Authentification_protocol_usage_example.svg :scale: 80% :align: center **Debug Authentification protocol usage example** ``` To open the debug port, do the following: **Field Technician** 1. To get the key type and ROT length, contact the OEM. OEM decides whether to use the generated certificate for any device with the same ROT keys or just one by specifying the UUID. 2. In the SEC Tool, create a workspace for the used target device, switch to the "PKI Management" view 3. Click the **Generate a debug key...** button and verify that both the key type and length of the DA key match those of the corresponding ROT key. 4. Click the **Create debug certificate request...** button. Optionally, specify an UUID to limit the use of the debug certificate. If the UUID is set to zero, it can be used for any device. UUID can be read from a device via UART or USB if the processor is in ISP mode and in the development life cycle. For processors in an advanced life cycle, the debug probe works. On most devices, CHECK\_UUID must be set in the SOCU fuse/PFR field to enable verification of the UUID in the debug certificate. 5. Send the certificate request to OEM 6. After the certificate from OEM is received, click the **Open debug port...** button. The connected probes are detected upon the dialog display. The list of detected probes can be updated by clicking the **Find probes** button. Select one of the detected probes. The authentication beacon is an optional parameter and it is independent of the credential beacon provided by the OEM. It is not interpreted by the debug authentication protocol, it is passed to the debugged application. 7. For devices with a dual key schema, it is necessary to provide the path to the manifest file, which contains information about the public keys and indicates which key was used for signing. The preferred approach is to provide the path to the certificate ZIP file, from which the manifest path will be prefilled and the correct dir structure with public keys will be created. 8. When the dialog is confirmed, a script is generated in workspace\\debug\_auth\\open\_debug\_port.\[bat\|sh\] and is executed. The dialog is closed if no error is reported by the script \(the operation is successful\). In case of failure, refer to section [Debug authentication](./09_troubleshooting.md#debug-authentication) for details on how to enable debug authentication. **Note:** nxpdebugmbox CLI tool can be found in `/tools/spsdk/` folder ```{eval-rst} .. figure:: _images/Dialog_for_opening_debug_port.png :scale: 80% :align: center **Dialog for opening debug port** ``` **OEM Developer** After receiving the request, click the **Generate debug certificate...** button. The certificate is by default generated into `/debug_auth`folder`, debug_auth_cert.dc.` A \*.zip archive with the same name is created, it contains the certificate and the `.txt` file note from OEM. For devices that support the dual key schema, the created ZIP file also contains a manifest with additional information for DA configuration and public keys. The note that is passed from field technician to OEM is displayed in the note field \(see Figure "Generation of debug certificate from certificate request"\). - **SoC** - mask value of `DCFG_CC_SOCU` controlling which debug domains are accessed via the authentication protocol - **Vendor usage** - field that can be used to define a vendor-specific debug policy. The use case can be Debug Credential \(DC\) certificate revocations, the department identifier, or the model identifier. - **Credential beacon** - a value that is not interpreted by DAP, it is passed to the application. The value is independent of the authentication beacon that will be provided by the field technician when the port is opened. - **Note** - text field where OEM can describe comments about reasons to generate the certificate - **Sign with ROT key** - sign the certificate with one of the ROT keys that were used to secure the device. ```{eval-rst} .. figure:: _images/Generation_of_debug_certificate_from_certificate_request.png :scale: 80% :align: center **Generation of debug certificate from certificate request** ``` ### Example of access rights to debug domains Examples are intended for testing purposes. Before the final usage, the setting should be revisited and modified to fulfill security requirements. In all examples below, ISP is enabled and UUID check is disabled. For some processors, UUID check must be set to enable the read of UUID by a debug probe. ```{table} KW45xx/K32W1xx and MCX W71x :name: kw45xx-k32w1xx-and-mcx-w71x |Fuse|Everything disabled|Everything enabled|Controlled by DA| |----|-------------------|------------------|----------------| |DCFG\_CC\_SOCU\_L1, DCFG\_CC\_SOCU\_L2|0x000000FF|0x0000FFFF|0x00004040| |DBG\_AUTH\_DIS|0x0|0x0|0x0| ``` ```{table} KW47xx and MCX W72x :name: kw47xx-and-mcx-w72x |Fuse| Everything disabled | Everything enabled |Controlled by DA| |----|---------------------|--------------------|----------------| |DCFG\_CC\_SOCU\_L1, DCFG\_CC\_SOCU\_L2|0x000001FF|0x0003FFFF|0x00008040| |DBG\_AUTH\_DIS|0x0|0x0|0x0| ``` ```{table} LPC55S0x/1x, MCXW236 and NHS52S04 :name: lpc55s0x-1x-mcxw236-and-nhs52s04 |PFR field|Everything disabled|Everything enabled|Controlled by DA| |---------|-------------------|------------------|----------------| |DCFG\_CC\_SOCU\_NS\_PIN, DCFG\_CC\_SOCU\_PIN|0xFF2000DF|0xFF2000DF|0xFFBF0040| |DCFG\_CC\_SOCU\_NS\_DFLT, DCFG\_CC\_SOCU\_DFLT|0xFFFF0000|0xFF2000DF|0xFFBF0040| ``` ```{table} LPC55S2x :name: lpc55s2x |PFR field|Everything disabled|Everything enabled|Controlled by DA| |---------|-------------------|------------------|----------------| |DCFG\_CC\_SOCU\_NS\_PIN, DCFG\_CC\_SOCU\_PIN|0xFF2000DF|0xFF2C00D3|0xFFBF0040| |DCFG\_CC\_SOCU\_NS\_DFLT, DCFG\_CC\_SOCU\_DFLT|0xFFFF0000|0xFF2C00D3|0xFFBF0040| ``` ```{table} LPC55S3x :name: lpc55s3x |PFR field|Everything disabled|Everything enabled\*|Controlled by DA| |---------|-------------------|--------------------|----------------| |DCFG\_CC\_SOCU\_NS\_PIN, DCFG\_CC\_SOCU\_PIN|0xFE3001CF|0xFE3001CF|0xFFFF0000| |DCFG\_CC\_SOCU\_NS\_DFLT, DCFG\_CC\_SOCU\_DFLT|0xFFBF0040|0xFE3001CF|0xFFFF0000| ``` **Note:** For debugging, authentication is still required but the domain cannot be disabled by the SoC mask in the DAC. ```{table} LPC55S6x :name: lpc55s6x |PFR field|Everything disabled|Everything enabled|Controlled by DA| |---------|-------------------|------------------|----------------| |DCFG\_CC\_SOCU\_NS\_PIN, DCFG\_CC\_SOCU\_PIN|0xFD0002FF|0xFD0002FF|0xFFBF0040| |DCFG\_CC\_SOCU\_NS\_DFLT, DCFG\_CC\_SOCU\_DFLT|0xFFBF0040|0xFD0002FF|0xFFBF0040| ``` ```{table} MCX Nx4x, MCX N23x and MCX N55xS :name: mcx-nx4x-mcx-n23x-and-mcx-n55xs |PFR field|Everything disabled|Everything enabled\*|Controlled by DA| |---------|-------------------|--------------------|----------------| |DCFG\_CC\_SOCU\_NS\_PIN, DCFG\_CC\_SOCU\_PIN|0xF81007EF|0xF81007EF|0xFFBF0040| |DCFG\_CC\_SOCU\_NS\_DFLT, DCFG\_CC\_SOCU\_DFLT|0xFFBF0040|0xF81007EF|0xFFBF0040| ``` **Note:** For debugging, authentication is still required but the domain cannot be disabled by the SoC mask in the DAC. ```{table} RT5xx/6xx :name: rt5xx-6xx |Fuse|Everything disabled|Everything enabled|Controlled by DA| |----|-------------------|------------------|----------------| |DCFG\_CC\_SOCU, DCFG\_CC\_SOCU\_NS|0x80FF408D|0x80FFFF20|0x00404088| |DCFG\_CC\_SOCU\_AP|0x7F00BF72|0x7F0000DF|0xFFBFBF77| ``` ```{table} RW61x :name: rw61x |Fuse|Everything disabled|Everything enabled\*|Controlled by DA| |----|-------------------|--------------------|----------------| |DCFG\_CC\_SOCU, DCFG\_CC\_SOCU\_NS|0x3FFA007E|0x3FFFFF14|0x1002000F| |DCFG\_CC\_SOCU\_AP|0xC005FF81|0xC00000EB|0xEFFDFFF0| ``` **Note:** For debugging, authentication is still required but the domain cannot be disabled by the SoC mask in the DAC. **RT118x** does not have any fuse to control the debugging rights. Debugging behavior depends on the life cycle state: - OEM\_OPEN: All debug is allowed. - OEM\_CLOSE: All debug is disabled by default but can be re-enabled using DAC. - OEM\_LOCKED: All debug is disabled and cannot be re-enabled. ## Signature provider workflow This section describes the process of setting up a signature provider and building an image signed by the signature provider. Examples of signature provider servers are available in `/sample_data/signature_provider_examples`. There are several servers supporting signing with RSA, ECC, and RSA/ECC using a certificate authority \(CA\). These examples demonstrate a full implementation of the API; however, in the real world, it is expected that the implementation will be changed by communication with an HW HSM module or custom HTTPS communication with another server. Examples of the server can be used to test the tool behavior when using the signature provider. Each server has example private keys and prepared public key response for the `public_keys_certs` endpoint. These keys should not be used in final products. ```{table} Key types supported in the server examples :name: key-types-supported-in-server-examples |Server example|Private keys|Public keys tree| |------|------------|-----------| |ca_rsa_ecc_server|CA-4xSRK-4xCSF-4xIMG ECC-p256
CA-4xSRK-4xCSF-4xIMG RSA-2048|hex of certs| |ecc_server|4xROT-4xIMG ECC-p256|hex of public keys| |rsa_server|4xROT-4xIMG RSA-2048|hex of public keys| |rt118x_ecc_rsa_server|4xSRK ECC-p256
4xSRK RSA-2048|hex of public keys| ``` The figure below displays variants of signature provider, the SEC Tool sends requests to a Custom signature provider HTTP server. This server should pass the request to one of the secure solutions and then pass the response back to the SEC Tool. Prepared examples implement only the Custom signature provider HTTP server. The example server is doing the operation that should be done by an HSM or external signature provider. It is up to the user to implement a complete solution. ```{eval-rst} .. figure:: _images/Expected_structure_of_signature_provider.svg :scale: 80% :align: center **Expected structure of signature provider** ``` ### Run the server Ensure that python 3.12 or higher is installed. Open the directory with the server implementation\(click the **Sample server implementations** link in signature provider dlg\), specify the SPSDK package version in `requirements.txt` \(use the same version as shown in **Menu bar > Help > About**\), and run the following commands: ``` # ensure, venv is installed pip install virtualenv # create virtual environment into .venv subfolder python -m venv ".venv" # activate it .venv\Scripts\activate # install all required packages into venv pip install -r requirements.txt # start the server python server.py ``` The server logs every action, so it is possible to review what actions were executed. ### Set up in the SEC Tool To use the signature provider example with the SEC Tool, follow these steps: 1. Create/use workspace for the processor. 2. Select the check-box **Use sign. provider** on the PKI tab. If there are keys in the workspace, they are moved to a back-up subfolder in the workspace. 3. Open the signature provider dialog by clicking **Configure...** next to the check-box from step 2. 4. Review the default parameters of your signature provider. If using the signature provider server from `resources\signature_provider_examples`, the default settings work. 5. Select the prehash option in the parameters table. When prehash is enabled, only a hash of the data is sent to the server for signing. Not all processors support all hash options. For example, processors with MBI can use only hash algorithms whose output length matches the length of the signing keys. See the reference manual for processor-specific details. 6. Click the **Test connection** button to verify if the server is configured properly. 7. There are two options to Import public keys: - In the same dialog, click the **Import public keys** button to import public keys from the server; this is a recommended way, however it can be used only if the server implements optional API **public\_keys\_certs**. - If the **Import public keys** command is not supported, the alternative way is to use **Import keys** from the **PKI management** tab. Make sure that public keys match private keys that are used on the signature provider site \(copy the keys to the folder with the signature provider example\). 8. On the **Build** tab, select the key as normally, now the config files for SB, MBI, and certification block will be using the signature provider configuration. 9. Now, the signature provider is configured. It is possible to build a signed image. #### Signature provider and debug authentication The SEC Tool supports signing of the DA certificate by the signature provider. The field technician flow of the DA key generation is the same as without the signature provider; the debug key pair generation is supported only locally. The only difference is that in the DAC generation on the OEM site, the signature provider is used for signing. This is transparent to the user as the public key is selected from the workspace keys. The only difference is in the generated configuration file, where the **sign_provider** field is set according to the signature provider setting. ## Script hooks workflow Script hooks are executed before or during build, write, and manufacturing script execution. Script hooks enable script customization outside the generated scripts. Hook scripts are located in the "hooks" subfolder and the new workspace contains the examples for the selected processor. Script hooks are not generated by the tool; they are expected to be fully under user control. If the hook script does not exist, it can be created with a single click in the GUI. ### Build script hooks 1. Pre-build hook: `pre_build_.bat/sh` is executed before the build script. This script can be generated to sign the MCUboot application image. This script does not have any argument and it is called only from the GUI before the build script is executed. 2. Build context hook: `build_context_.bat/sh` is called at the beginning of the build script and allows users to add or modify the environment variables. This hook is called without arguments. 3. Build hook: the build_.bat/sh script is executed after each main step in the build script. This script is called from the build script and the name of the previous step is passed as an argument. All the supported steps are handled in the generated examples. If a hook step call fails, the build script execution stops and exits with an error. ### Write script hooks 1. Write the context hook: the `write_context_.bat/sh` script is called at the beginning of the write script and allows users to add or modify the environment variables. This hook is called without arguments. 2. Write the hook: the `write_.bat/sh` script is executed after every main step in the write script. The script is called from the write script and the name of the previous step is passed as an argument. All the supported steps are handled in the generated example. If a hook step call fails, the write script execution stops and exits with an error. ### Manufacturing hooks Manufacturing hook: `manufacturing_.bat/sh` is called at the beginning and end of the manufacturing process before the first task is started and after the last task is finished. If manufacturing hook execution for step **started** fails, planned manufacturing steps are not executed. The call for step **finished** has an additional argument **status** that can have two values **ok** or **fail** that denote the execution status of the manufacturing process: **ok** if all tasks were finished successfully, **fail** otherwise. ### Typical usage Here are a few examples how the hook scripts can be used to customize the build, write, or manufacturing script without the modification of the script generated from the SEC Tool: - Update the input source file\(s\) for the build. - Fix the problem in the write script or apply an additional action that updates the previous action. - Synchronize the manufacturing operation with the assembly line. ## Zephyr This chapter describes the steps to successfully boot up the device Zephyr-based projects. It describes the VS Code setup, creation of the bootable image, connecting your device, setting up your boot preferences, and writing the image into the selected boot memory. Common steps are described first, followed by device family-specific content. It is assumed that the image is executed on an NXP evaluation board. This chapter addresses image preparation for the VS Code IDE. ** Note: **: Debug build configuration is used unless specified differently. For Release build configuration, the steps are the same. More information about Zephyr, VS Code, and MCboot can be found at: - [Working With Zephyr](./10_references.md#working-with-zephyr) - [Zephyr Knowledge Hub](./10_references.md#zephyr-knowledge-hub) ### Common steps #### Prerequisites Option if VS Code is not installed yet: - Use the MCUXpresso Installer to set up all required dependencies, including VS Code; make sure that you select the "Zephyr Developer" option. Option if VS Code is already installed: - Install the "MCUXpresso for VS Code" extension for VS Code: https://marketplace.visualstudio.com/items?itemName=NXPSemiconductors.mcuxpresso - Use the MCUXpresso Installer to set up all required dependencies; make sure that you select the "Zephyr Developer" option. #### Import Zephyr repository 1. Open the MCUXpresso for VS Code extension. 2. From the Quick Start panel, select "Import Repository" (A remote repository was used for this workflow, although other options are also supported). 3. Select the latest Zephyr revision (v4.3.0 was used for the following workflows) and specify the target folder. 4. Click the **Import** button. ### Standalone Zephyr application This chapter describes the steps to successfully boot up the device Zephyr-based project without a secondary bootloader. #### Project creation 1. In VS Code, from the Quick Start panel, select "Import Example from Repository". 2. Select the cloned repository from the previous step. 3. Select your board. 4. Select the "zephyr/samples/basic/blinky" template. 5. Select "App type" as the "Freestanding Application". 6. Fill in the project name, location path. 7. Select Zephyr-SDK - Default Zephyr SDK. 8. Click the **Import** button. 9. Build an application. #### Setting up Secure Provisioning Tool 1. Start Secure Provisioning Tool: - Windows: Double-click the desktop shortcut, or use the Windows Start menu to locate the tool. - MacOS: Click the shortcut in the Dock, or use the Launchpad to locate the tool. - Linux: Click the shortcut in the Launcher, or use the Dash to locate the tool. 2. Create a workspace by selecting File > New workspace … from the menu bar. Select the path to the new workspace. Then select the target processor and click **Create**. 3. Connect the device to the host through USB, UART, SPI, or I2C. 4. Confirm that the connection is working by selecting Target > Connection … from the menu bar and clicking the **Test** button. Tweak if necessary. 5. Configure the Source Image as `/debug/zephyr/zephyr.elf` or `/debug/zephyr/zephyr.bin`. 6. If a pop-up dialog detecting DCD/FCB appears, confirm the defaults. 7. Check if the target memory is correct based on your board and project. 8. Switch the board to ISP mode. 9. Build and Write application to the device. 10. Switch the board to run boot from the selected target memory, reset. ### MCUBoot Zephyr application This chapter describes the steps to successfully boot up the device Zephyr-based project with the MCUboot secondary bootloader. The MCUboot is part of the described example project, so only one project is imported. This chapter does not cover neither replacing the signing key nor signing by the SEC tool as it requires extra changes in the VS Code project and Zephyr does signing of the application automatically. #### Project Creation 1. In VS Code, from the Quick Start panel, select "Import Example from Repository". 2. Select the cloned repository from the previous step. 3. Select your board. 4. Select the "bootloader/mcuboot/samples/zephyr/hello-world" template. 5. Select "App type" as the "Freestanding Application". 6. Fill in the project name, location path. 7. Select the Zephyr-SDK - Default Zephyr SDK. 8. Click the **Import** button. 9. Build the application. During the build several MCUboot actions are executed: 1. Exporting the public portion of the signing key into the C file (autogen-pubkey.c). 2. The MCUboot application is built into `debug/mcuboot/zephyr/zephyr.bin`. 3. The application itself is built into `debug/boot-zephyr-hello-world/zephyr/zephyr.bin`. 4. The application is signed with the private key into a new file `debug/boot-zephyr-hello-world/zephyr/zephyr.signed.bin`. It is necessary to get information on which address the signed application is programmed into the memory. In the `debug/boot-zephyr-hello-world/zephyr/zephyr_final.map` file in the "Memory Configuration" section, the "FLASH" row and "Origin" column contain this information. For example, for MIMXRT1060-EVKC it is 0x60020000. #### Setting up Secure Provisioning Tool 1. Start Secure Provisioning Tool: - Windows: Double-click the desktop shortcut, or use the Windows Start menu to locate the tool. - MacOS: Click the shortcut in the Dock, or use the Launchpad to locate the tool. - Linux: Click the shortcut in the Launcher, or use the Dash to locate the tool. 2. Create a workspace by selecting File > New workspace … from the menu bar. Select the path to the new workspace. Then select the target processor and click **Create**. 3. Connect the device to the host through USB, UART, SPI, or I2C. 4. Confirm that the connection is working by selecting Target > Connection … from the menu bar and clicking the **Test** button. Tweak if necessary. 5. Configure the Source Image as `/debug/mcuboot/zephyr/zephyr.elf` or `/debug/mcuboot/zephyr/zephyr.bin` (the MCUboot). 6. If a pop-up dialog detecting DCD/FCB appears, confirm the defaults. 7. Check if the target memory is correct based on your board and project. 8. Click the **Additional images** button, configure for example, Image 1 to `zephyr.signed.bin`, set the "Boot mem. addr" obtained from the `zephyr_final.map` file. Confirm the dialog. 8. Switch the board to ISP mode. 9. Build and Write application to the device. 10. Switch the board to run boot from the selected target memory, reset. ### Zephyr examples with MCUboot in different memory Not every Zephyr example project can be used as it is. Additional workflow or changes in the project are required. For example, in older Zephyr for MCX N devices, the QSPI examples require a (MCUBoot) bootloader in the internal flash by default. The default start address is not usable for a bootable image creation without the bootloader. For details, see the Zephyr documentation for the given board. Either the bootloader in the internal flash has to be used or the start address must be changed. For the mentioned MCX N devices, the start address can be changed in the `build/zephyr/.config` file: ``` CONFIG_FLASH_BASE_ADDRESS=0x90000000 ``` has to be changed to ``` CONFIG_FLASH_BASE_ADDRESS=0x90001000 ``` ### Disabling MCUboot in Zephyr examples If MCUboot is not required but is enabled in the example, it can be disabled by modifying the following files: - prj.conf: ``` CONFIG_BOOTLOADER_MCUBOOT=n ``` - sysbuild.conf: ``` SB_CONFIG_BOOTLOADER_MCUBOOT=n ``` ## Manufacturing workflow For the manufacturing operations, the tool offers a simplified user interface focused on the manufacturing only. ### Create manufacturing package OEM can create a manufacturing package \(\*.zip\) that can be used to transfer files to the factory. The manufacturing package can be created: - On the **Write image** view - for provisioning using the current write script - In the **SB editor** - to apply commands specified in the SB file ```{eval-rst} .. figure:: _images/Create_Manufacturing_Package_dialog.png :scale: 80% :align: center **Create Manufacturing Package dialog** ``` The **Create Manufacturing Package** dialog allows the user to: - Check package parameters overview. - Review files included in the package. - Check the write script arguments, the arguments are in the same format as they are used in Manufacturing Tool. - Select the output manufacturing package file path. - Set the password for the ZIP file. The AES algorithm is used to encrypt files in the ZIP file; however, the file metadata \(like file names and file sizes\) are not encrypted. - For the EdgeLock 2GO provisioning, it is possible to optionally specify the API key in the manufacturing package, but it can be specified later during manufacturing ### Performance optimization It is supposed that the provisioning/write script will be executed several times to address different development issues, so the script is designed primary for this use case and may contain some parts that are not necessary in manufacturing when the provisioning is applied to an empty processor. Here are some tips to improve manufacturing performance by manually modifying the generated script: - It might not be needed to erase boot memory. If the processor is new, the flash is already erased. - It might not be needed to detect if the chip is already secured; this part in the write script allows updating application for secured processors \(for chips where it is supported\) - A longer sequence of **blhost** operations might not be optimal, because the **blhost** initialization time is not insignificant. It might be better to move the operations into the SB file \(see SB editor\) or use **blhost batch** command \(see SPSDK documentation for details\). - If the processor is reset during manufacturing, there is a delay time until it boots and the OS driver reconnects. By default, it is 3 seconds. The time can be adjusted in preferences. ### Manufacturing operations On the manufacturing site, the manufacturing package can be imported using **main menu \> File \> Import Manufacturing Package...**. During import, the files from the package are extracted into the new workspace - called **manufacturing workspace**. For more information about importing the package, see [Import workspace from the ZIP](./05_user_interface.md#import-workspace-from-the-zip). Once the workspace is created \(or reopened\), the Manufacturing Tool (for details, see [Manufacturing Tool](./05_user_interface.md#manufacturing-tool) ) is displayed, and the rest of the tool functionality is not available. If the Manufacturing Tool is closed, the whole tool operation is finished. If you restart the tool, it offers to continue manufacturing, or to select another workspace: ```{eval-rst} .. figure:: _images/Confirmation_to_reopen_manufacturing.png :scale: 80% :align: center **Confirmation to reopen manufacturing** ``` If the manufacturing package contains a write script, check if the `SPT_INSTALL_BIN` environment variable in the script points to the installation directory on the computer. If not, it is recommended to set the environment variable globally or update the write script manually. For **serial** connection: Adjust the baud rate, the default value is 115200; however, for several processors, baud rates up to 1000000 were successfully tested. ### Steps in the manufacturing production 1. Connect one or more processors via USB or serial line or I2C or SPI and click the Autodetect button to detect the connected devices. In case the tool detects devices that should not be affected by the manufacturing, such as serial ports used by other devices, disable them. Then click **Test connection** below to check the connection with all enabled processors and ensure the test passes. 2. To start the trust provisioning operation, click the Start button. Wait until all operations are finished. 3. If any problem is reported, click to the status cell to show the log and fix the problem. 4. Continue with step 1 The number of successfully provisioned devices is displayed on the bottom of the Manufacturing Tool window, but it is not 100% reliable. ### Manufacturing logs Manufacturing logs are stored in the manufacturing workspace, in the subdirectory `logs/YYYY-MM-DD/`. The log file name is `manufacturing_log_YYYY-MM-DD_hh-mm-ss_#.log`, where `#` represents index of the manufacturing task being executed in parallel. It is possible to export them using the **Export logs** button from the manufacturing window. The export allows to select one day (a date) or all logs and exports the selected logs into the ZIP file. ## MCUboot workflow MCUboot is an open source secure bootloader for 32-bit microcontrollers. For details, see [MCUboot Documentation](./10_references.md#mcuboot-documentation). It has been ported to many NXP processors, and you can find it supported in the MCUXpresso SDK. For details, see `boards\\ota_examples\mcuboot*`. For most of the processors, the SEC Tool contains a default configuration compatible with project examples provided in the MCUXpresso SDK. Therefore, there is a “sample application” built from MCUXpresso SDK for the EVK/FRDM board and the default imgtool parameters match MCUXpresso SDK. For the rest of the processors, the support for MCUboot was not tested; however, it can still be configured in the SEC Tool. ### Steps to start MCUboot for NXP board via New Workspace 1. Open the **New Workspace** dialog and select the processor. 2. Connect the board via UART, ensure that the processor boot is in ISP mode. It is possible to use other connections, the UART is used because the mcuboot application is built with the debug console and prints the status that can be verified using the terminal. 3. Select the MCUboot bootloader image, and the corresponding sample application for the selected processor (including both the bootloader and executable image) will be automatically chosen. If no image is selected, it indicates that a sample application is not available for the selected processor. In such cases, refer to the manual configuration instructions below 4. Select the required profile with memory settings compatible with the sample application, and create the workspace. For MCX N series, IFR must be used. 5. The MCUboot Sign Image dialog will open with all required options preselected, so it is possible to save the options and sign the image. 6. Build and write the bootable image into the processor. **Note:** To verify everything works correctly, refer to step 9. of the manual configuration below. ### Steps to start MCUboot with such a processor manually 1. Create a new workspace for the selected processor. 2. Connect the board via UART, ensure that the processor boot is in ISP mode, and check the connection \(**main menu \> Target \> Connection**...\). It is possible to use other connections, the UART is used because the mcuboot application is built with the debug console and prints the status that can be verified using the terminal. 3. Verify the selected boot memory in **main menu \> Target \> Boot Memory...**. For MCX N series, IFR must be used. 4. On the **Build image** view, select the “mcuboot opensource” application as “Source executable image”. The prebuilt application is available in `sample_data\targets\\source_images\_mcuboot_opensource.s19`. You can also build your own from MCUXpresso SDK. If the application contains a configuration of the external flash \(FCB\), the tool detects and offers to use it. It is recommended to accept. 5. Open **main menu \> Tools \> MCUboot \> Sign Image** and configure the following: - The secondary application to be signed; the prebuilt application is available in `sample_data\targets\\source_images\_ota_mcuboot_basic.s19` - The signing key; it is located in the same folder that the prebuilt application or in MCUXpresso SDK, in folder `boards\\ota_examples\mcuboot_opensource\keys\`. Depending on the platform. use either `sign-rsa2048-priv.pem` or `sign-ecdsa-p256-priv.pem`. Keys protected by a password are not supported yet. - The imgtool arguments by default should match the SDK example. It is not needed to change them. - Click the **Sign** button to sign the application; fix problems, if any. - Ensure that the check boxes below are selected: - the first check-box: the tool creates the pre-build hook script that signs the application before each build - second check-box: the tool reconfigures additional images, so the signed image is written to the target address; keep “Image 1” - Verify the target address of the application. - Close the dialog by clicking the **Save & Close** button. 6. On the **Build** tab, double-check that the **Build script hooks** section contains the pre-build script. 7. Open **Additional Images** and check that the signed application is properly configured as “Image 1”. 8. Build and write the bootable image into the processor. 9. Open a terminal \(in MCUXpresso IDE go to **main menu \> Windows \> Show View \> Other \> Terminal**\), select the UART port, confirm, and reset the processor. You should receive the following text: ``` hello sbl. Bootloader Version 2.0.0 Primary slot: version=1.0.0+0 Image 0 Secondary slot: Image not found writing copy_done; fa_id=0 off=0xfffd0 (0xfffd0) Image 0 loaded from the primary slot Bootloader chainload address offset: 0x0 Reset_Handler address offset: 0x400 Jumping to the image Booting the primary slot - flash remapping is disabled ************************************* * Basic MCUBoot application example * ************************************* Built Apr 16 YYYY 12:34:56 ``` **To sign and write a second copy of the application, follow additional steps:** 1. Disconnect the terminal if it is still open. Reset the board to ISP mode. 2. Open **main menu \> Tools \> MCUboot \> Sign Image**... 3. Keep the same input application image. 4. Change the output image name, for example add suffix 1\_1 5. In imgtool arguments, change version to 1.1 6. In the **Set additional image** section change: - Image 2 - Target address - increase the address by the slot size \(see the slot size parameter in the imgtool arguments\) 7. Save and Close. **Note:** The pre-build script will be overwritten and it will sign Image 2. The previously signed Image 1 remains on the disk untouched and it will be written to flash at the original location. 8. Open **Additional Images** and check that there are two applications: “Image 1” and “Image 2”. 9. Build and write. 10. Connect the terminal, switch the board to boot from the selected boot memory, and reset. The terminal should receive the following text: ``` hello sbl. Bootloader Version 2.0.0 Primary slot: version=1.0.0+0 Secondary slot: version=1.1.0+0 writing copy_done; fa_id=1 off=0xfffd0 (0x1fffd0) Image 0 loaded from the secondary slot Bootloader chainload address offset: 0x100000 Reset_Handler address offset: 0x100400 Jumping to the image Booting the secondary slot - flash remapping is enabled ************************************* * Basic MCUBoot application example * ************************************* Built Apr 16 YYYY 13:24:56 ``` ## EdgeLock 2GO trust provisioning workflow EdgeLock 2GO is a fully managed cloud platform operated by NXP that provides secure provisioning services for easy deployment and maintenance of IoT devices using supported NXP products. The service allows creating and managing secure objects, such as symmetric keys, key-pairs, and certificates that are then securely provisioned into your NXP MCU or MPU. The tool supports the following flows: - **EdgeLock 2GO with device ID** flow, where the manufacturing facility retrieves secure objects from EdgeLock 2GO cloud server during the production process specifically for each processor - **EdgeLock 2GO per product type** flow, where OEM retrieves secure objects database from EdgeLock 2GO server and production in manufacturing facility can operate without online access to EdgeLock 2GO server ### EdgeLock 2GO with device ID, high-level description The figures below correspond to the sequence of actions indicated on Figure "EdgeLock 2GO trust provisioning workflow". **Configuration process** 1. OEM prepares a secure configuration and verifies it locally. Then the SEC Tool provides all secure objects, and the OEM uploads them via the [EdgeLock 2GO web portal](./10_references.md#edgelock-2go-web-portal). 2. OEM sends to manufacturing facility manufacturing package generated from SEC Tool. **Manufacturing process for EdgeLock 2GO with device ID** 3. The tool fetches the processor UUID 4. The tool requests secure objects for the given UUID. The EdgeLock 2GO server validates UUID, generates secure objects, and encrypts them with EdgeLock 2GO root of trust. Secure objects are downloaded to the manufacturing machine. 5. Secure objects and EdgeLock 2GO provisioning firmware are loaded to the target processor. The firmware is invoked to install the secure objects into the target location. The application image is applied into the target boot memory. ```{eval-rst} .. figure:: _images/EdgeLock_2GO_Trust_Provisioning_workflow.svg :scale: 80% :align: center **EdgeLock 2GO trust provisioning workflow** ``` ### EdgeLock 2GO per product type, high-level description **Configuration process** 1. OEM prepares a secure configuration and verifies it locally. Then the SEC Tool provides all secure objects, and the OEM uploads them via the [EdgeLock 2GO web portal](./10_references.md#edgelock-2go-web-portal). **Note:** secure objects for device ID flow and per product flow are the same; however, at the EdgeLock 2GO web portal the device group must be created with different parameters. 2. OEM downloads the database of secure objects and provides the database and manufacturing package to the manufacturing facility. **Manufacturing process for EdgeLock 2GO per product type** 3. The tool fetches the processor UUID and verifies in the database that it is not provisioned yet. 4. The tool fetches secure objects from the database and records into DB UUID of the provisioned device. 5. Secure objects and EdgeLock 2GO provisioning firmware are loaded to the target processor. The firmware is invoked to install the secure objects into the target location. The application image is applied into the target boot memory. ### EdgeLock 2GO flow, step by step This chapter contains a detailed, step-by-step, description of the provisioning flow. The chapter is split into two phases: - **development**: description of how to test the provisioning process with irreversible changes in the processor - **production**: information on how to switch to the deployment life cycle and prepare a package for the manufacturing facility For processor-specific information, see [Processor-specific workflows](./06_processor_specific_workflow.md). #### EdgeLock 2GO flow, step by step, development To configure EdgeLock 2GO provisioning, do the following steps: 1. Turn on secure boot mode and verify that the application works properly. 2. On the [EdgeLock 2GO server](./10_references.md#edgelock-2go-web-portal), create the device group for the product and create an API key. For details, see [EdgeLock 2GO Configuration via web portal](#edgelock-2go-configuration-via-web-portal). 3. In the **main menu \> Target \> Trust Provisioning Mode**, select **EdgeLock 2GO**. Select either **EdgeLock 2GO with device ID** or **EdgeLock 2GO per product type**. Fill the EdgeLock 2GO parameters and test the connection to the server. 4. Install the GnuPG Tool and take advantage of the prepared encryption script. *OS-specific notes:* - Windows: Kleopatra for Windows is recommended: [Kleopatra for Windows (GPG4Win)](./10_references.md#kleopatra-for-windows-gpg4win). The encryption can also be done both manually using “Kleopatra GUI”. See *EdgeLock 2GO Quick Start Guide* \(document AN13255 on [EdgeLock 2GO server](./10_references.md#edgelock-2go-web-portal)\) or using the way described above \(GnuPG utilities are installed with gpg4win\). - Ubuntu: use the gpg package in the Ubuntu repositories. - macOS: gnupg available in the brew package system is a recommended option; GnuPG for OS X should also work \(see [GnuPG downloads](./10_references.md#gnupg-downloads) ) 5. Steps needed to enable the GPG encryption in the build script: - The encryption is done in the `el2go/encrypt_el2go_files_*.*` script generated into the workspace. Use the **Update files** button on the Build page to update the script. - Import the EdgeLock 2GO public key for encryption, see the generated script for how to do it - Generate RSA key pair for signing - `gpg --full-generate-key`. Use 2048 or 4096 key size. - Set environment variables - `EL2GO_GPG_PASSWORD` - password for the generated key pair - `EL2GO_GPG_SIGN_KEY` - identify which key should be used for signing using key ID available by `gpg--list-secret-keys`. If the `EL2GO_GPG_SIGN_KEY` environment variable is defined, the encryption is invoked from the build script as a part of the build action. 6. Ensure that the development life cycle is selected in the **main menu \> Target \> Life Cycle**. For development purposes, the EdgeLock 2GO verification is supported with the open life cycle. This is not intended for production. 7. On the build page, click **Build image** to build the application. Ensure that there are no errors. Ensure the connected processor and target flash memory are clear. 8. Open the `/el2go/publish` subfolder and upload all secure assets into the [EdgeLock 2GO server](./10_references.md#edgelock-2go-web-portal). Follow the instructions provided in [EdgeLock 2GO Configuration via web portal](#edgelock-2go-configuration-via-web-portal). **Note:** Files for the EdgeLock 2GO server are also displayed on the build page. In the generated files, they are marked by the el2go cloud icon. The description is displayed in the tooltip. 9. For EdgeLock 2GO per product flow, follow [Create database with secure objects for EdgeLock 2GO per product type](#database-with-secure-objects-for-edgelock-2go-per-product-type). 10. Go to the **Write** page and run the Write operation. #### EdgeLock 2GO flow, step by step, production 12. If everything works as expected, set the deployment life cycle and repeat steps 7, 8, 9, 10. Make sure that the policy for uploaded secure objects is aligned with the life cycle. 13. If everything works as expected, create the manufacturing package. For details, see [Create manufacturing package](#create-manufacturing-package). For API key distribution, see [API key to access EdgeLock 2GO server](#api-key-to-access-edgelock-2go-server). ### API key to access EdgeLock 2GO server - For development, the API key must be specified in the **Trust Provisioning Mode** dialog. - For **EdgeLock 2GO per product type**, the API key is not used in the manufacturing - For **EdgeLock 2GO with device ID**, the API key is also needed for manufacturing: - For the manufacturing package, the API key can be specified optionally; if it is specified, it is recommended to encrypt the package with a password to protect the access. - If the API key is not specified in the manufacturing package, it can be specified in the manufacturing dialog or via the environment variable SEC\_EL2GO\_API\_KEY. - For EdgeLock 2GO trust provisioning, the following access needs to be enabled for the manufacturing API key on the EdgeLock 2GO server: - View - View device groups - General - Register devices - Remote trust provisioning - View secure objects and their intermediate CAs - For EdgeLock 2GO WPC provisioning, the following access needs to be enabled for the manufacturing API key on the EdgeLock 2GO server: - View - View Qi related data - Manage - Assign and unassign Qi templates to Device Groups and query jobs for batch processing ### EdgeLock 2GO configuration via web portal EdgeLock 2GO web portal URL: [EdgeLock 2GO web portal](./10_references.md#edgelock-2go-web-portal) The following Application Note provides detailed information: [EdgeLock 2GO Provisioning via Secure Provisioning Tool (SEC) for MCUs (document AN14624)](./10_references.md#edgelock-2go-application-note). **How to create a device group** - Devices \> New Device Group - Assign any name - Hardware family type: MPU and MCU - Hardware option: product name - Hardware type and product name: select a processor by name **How to create RKTH secure object** - Secure Objects \> New Secure Object - Select type: OEM FW Authentication Key Hash - Assign any name - Provide a binary file: - Usage policies: add a custom policy. Select the **Open** or **Closed/Locked** policy. **Open** is used for development and testing, **Closed** and **Closed/Locked** are used for production. The policy is to be aligned with the life cycle selected in the tool. For details, see processor-specific recommendations. **How to create CUST-MK-SK secure object** - Secure Objects \> New Secure Object - Select type: OEM FW Decryption Key - Assign any name - Provide the key material \(.asc\): provide a signed and encrypted key. It is generated by a SEC Tool via GnuPG. - Provide the public key to use it for verifying the signature of the encrypted key. \(.asc\): your public key - Usage policies: same as RKTH; the policy must be the same for all secure objects used in one device group. **Other secure object** See processor-specific information in [Processor-specific workflows](./06_processor_specific_workflow.md). ### Database with secure objects for EdgeLock 2GO per product type There are two types of the databases: - **static database**: does not contain any processor specific secure objects - **dynamic database**: contains processor-specific certificates To create a database of secure objects for "offline" provisioning (EdgeLock 2GO per product type), follow these steps: 1. Open **main menu > Targets > Trust Provisioning Mode...** and ensure **EdgeLock 2GO per product type** is selected. 2. In **Per Product Database** panel, specify: - number of devices per database - number of databases to be generated These parameters will be used for dynamic database only. For a static database, the parameters will be ignored. 3. Click the button to start generation. The generation of dynamic databases may require several hours when processing a large number of processors or secure objects. A progress bar with an estimated completion time is displayed. Do not close the window until the database generation is complete. 4. Click the **Download** button to download the databases from the server. For the write operation (in development), the database name is hard-coded to `/trust_provisioning/el2go_product_batch.db`. For manufacturing operation, the database name and location can be selected in the manufacturing dialog. Databases are not included in the manufacturing package and are expected to be delivered separately. ## Merge Images Tool workflow This section describes merging two separate images into one single image. The reason for merging might be signing both images together during the build process. This section is written for MCUXpresso IDE with the Trust zone hello world SDK example, which contains two separate projects `_hello_world_s` and `_hello_worlds_ns` linked together. It is necessary to remove the link between the projects (MCUXpresso IDE) to generate two separated images instead of one image created during the build process by merging both projects together. As an example processor the MIMXRT595 is used. For other processors the workflow is the same, except of the start addresses. ### Building the TrustZone example projects for merge 1. Remove linking between both projects by selecting the non-secured project `_hello_world_ns` go to **Project \> Properties \> Project References** and unchecking the `_hello_world_s` from the references. 2. Build both projects without any modifications 3. This example uses .s19 files so the final .axf files need to be converted. To do so, go to the Debug folder for both projects, right-click the generated `_hello_world_*.axf` file, and choose **Binary Utilities \> Create S-Record**. ### Merging two images into one 1. Open the Merge Tool by selecting **main menu \> Tools \> Merge Tool**. 2. Select `_hello_world_s.s19`. The target address will be automatically set to `0x18001000` (secured memory area) 3. For MIMXRT595 processors, only the non-secured address can be written by the user. The given address of the first image is in the secured memory map. Change the target address of the first image to `0x08001000` (non-secured memory area) 4. Select `_hello_world_ns.s19`. The target address will be automatically set to `0x08100000` (non-secured memory area) 5. Check the **Apply the merged images as the Source executable image on Build image view** checkbox 6. Leave the rest as it is and press the OK button 7. Check that the image is automatically applied as a Source executable image and its start address is updated as well ### Signing merged image To sign and build the merged image, see the [Booting signed image using shadow registers](./06_processor_specific_workflow.md#booting-signed-image-using-shadow-registers) section, but use the merged image as a Source executable image instead. ## Custom USB VID and PID devices workflow If you have a device with custom VID&PID, it is possible to select the custom VID&PID in the **main menu > Target > Connection**. Selected VID&PID is used for the *whole* write operation. Write script does not support a change of VID&PID during its execution. It is recommended to change VID&PID prior to the write operation (for example, using PFR configuration or OTP configuration in **Advanced mode**), reset the processor and then start the write operation with custom VID&PID. For manufacturing operation, custom VID&PID must be selected in the Connection configuration during the creation of the manufacturing package. With such configuration, the manufacturing operation accepts both default and custom VID&PID.