# Installation This chapter describes the procedure required to install SEC on Windows, macOS, and Linux operating systems. For the supported operating systems, refer to Minimum system requirements. ## Minimum system requirements The tool runs on Microsoft\(R\) Windows\(R\), Ubuntu, and macOS operating systems. The detailed system requirements are specified in [Secure Provisioning Tool Release Notes](./10_references.md#secure-provisioning-tool-release-notes). The document also describes what debug probe drivers should be installed. These drivers might also be needed for communication with the processor in ISP mode where the probe provides USB to UART/SPI/I2C converter. ## Windows To install SEC as a desktop application on a local host, perform the following steps: 1. Visit the [Secure Provisioning Tool home page](./10_references.md#secure-provisioning-tool-home-page) to download the SEC installer for Windows. 2. Double-click the `MCUXpresso_Secure_Provisioning_.exe` installer to begin installation. 3. On the first page of the wizard, click **Next**. ```{eval-rst} .. figure:: _images/SEC_tool_setup.png :scale: 80% :align: center **Secure Provisioning Tool Setup** ``` 4. On the **End-User License Agreement** page of the wizard, select **I accept the terms of the License Agreement** and click **Next**. ```{eval-rst} .. figure:: _images/accepting_the_end_user_license_agreement.png :scale: 80% :align: center **Accepting the end-user license agreement** ``` 5. On the **Select Installation Folder** page of the wizard, select **Browse** and navigate to the destination folder you want to install the SEC to and click **Next**. ```{eval-rst} .. figure:: _images/selecting_installation_folder.png :scale: 80% :align: center **Selecting installation folder** ``` 6. On the **Configure Shortcuts** page of the wizard, select the shortcuts you want to be created for SEC and click **Next**. ```{eval-rst} .. figure:: _images/configuring_shortcuts.png :scale: 80% :align: center **Configuring shortcuts** ``` 7. On the **Ready to Install** page of the wizard, select **Install**. The setup begins the installation. **Note:** If you want to review or change any of your installation settings, click **Back**. Click **Cancel** to exit the wizard. The installer prompts you when the installation completes. ```{eval-rst} .. figure:: _images/ready_to_install.png :scale: 80% :align: center **Ready to install** .. figure:: _images/installing_sec_tool.png :scale: 80% :align: center **Installing Secure Provisioning Tool** ``` 8. Click **Finish** to close and exit the setup wizard. ```{eval-rst} .. figure:: _images/completing_installation.png :scale: 80% :align: center **Completing installation** ``` 9. To start using SEC, run the tool from the desktop shortcut on the desktop or from the **Start** menu. You can also navigate to the *\\bin\\* folder and launch the `securep.exe` or launch the shortcut in the **. ### Windows CLI It is possible to install the SEC Tool using the command line. In this case, use **Run the installer** with the following parameters: start /wait ``` MCUXpresso_Secure_Provisioning_YY.MM.exe /exenoui /qn ``` ## MacOS To install SEC as a desktop application on a local host, perform the following steps: 1. Visit the [Secure Provisioning Tool home page](./10_references.md#secure-provisioning-tool-home-page) to download the SEC installer for macOS. Based on your computer, select either an installer for an Intel or Apple M processor. 2. Double-click the `MCUXpresso_Secure_Provisioning_YY.MM.pkg` to start the **Install MCUXpresso Secure Provisioning Tool** wizard. **Note:** When you try to open the macOS installer, you may receive an error. To avoid it, manually select the option **Mac App Store and identified developers** in the **Security & Privacy** menu. 3. On the **Introduction** page, click **Continue**. ```{eval-rst} .. figure:: _images/introduction.png :scale: 80% :align: center **Introduction** ``` 4. On the **Software License Agreement** page, click **Continue**. ```{eval-rst} .. figure:: _images/software_license_agreement.png :scale: 80% :align: center **Software license agreement** ``` 5. Confirm that you have read and agreed to the terms of the Software License Agreement by clicking **Agree**. ```{eval-rst} .. figure:: _images/accepting_software_license_agreement.png :scale: 80% :align: center **Accepting software license agreement** ``` 6. On the **Destination Select** page, click the green arrow to select the installation folder, and once done, click **Continue**. ```{eval-rst} .. figure:: _images/select_destination.png :scale: 80% :align: center **Select destination** ``` 7. On the **Installation Type** page, click **Install**. ```{eval-rst} .. figure:: _images/installation_type.png :scale: 80% :align: center **Installation type** ``` 8. Type in your login credentials to continue with the installation and click **Install Software**. ```{eval-rst} .. figure:: _images/install_software.png :scale: 80% :align: center **Install software** ``` 9. Click **Continue**. Unless errors are reported, the **Summary** page confirms that the installation was completed successfully. 10. On the **Summary** page, click **Close**. ```{eval-rst} .. figure:: _images/summary.png :scale: 80% :align: center **Summary** ``` ### Enabling USB connection on macOS During the first connection to the target by USB, macOS X Catalina blocks the access to USB HID devices as a security measure and the operation will fail with error. In macOS 13 \(Ventura\), this works differently and these steps are not needed. Perform the following steps to enable USB connection: 1. In the OS security alert message box, select **Open System Preferences**. ```{eval-rst} .. figure:: _images/open_system_preferences.png :scale: 100% :align: center **Open System Preferences** ``` 2. Unlock **Privacy** preferences to enable changes. 3. Select **MCUXpresso Secure Provisioning Tool YY.MM**, confirm, and quit the application. ```{eval-rst} .. figure:: _images/confirm_change.png :scale: 100% :align: center **Confirm change** ``` 4. Lock **Privacy** preferences. 5. If the application was not closed, close it manually. 6. Start the application and proceed with the operation. ## Linux Installation of SEC on Ubuntu can be done in the Terminal. 1. Visit the [Secure Provisioning Tool home page](./10_references.md#secure-provisioning-tool-home-page) to download the SEC installer for Linux. 2. Open the terminal and change the directory where the installer is downloaded, install using dpkg with sudo. ``` $ cd ~/Downloads $ sudo dpkg -i mcuxpresso-secure-provisioning-__.deb ``` If the command executed with sudo is successful, the setup installs the SEC Tool in the dedicated folder /opt/nxp/. **Note:** SEC depends on other packages that have to be installed in advance: ``` $ sudo apt install libhidapi-dev libsdl2-2.0-0 ``` ## Uninstalling ### Windows The Secure Provisioning Tool can be uninstalled in the following ways: - by using Settings \| Apps & features ```{eval-rst} .. figure:: _images/settings.png :scale: 45% :align: center **Settings** ``` - by navigating into the `%APPDATA%\NXP Semiconductors` and then finding the appropriate MSI installer in the `Secure Provisioning Tool YY.MM\install\` folder and choosing the **Remove** option in the wizard. ```{eval-rst} .. figure:: _images/secure_provisioning_tool_setup_wizard.png :scale: 80% :align: center **Secure Provisioning Tool setup wizard** ``` ### MacOS The Secure Provisioning Tool can be uninstalled using Finder, by navigating to Applications, and moving `SEC_Provi_##.##` into the Trash. ### Linux The Secure Provisioning Tool can be uninstalled by using the Debian package manager. In the Terminal, you can get the list of secure provisioning tools with the package names: ``` $ dpkg --list "*-secure-provisioning*" Desired=Unknown/Install/Remove/Purge/Hold | Status=Not/Inst/Conf-files/Unpacked/halF-conf/Half-inst/trig-aWait/Trig-pend |/ Err?=(none)/Reinst-required (Status,Err: uppercase=bad) ||/ Name Version Architecture Description +++-=======================================-============-============-==================================== ii mcuxpresso-secure-provisioning-25.09 25.09 amd64 MCUXpresso Secure Provisioning Tool ii mcuxpresso-secure-provisioning-v3.1 3.1 amd64 MCUXpresso Secure Provisioning ii mcuxpresso-secure-provisioning-v4 4.0 amd64 MCUXpresso Secure Provisioning ``` Now, the desired version can be uninstalled: ``` $ sudo dpkg --remove mcuxpresso-secure-provisioning-25.09 ``` ### Remove configuration files The user preferences are stored in the folder `\.nxp\secure_provisioning_\` and are not removed by uninstalling the product. These folders can be removed manually. For more details about preferences, see [Preferences](./05_user_interface.md#preferences). ### Remove restricted data The restricted data are installed in the folder `\.nxp\secure_provisioning_restricted_data\` and are not removed by uninstalling the product. These folders can be removed manually.