Terms and definitions

Table 2. Terms and definitions

Term

Definition

AAD

Additional Authenticated Data; typically used with AES-GCM

ADKP

Application Debug Key/Password

AES

Advanced Encryption Standard

AES-128

Rijndael cipher with block and key sizes of 128 bits

AHAB

Advanced High Assurance Boot

ASB

Advanced Secure Boot

ATF

ARM Trusted Firmware

BCA

Bootloader Configuration Area

BEE

Bus Encryption Engine

Block cipher

Encryption algorithm that works on blocks of N={64, 128, …} bits

CA

Certificate Authority, the holder of a private key used to certify public keys

CAAM

Cryptographic Acceleration and Assurance Module, an accelerator for encryption, stream cipher, and hashing algorithms, with a random number generator and runtime integrity checker

CBC

Cipher Block Chaining, a cipher mode that uses the feedback between the ciphertext blocks

CBC-MAC

A message authentication code computed with a block cipher

CFPA

Customer In-field Programmable Area

Cipher block

The minimum amount of data on which a block cipher operates

Ciphertext

Encrypted data

CMAC

Cipher-based Message Authentication Code

CMPA

Customer Manufacturing/Factory Programmable Area

CMS

Cryptographic Message Syntax, a general format for data that may have cryptography applied to it, such as digital signatures and digital envelopes. HAB uses the CMS as a container holding PKCS#1 signatures.

CR

Core Reset

CSEc

Cryptographic Services Engine / EdgeLock Accelerator, feature set for various encryption, decryption, and authentication algorithms built to meet the SHE specification.

CSF

Command Sequence File, a binary data structure interpreted by the HAB to guide authentication operations

DA

Debug Authentication

DAC

Debug Authentication Certificate

DAP

Debug Authentication Protocol

DCD

Device Configuration Data, a binary table used by the ROM code to configure the device at an early boot stage

DCP

Data coprocessor, an accelerator for AES encryption and SHA hashing algorithms

DEK

Data encryption key, a one-time session key used to encrypt the bulk of the boot image

DUK

Device Unique Key

DUKB

DUK certificate block

ECB

Electronic Code Book, a cipher mode with no feedback between the ciphertext blocks

ECC

Elliptic Curve Cryptography

ECDSA

Elliptic Curve Digital Signature Algorithm

EdDSA

Edwards-curve Digital Signature Algorithm

ECU

Electronic Control Unit

EKIB

Encrypted Key Info Block

ELE

EdgeLock Secure Enclave

EPRDB

Encrypted Protection Region Descriptor Block

EXT. CMPA

Extended CMPA region; customer‑defined data cannot be updated in Locked LC

EXT. CFPA

Extended CFPA region; customer‑defined data can be updated in Locked LC

FAC

Flash Access Controlled

FCB

Flash Configuration Block or Flash Control Block

FCF

Flash Configuration Field; can also be referenced as FCB

GCM

Galois/Counter Mode; it is a mode of operation for symmetric key cryptographic block ciphers, most commonly used with AES

GUI

Graphical User Interface

HAB

High Assurance Boot, a software library executed in internal ROM on the Freescale processor at boot time that, among other things, authenticates software in external memory by verifying digital signatures in accordance with a CSF. This document is strictly limited to processors running HABv4

Hash

Digest computation algorithm

HSE

Hardware Security Engine

HSM

Hardware System Module

IEE

Inline Encryption Engine

IFR

Information Flash Region

IMG

Image Signing Key, interchangeable term with ISK

ISK

Image Signing Key, interchangeable term with IMG

ISP

In-system programming, a mode in which the processor can be programmed directly into the product

IVT

Image Vector Table

KEK

Key Encryption Key, used to encrypt a session key or DEK

KeyBlob

KeyBlob is a data structure that wraps the key and the counter and the range of image decryption using AESCTR (AES in Counter mode) algorithm

KIB

Key Info Block with KEY and IV for AES128-CBC, recall the key and IV used in PRDB wrap and unwrap is defined as key info block

MAC

Message Authentication Code. Provides integrity and authentication checks

Message digest

A unique value computed from the data using a hash algorithm; provides only an integrity check (unless encrypted)

MLDSA

Module-Lattice-Based Digital Signature Algorithm, a post-quantum cryptographic standard designed to provide secure digital signatures that are resistant to attacks from quantum computers

NBU

Narrowband Unit

NDA

Non-disclosure Agreement

OEI

Optional Executable Image

OEM

Original Equipment Manufacturer

OS

Operating System

OTFAD

On-The-Fly AES Decryption

OTP

One-Time Programmable. OTP hardware includes masked ROM, and electrically programmable fuses (eFuses).

OTPMK

One-Time Programmable Master Key

PFR

Protected Flash Region

PKCS#1

Standard specifying the use of the RSA algorithm. For more information, see PKCS#1 Wikipedia article and RSA PKCS#1 security archive Security archive.

PKI

Public Key Infrastructure, a hierarchy of public key certificates in which each certificate (except the root certificate) can be verified using the public key above it

Plaintext

Unencrypted data

PQC

Post-Quantum Cryptography – cryptographic algorithms designed to be secure against quantum computers

PRDB

Protection Region Descriptor Block recalls the counter and the range of image decryption using the AES-CTR algorithm

PRINCE

lightweight block cipher designed for low-latency hardware implementations, especially in environments like embedded systems and IoT devices

PUC

Product Unit Certificates

PUF

Physical Unclonable Function

pyOCD

Python-based tool and API for debugging, programming, and exploring Arm Cortex microcontrollers; for details, see pyOCD official website

Rijndael

Block cipher chosen by the US Government to replace DES; pronounced rain-dahl

ROMCFG

ROM Bootloader configurations

RoT

Root of Trust

RSA

A public key cryptography algorithm developed by Rivest, Shamir, and Adleman; Hardware accelerator (including hash acceleration) is found on some processors

RSA-PSS

RSA probabilistic signature scheme

SDP

Serial Download Protocol, also called UART/USB Serial Download mode. IT allows code provisioning through UART or USB during production and development phases

SEC Tool

Secure Provisioning Tool

Session key

The encryption key is generated at the time of encryption. Only ever used once

SHA

Secure Hash Algorithm, family of cryptographic hash functions

SHE

Secure Hardware Extension

SI

Secure installer

SMR

Secure Memory Region

SNVS

Secure Non-Volatile Storage

SPL

Secondary Program Loader

SPSDK

Secure Provisioning SDK, an open source Python library, and command-line tools for secure provisioning of NXP processors

SRK

Super Root Key, an RSA key pair that forms the start of the boot-time authentication chain. The hash of the SRK public key is embedded in the processor using OTP hardware. The SRK private key is held by the CA. Unless explicitly noted, SRK in this document refers to the public key only

TEE

Trusted Execution Environment

UID

Unique Identifier, a unique value (such as a serial number) assigned to each processor during fabrication

UUID

Same as UID

USB VID/PID

USB stands for Universal Serial Bus, VID = Vendor ID, PID = Product ID

UUU

Universal Update Utility used to download images to different MPU devices

V2X

Vehicle-to-everything is a standalone cryptographic accelerator (EdgeLock Accelerator) on i.MX 95

WPC

Wireless Power Consortium

XIP

Execute-In-Place refers to a software image that is executed directly from its non-volatile storage location rather than first being copied to volatile memory

XMCD

External Memory Configuration Data