Release Notes for MCUXpresso Secure Provisioning Tool#
Version: 25.06
Date: June-2025
Overview#
MCUXpresso Secure Provisioning Tool (SEC) is a graphical user interface (GUI) tool covering secure boot process and trust provisioning capabilities, primarily aimed at microcontroller customers. It provides a unified GUI front-end over SPSDK command-line tools. The tool is designed to help users to prepare complex security configuration easily, while it keeps the possibility to customize the generated scripts.
Supported processors#
i.MX RT1xxx processors:
RT101x, RT102x, RT104x, RT1050, RT106x
RT116x, RT117x, RT118x
i.MX RT5xx/6xx/7xx processors:
RT5xxS, RT685S, RT7xxS
Kinetis W processors:
K32W148, KW45B41Zx, KW47B42Zxx, KW47Z420xx, KW45Z410xx
LPC55Sxx and LPC55xx processors:
LPC55S6x, LPC55S3x, LPC55S2x, LPC55S1x and LPC55S0x
LPC553x, LPC552x, LPC551x and LPC550x
LPC865
NHS52S04
MC56F816xx/7xx/8xx processors
MCX processors:
MCXA13x, MCXA14x, MCXA15x
MCXCx4x
MCXE24x
MCXN94x, MCXN54x, MCXN23x
MCXW236, MCXW716x, MCXW727x
RW61x processors
MWCT2x12/D2 processors
i.MX 9x processors:
MIMX9352
MIMX9596
Features#
Conversion of ELF executables, SREC, HEX, and raw binaries into bootable images files
Credentials (keys, signatures, and certificates) generation and management associated with signed/encrypted images
Target device connection via UART, USB-HID, SPI, and I2C
Writing FlexSPI NOR, FlexSPI NAND, SEMC NAND, eMMC or SD card boot device including configuration of the boot device parameters
Use of DCD/XMCD configuration for SDRAM images bootup
Programming customizable eFuses and/or protected flash regions per image and use case requirements
Optional batch scripts generation for later use without the GUI
Streamlined operation for general users
Manufacturing Tool with the support of parallel execution
Trust provisioning and device HSM provisioning for selected processors
Flash programming GUI tool
Debug authentication
SB editor tool including support of device HSM SB files
Support of MCUboot secondary bootloader
Detailed supported features for each processor in the user guide (see SEC-Tool-Features.xls spreadsheet embedded in the PDF)
Available for Windows, Linux, and macOS
System requirements#
One of the following Host Operating systems:
Microsoft(R) Windows(R) 11 (64-bit)
macOS 14 Sonoma (Intel x86_64 or Aarch64)
Ubuntu 22.04 LTS 64 bit, with “OpenSSL 1.1.1f 31 Mar 2020”; GNOME recommended
Ubuntu 24.04 LTS 64 bit, with GNOME and OpenSSL 3.0.13 30 Jan 2024; GNOME is recommended.
4 GB RAM or more
Minimal display with resolution:
Windows: 1280 x 720 with 100% scale; higher resolution can be used with higher scale (for example 1920 x 1080 with 150% scale)
Linux: 1366 x 768
P&E Micro debug probe users: install drivers from P&E web site or install MCUXpresso IDE
P&E Micro does not support macOS Aarch64
Lauterbach debug probe users: install Lauterbach from Lauterbach web site and configure access over network in config.t32
MCU-Link or LPC-Link debug probe users: install drivers from NXP web site (see user guide for the links)
Known issues and limitations#
For more information, see chapter Troubleshooting in the documentation.
What is new#
This chapter provides details about the changes for each released version of the tool.
Version 25.06, June-2025#
Supported new processors:
MCXE24x processors: MCXE245, MCXE246, MCXE247
KW45Z410xx processors: KW45Z41052, KW45Z41053, KW45Z41082, KW45Z41083
Supported Edgelock 2GO WPC provisioning for the MWCT processors
Added support for secure boot for the KW47 and MCXW727x processors
Added high-level command for KW processors to update NBU firmware
Added support for fuses longer than 32 bits
Added support for encryption, firmware version for the i.MX RT7xx processors
Added full support for custom VID&PID in manufacturing; Improved logs for manufacturing
To prioritize the tool improvements, an option to collect information about the tool usage is added.
Added an option to lock RT116x/7x fuses during programming
Workspace Wizard: Processors in the tree are organized by purpose
Dropped support of the following features:
Smart card trust provisioning
Loading settings created by the tool version 4.x or older
LPC55xx and RT5xx/6xx: Workspace subdirectory “gen_sb” renamed to “config”, unified with other processors
Integrated SPSDK 3.0.1 with several incompatibilities, such as:
Parameter “file” in the SB load command is renamed to “data”
BD file converted to YAML format
mbi_config.yaml unified and removed unused fields
Parameters for several SPSDK applications changed
Removed support of smart card trust provisioning
Added logs into
workspace/logs
OTP, PFR, IFR and FCF/BCA descriptions unified with SPSDK
MCUboot application updated from 2.0 to 2.1
Added RW61x Edgelock2GO provisioning FW v2.0
Version 25.03.01, April-2025#
Minor update to fix failure of the LPCs write script for Windows if CFPA is not updated
Version 25.03, March-2025#
Supported new processors:
i.MX RT1043 and RT1046 processors
MCX A13x processors
MCX C processors: MCXC041, MCXC242, MCXC444
MCX W236 processor
i.MX 9352 (unsigned and signed images)
KW47 and MCXW727x processors, unsigned boot types only
Support of EdgeLock 2GO Trust provisioning for KW45, K32W, MCXW71x and MCXN
LPC55Sxx and NHS: added support of dual boot (ping/pong)
RT7xx: added support of signed load-to-ram image via SB file; added XMCD support
Key revocation for LPC55Sxx/RTxxx processors
RT118x: added support for RSA-PSS keys
Added Merge Images tool to merge up to 8 images into one single binary file
Ability to export and import workspace, see
main menu > FileAdded command
main menu > Help > Release notesLPC55Sxx and RT5xx/6xx: RSA4K bit set if 4K keys generated, so debug authentication works
Option to check for a new version of the tool, see
main menu > File > PreferencesAdded detection whether device HSM rebuild is needed, if not it is skipped automatically
Log files moved to new workspace sub-directory called ‘logs’
CMPA and CFPA yaml files contains values in RAW format, to avoid problems with hidden post progress conversions
Added warning if user opens a workspace from older version
Improved names of the boot modes (plain vs encrypted)
Fuses from restricted data package moved to the tool and they are no more restricted
LPC55S0x/1x/2x/6x and NHS52S04: Backward incompatibility with version 10:
PFR.CMPA.RSA4K bit-field is not preset by the tool; it is only validated and warning is displayed
Integrated SPSDK 2.6.1 with lpcprog and nxpuuu tools
nxpuuu is intended to replace uuu tool which is now deprecated and might be removed in next release
Lauterbach debug probe support (Windows only)
Version 10.0, November 2024#
A new dialog for workspace creation with predefined profiles is added.
Support for MCX W71xx processors is added.
Preliminary support for i.MX RT798, plain, crc, and signed images is added.
Preliminary support for i.MX 95, silicon revision a1, unsigned images is added.
Support of EdgeLock 2GO Trust provisioning for MCXNx4x and RW61x; device HSM unified with the EdgeLock 2GO process is added.
RW61x: FRDM-RW61x is now the default memory configuration for a new workspace; fuses were updated.
The Manufacturing package can be optionally encrypted with a password.
A hook for modification of environment variables at the start of the build and write scripts is added.
Support of additional images for KW45xx and K32W1xx is added.
Additional predefined configurations are added for the boot memory configuration (not verified on silicon).
The `Create FCB` command is now back-up and restores the content of the memory where FCB is stored.
The TrustZone templates are now preset on the build page, so it is easier to find them and customize; the file can be also in the YAML format.
i.MX RT10xx: the SEC_SET_ENGINE section is removed from the BD file.
Third-party licenses are added into the product layout. See the “licenses” subfolder.
Support of environment variables in CLI is added. Environment variables are supported in all paths arguments and in configuration json files.
Integrated NXP Secure Provisioning SDK 2.3.1
Version 9.0.1, August 2024#
Authentication for ECC keys for i.MX RT116x/7x is fixed.
Authentication for ECC 384/521 is fixed.
The random invalid signature for ECC 256 is fixed.
Freeze in the PRINCE dialog setting for MCXN and LPCs is fixed.
MCX N PRINCE incorrect configuration, mainly if more regions are configured, is fixed by the configMemory parameter in the SB file.
Version 9.0, July 2024#
Support for MCF56816xx/7xx/8xx processors is added.
Support for MCXN23x and additional MCXA14x/MCXA15x processors is added.
Support for MWCT2x12/D2 processors is added.
Support for the NHS52S04 processor is added.
Support for MCUboot - open source secondary bootloader ia added.
Additional images can be used for most of the processors (except KW).
The exported OTP/PFR/IFR configuration now contains the page name that is validated during the import.
The firmware version is supported for LPC55Sxx and i.MX RTxxx processors; for RT118x it is available only for signed images.
The minimal firmware version can now be specified in the firmware configuration dialog.
Support for build, write, and manufacturing script hooks is added.
The limitation for key chain length for LPC55S6x and i.MX RTxxx processors is removed; for other LPCs changed to warning.
The support for FlexSPI instance selection for FlexSPI NAND for i.MX RT116x/7x is added.
The supported key revocation constraint for LPC55S3x, MCX N1xx, RW61x, KW45, and K32W processors.
The MBI image is partially erased before the device HSM, so it does not boot after reset. Applies for MCXN10, MCXN11, LPC55S3x, RW61x, and MWCT2x12.
In the installation layout, the “sample_data” sub-folder (soft link) is created. It contains sample binary applications, signature provider examples, trust zone, XMCD, and DCD configuration templates.
Signature provider:
Support of sending only a hash of the data for signing is added.
Incompatible change in encoding of send public keys, public keys are encoded in the standard key encodings (pem, der, nxp) instead of the hex format.
Integrated NXP Secure Provisioning SDK 2.2.x with the following highlighted changes:
New tools: nxpmemcfg, dk6prog, el2go, nxpwpc
i.MX RT1050/6x: eMMC supported
RW61x: device HSM provisioning now required device HSM loader from restricted data
The support for JLink and PEmicro debug libraries is removed. All debug probes are now supported via pyOCD.
CLI tools (imgtool and uuu) are added.
CLI: support to save or change workspace settings and specify additional images is added.
$check_fw_versions SB2.1 high-level commands for SB editor are fixed.
The default flash (W25Q512NWEQ) for i.MX RT117x based on the flash used on RT117x-EVKB is fixed.
The key used to sign flashloader for i.MX RT10xx and RT116x/7x is fixed - changed from the first key to the selected key.
The flashloader for i.MX RT1181/82 processors is fixed.
Version 8.0, January 2024#
LPC55S3x, KW45xx, K32W1xx: added support for images executed in RAM (xip images)
Added support for MCXN9xx/MCXN5xx/MCXA14x/MCXA15x processors
Added support for i.MX RT118x processors with new option to include additional images into the build
RT1181 and RT1182 processors are not available in the release time, the tool was tested on preproduction silicon only
Added support for RW61x processors (including shadow registers)
Added support for SB 2.1 Editor, supported for i.MX RTxxx and LPC55Sxx processors
Added an option to configure signature provider via a custom web server
Added an option to specify separate FCB files for flash programming and runtime
Supported ECC keys for i.MX RT116x/7x
i.MX RT11xx bootable image can be used as the source image for the build (previously this was only for RT10xx)
Added support for multiple monitors
Integrated NXP Secure Provisioning SDK 2.x with the following highlighted changes:
elftosb tool removed, replaced by nxpimage; nxpkeygen tool replaced by nxpcrypto
updated changes in command-line arguments
several additional incompatible changes in configuration files
LPC55S3x, KW45xx, K32W1xx: spsdk/nxpkeygen tool replaced by spsdk/nxpcrypto
Removed legacy tools arm-none-eabi-objcopy, blhost, sdphost, elftosb, image_enc, and cst (fully replaced by spsdk tools)
New installer for Mac OS with Apple M processor (previously Intel processor only was supported)
Windows: the workspace can now be located on a drive with a letter other than the letter of the installed application.
Version 7.0, July 2023#
Smart card trust provisioning is supported for the LPC55S36 processor
Smart card trust provisioning is supported only for smart card 1.2 or higher
Redesigned configuration of boot memory; added support for user presets and custom-protected area
Newly added dual image (ping/pong) boot support is extended to LPC55(S)3x, KW45xx, K32W1xx, and RT116x/7x
Added support for SB 3.1 editor for LPC55S3x, KW45xx, and K32W1xx processors
Improved configuration of IFR/ROMCFG for KW45xx and K32W1xx processors, now configured per 16-byte blocks
i.MX RT116x/7x: legacy elftosb and image_enc tools are replaced by spsdk/nxpimage
i.MX RT116x/7x: flashloader is updated and detection of locked fuses (via blhost get-property 31) is added
i.MX RT116x/7x: eMMC is supported
i.MX RT11xx: XMCD is supported, either via the link to the configuration file or via a simplified GUI editor
i.MX RT10xx: support for SPI NAND is added
Grouping of processors in the “New workspace” dialog is improved
NXP Secure Provisioning SDK 1.10.2 is integrated
Version 6.0, March 2023#
Added KW45xx and K32W1xx processors
Enabled support of the LPC55S36 processor
Fixed configuration of boot device Macronix_MX25UM51345G_A.json, so it matches recommendations from reference manuals
LPC55Sxx: DICE can be enabled by the user, UDS key initialized in the write script
LPC55Sxx and i.MX RTxxx: It is possible to regenerate ROT certificates with a different serial number (for key revocation)
LPC55Sxx: The CFPA content is verified before write and an error is reported if the version is not incremented (GUI only)
LPC55Sxx: Added support for encrypted plain boot type
Added i.MX RT1040 processor
i.MX RT1060: a new EVK board revision supported: MIMXRT1060-EVKC
i.MX RT107x: a new EVK board revision supported: RT1170-EVKB
i.MX R685: a new EVK board supported: RT600-AUD-EVK
i.MX RT5xx: Added support for dual image (ping/pong) boot with PUF key source
i.MX RT5xx and RT6xx: Added support eMMC and SD card
i.MX RT6xx: Added support for debug authentication
Trust provisioning: added support for multiple smart cards, USB connection, and performance improvements
Flash programmer performance improvements for higher buffer sizes
Build view: displayed all generated files and their status
Window locations and sizes are stored in preferences
The tool display “dirty” flag; if settings are not saved on the disk; added new preference to save automatically
Setting file
spt_settings.jsonchanged tosettings.sptjsonFile extension
.sptjsonassociated with the SEC tool, so it can be opened directly with the toolCLI: New argument in write scripts: erase_all - perform an erase of the entire flash memory instead erasing regions only
Tool localized to Chinese
Legacy blhost updated to v2.6.7
LPC55S69: dropped support of trust provisioning firmware for silicon revision 8
i.MX RT633S: the processor removed, no more supported
Integrated NXP Secure Provisioning SDK 1.9.1
Version 5.0, November 2022#
Added support for LPC55xx and LPC553x processors (non-S)
Added support for main menu > Tools > Flash Programmer
Added support for trust provisioning using Smart Card for LPC55S0x/1x processors
Added support for device HSM provisioning for i.MX RT6xx processors
Added support for dual image (ping/pong) boot for i.MX RTxxx processors with OTP key source
Legacy elftosb is replaced by elftosb from SPSDK for i.MX RTxxx processors
OTP Configuration is moved from the Write image page to the Build image page
write_parameters.jsonis generated for write with parameters reused from build; CLI parameters updatedAdded support for burning fuses in SB file for i.MX RTxxx processors
Added support for debug authentication for LPC55Sxx and i.MX RTxxx processors
Added support for OTFAD encrypted boot mode with master key for i.MX RT1011 processor
Added support for FlexSPI NAND boot for i.MX RT117x/RT116x processors
Added support for localization, Manufacturing Tool is localized to Chinese (see Preferences)
Added “MX25U51245G_B” boot device configuration for i.MX RT600-AUD-EVK
The command “main menu> File > Generate Scripts” is removed, it was replaced by the link on Build image and Write image views
Integrated SPSDK 1.7 with the following highlighted changes:
new tools: nxpimage and nxpcrypto
elftosb: added support to burn fuses in the SB file
Version 4.1.1, July 2022#
Trust provisioning tools are updated from NXP Secure Provisioning SDK 1.6.3
Version 4.1, June 2022#
LPC55S69: 2 versions of trust provisioning firmware for different silicon revisions are now supported.
Ubuntu 22.04 LTS is supported
Version 4.0.1, May 2022#
Windows: Fix for LPC55Sxx write script in sealing the CMPA page
Updated terminology in GUI and documentation
Version 4.0, May 2022#
Added support for Trust Provisioning using Smart Card for LPC55S6x/2x
Added support for “life cycle” selection instead of the “Enable security” checkbox (for all processors)
Added support for Encrypted (HAB) and Encrypted (IEE) boot modes for RT11xx
Added support for FlexSPI instance selection for i.MX RT11xx processors
Added support for OTFAD encrypted boot mode with user keys for i.MX RT1010 processors
Added support for SPI and I2C connection types (for LPC55Sxx and i.MX RTxxx)
Improved fields and bits names in PFC Configuration for LPC55Sxx processors
Improvements on the Manufacturing Tool: Added counter of successful operations and a “Test connection” button
Improved layout of PFR Configuration dialog for improving the user experience on Linux
Several fixes and improvements for write script for i.MX RTxxx processors
Added a “Clear CMPA” button into the PFR configuration dialog
CLI command “clear-security” was removed. It was replaced by the PFR configuration and a “Clear CMPA” button
Windows: Fixed the problem that the Secure Provisioning Tool does not run with some region settings
Integrated SPSDK 1.6 with the following highlighted changes:
Additional CLI tools added: tpconfig, tphost, nxpcertgen, nxpdevhsm, shadowregs, nxpdevscan
blhost:
The performance of the “receive-sb-file” command was significantly improved; however, if it fails, the reported error code might not be correct; use the parameter “–check-errors” to see the detailed problem information
The command “efuse-program-once” automatically verifies the written value to avoid problems on i.MX RT11xx processors, where the write failure was reported as a successful operation (see also –verify/–no-verify option)
pfr, pfrc:
The names of the fields and their bits were updated without preserving backward compatibility.
Version 3.1, August 2021#
Support for Mac OS X Big Sur (version 11) is added; support for Microsoft(R) Windows(R) 7 is dropped.
Support for i.MX RT1171, RT1172, RT1173, RT1175, RT1165, RT1166 is added.
The CLI command “write_fuses” was removed, it was replaced by OTP Configuration.
[LPC55Sxx] Support for PFR Configuration GUI is added.
[LPC55Sxx] Support for PRINCE encryption of “Whole image” without the necessity to enter an exact address range is added.
[RTxxx, RT11xx] support for OTFAD encryption is added.
Support for i.MX RT1010: Unsigned and Authenticated (HAB) modes are added.
NXP Secure Provisioning SDK 1.4 is integrated.
Version 3.0, April 2021#
Support for i.MX RT1176: Unsigned and Signed modes is added.
Support for i.MX RT5xx/RT6xx: Unsigned/CRC/Signed boot modes is added.
Support for PRINCE encryption for LPC55Sxx processors is added.
Support for OTP configuration is added.
Support for Manufacturing Tool is added.
[LPC55Sxx] CMPA/CFPA.bin files generated using the PFR tool; CMPA/CFPA.json used as an input
[LPC55Sxx] The initial version of CFPA for Signed boot mode (0x02000_0000 to 0x0000_0002) is fixed.
i.MX RT10xx/RT11xx: support for restricted data is added.
RT5xx/RT6xx: the ability to use Shadow registers instead of using FUSEs
Support for Ubuntu 20.04 is added.
blhost and sdphost utilities are replaced with SPSDK alternatives; new CLI utilities: pfr, nxpkeygen, and nxpdebugmbox (Debug Authentication) in tools/spsdk are added.
LPC55Sxx Key Store: The key store is initialized only once in the device life cycle and after that SBKEK cannot be changed.
i.MX RT10xx GPx fuse lock: lock for the GPx fuse provided in previous versions was removed in V3 as the lock is not required for a bootable image;
Note: However, it is still recommended to lock the fuse; see “OTP Configuration”
Version 2.1, December 2020#
Support for i.MX RT1015, i.MX RT1024, LPC55S06, and LPC55S04 is added.
Mac OS X - fixed saving the workspace setting in case the App Menu “securep | Quit securep” is used.
Mac OS X - fixed connection dialog freeze in case a wrong UART is used.
[LPC55Sxx] several improvements for Signed LPC images
[LPC55Sxx] CLI allows setting/overriding the Trust Zone Settings.
Other minor improvements and bug-fixes
Version 2.0, August 2020#
Support for i.MX RT1020 and i.MX RT1064 is added.
Support for LPC55S6x, LPC55S2x, and LPC55S1x is added.
Unsigned, Unsigned CRC, and Signed boot modes
TrustZone support (bin + json)
Key Management - Secure Boot, Generation of ROT keys
BEE boot for i.MX RT10xx
OTPMK
SW-GP2/GP4
Import/Export Keys between workspaces
The connection dialog is improved, it supports UART test connection, processor detection and detection of fuse status are improved.
Version 1.0.1, January 2020#
Support for Mac OS X Catalina (10.15) + Ubuntu 18.04 is added.
Termination of subprocesses of long-running tasks is fixed.
Version 1.0, December 2019#
Initial version with i.MX RT1050 and i.MX RT1060; for Windows
Revision history#
Table 1. Revision history
Document ID |
Release date |
Description |
|---|---|---|
MCUXSPTRN v.12 |
30 June 2025 |
Features for 25.06 are added. |
MCUXSPTRN v.11 |
14 April 2025 |
Changes for 25.03.01 are added. |
MCUXSPTRN v.10 |
28 March 2025 |
Features for 25.03 are added. |
MCUXSPTRN v.9 |
13 November 2024 |
Features for v.10 are added. |
MCUXSPTRN v.8 |
19 August 2024 |
Features for v.9.0.1 are added. |
MCUXSPTRN v.7 |
31 July 2024 |
Features for v.9 are added. |
MCUXSPTRN v.6 |
11 January 2024 |
Features for v.8 are added. |
MCUXSPTRN v.5 |
20 July 2023 |
Features for v.7 are added. |
MCUXSPTRN v.4 |
15 March 2023 |
Features for v.6 are added. |
MCUXSPTRN v.3 |
30 September 2022 |
Features for v.5 are added. |
MCUXSPTRN v.2 |
24 June 2022 |
Features for v.4.1 are added. |
MCUXSPTRN v.1 |
10 May 2022 |
Features for v.4.0.1 are added. |
MCUXSPTRN v.0 |
28 April 2022 |
Initial release |