# Generate code

The **Pins** tool generates the output code for current configuration automatically. You can also select **Pins** > **Refresh** from the **Main Menu** to update the code manually. All output code files are displayed in the **Code Preview** view. To copy the code, perform the copy/paste operation or click the **Export** icon in the right up corner of **Code Preview** view.

```{eval-rst}
.. figure:: _images/generate_code.png
   :scale: 70%
   :align: center

   **Generate code**
```

Alternatively, you can also export generated output in various types of output like source files, plain pins configuration data in CSV, modified registers content or as pins configuration report in HTML per specific export wizard selectable from **File** > **Export** from the **Main Menu**.