MCUXpresso SDK Documentation

Creating a Bluetooth LE application when the Host Stack runs on another processor#

This section describes how to create a Bluetooth Low Energy application (host), when the Bluetooth Low Energy Host Stack is running on another processor (blackbox). The section alsp provides sample code to explain how to achieve this.

The supported serial interfaces between the two chips (application and the Bluetooth Low Energy Host Stack) are UART, SPI, or USB.

Typical applications employing Bluetooth LE Host Stack blackboxes are host systems such as a PC tool or an embedded system that has an application implementation. This chapter describes an embedded application.

For more information, refer to Bluetooth Low Energy Host Stack FSCI Reference Manual. This document provides explicit information on exercising the Bluetooth Low Energy Host Stack functionality through a serial communication interface to a host system.

Serial manager and FSCI configuration#

For creating an embedded application that communicates with the Bluetooth Low Energy Host Stack using the serial interface, the following steps must be done:

Serial manager initialization#

The function that must be called for Serial Manager initialization is located in SerialManager.h:

/* Init serial manager */
SerialManager_Init();

Parent topic:Serial manager and FSCI configuration

FSCI configuration and initialization#

By default, the FSCI module is disabled. It must be enabled by setting gFsciIncluded_c to 1. Also, gFsciLenHas2Bytes_c must be set to 1 because Bluetooth Low Energy Host Stack interface commands and events need serial packets bigger than 255 octets.

For more information on the following configuration parameters, refer to the FSCI chapter of the Connectivity Framework Reference Manual.

To configure the FSCI module, the following parameters can be set on both the Bluetooth Low Energy Application project and the Bluetooth Low Energy FSCI blackbox:

/* Enable/Disable FSCI */
#define gFsciIncluded_c                 1

/* Enable/Disable FSCI Low Power Commands*/
#define gFSCI_IncludeLpmCommands_c      0

/* Defines FSCI length - set this to FALSE is FSCI length has 1 byte */
#define gFsciLenHas2Bytes_c             1

/* Defines FSCI maximum payload length */
#define gFsciMaxPayloadLen_c            1660

/* Enable/Disable Ack transmission */
#define gFsciTxAck_c                    0

/* Enable/Disable Ack reception */
#define gFsciRxAck_c                    0

/* Enable FSCI Rx restart with timeout */
#define gFsciRxTimeout_c                1
#define mFsciRxTimeoutUsePolling_c      1

/* Use Misra Compliant version of FSCI module */
#define gFsciUseDedicatedTask_c         1

/* FSCI task size */
#if defined(DEBUG)
#define gFsciTaskStackSize_c            4600
#else
#define gFsciTaskStackSize_c            2600
#endif

To perform the FSCI module initialization, the following code can be used:

/* Define fsci serial manager handle */
  #if defined(gFsciIncluded_c) && (gFsciIncluded_c > 0)
    extern serial_handle_t g_fsciHandleList[gFsciIncluded_c];
  #endif /*gFsciIncluded_c > 0*/

void BluetoothLEHost_AppInit(void)
{
    /* Init FSCI */
    FSCI_commInit( g_fsciHandleList );

    /* Register BLE handlers in FSCI */
    fsciBleRegister(0);
    ...	
}

Parent topic:Serial manager and FSCI configuration

FSCI handlers (GAP, GATT, and GATTDB) registration#

For receiving messages from all the Bluetooth Low Energy Host Stack serial interfacing layers (GAP, GATT, and GATTDB), a function handler must be registered in FSCI for each layer:

fsciBleRegister(0);

Parent topic:Serial manager and FSCI configuration

Parent topic:Creating a Bluetooth LE application when the Host Stack runs on another processor

Bluetooth Low Energy Host Stack initialization#

The Bluetooth Low Energy Host Stack must be initialized when platform setup is complete and all RTOS tasks have been started. This initialization is done by restarting the blackbox using a FSCI CPU Reset Request command. This is performed automatically by the Ble_Initialize(App_GenericCallback) function.

/* Send FSCI CPU reset command to BlackBox */
FSCI_transmitPayload(gFSCI_ReqOpcodeGroup_c, mFsciMsgResetCPUReq_c, NULL, 0, fsciInterface);

The completion of the Bluetooth Low Energy Host Stack initialization is signaled by the reception of the GAP-GenericEventInitializationComplete.Indication event (over the serial communication interface, in FSCI). The Bluetooth Low Energy-HostInitialize.Request command is not required to be sent to the blackbox (the entire initialization is performed by the blackbox, when it resets).

Parent topic:Creating a Bluetooth LE application when the Host Stack runs on another processor

GATT database configuration#

The GATT database always resides on the same processor as the entire Bluetooth Low Energy Host Stack, so the attributes must be added by the host application using the serial communication interface.

To create a GATT database remotely, GATTDBDynamic commands must be used. The GATTDBDynamic API is provided to the user that performs all the required memory allocations and sends the FSCI commands to the blackbox. The result of the operation is returned, including optionally the service, characteristic, and ‘cccd’ handles returned by the blackbox.

Current supported API for adding services is the following:

bleResult_t GattDbDynamic_AddGattService (gattServiceHandles_t* pOutServiceHandles);
bleResult_t GattDbDynamic_AddGapService (gapServiceHandles_t* pOutServiceHandles);
bleResult_t GattDbDynamic_AddIpssService (ipssServiceHandles_t* pOutServiceHandles);
bleResult_t GattDbDynamic_AddHeartRateService (heartRateServiceHandles_t* pOutServiceHandles);
bleResult_t GattDbDynamic_AddBatteryService (batteryServiceHandles_t* pOutServiceHandles);
bleResult_t GattDbDynamic_AddDeviceInformationService (deviceInfoServiceHandles_t* pOutServiceHandles);

The service handles are optional.

Also, a generic function is provided, so that the user can add any generic service to the database:

bleResult_t GattDbDynamic_AddServiceInDatabase (serviceInfo_t* pServiceInfo);

Usually, a Bluetooth Low Energy Application is ported from a single chip solution, where the Bluetooth Low Energy Application and the Bluetooth Low Energy stack reside on the same processor and the GATT database is populated statically. The user should remove all the attribute handles from any structure and replace them with gGattDbInvalidHandle_d. The attribute handles should be populated after the services are added dynamically to the database with the handles returned by the previous API.

Parent topic:Creating a Bluetooth LE application when the Host Stack runs on another processor

FSCI host layer#

The Bluetooth Low Energy GAP, GATT, GATTDB, and L2CAP APIs are included in the Bluetooth Low Energy interface. When these APIs reside on a separate processor than the Bluetooth Low Energy stack, they are implemented as an FSCI Host Layer that should be added to the Bluetooth Low Energy Application project.

This layer is responsible for serializing API to the corresponding FSCI commands. The layer also sends these APIs to the blackbox, receives and deserializes FSCI statuses and events, presents them to the Bluetooth Low Energy Application, and arbitrates access from multiple tasks to the serial interface.

All the GAP, GATT, GATTDB, and L2CAP APIs are executed asynchronously, so the user context blocks waiting for the response from the blackbox. The response can be the status of the request or optionally an FSCI event, which includes the output parameters of a synchronous function.

There are also functions without parameters that are not executed synchronously and they are provided asynchronously through a later FSCI event. It is the responsibility of the FSCI Host layer to keep the application-allocated memory between the time of the request and the completion of the event with the actual values of the output parameters and populate them accordingly.

The Bluetooth Low Energy API execution inside the FSCI Host layer first waits for gaining access to the serial interface through a mutex. Once the access is gained, the FSCI request is sent to the serial interface to the blackbox. Then, by default, the serial interface response is received by polling until the whole FSCI packet is received. The other option available is to block the user task to wait for an OS event that is set by the FSCI module when the status is received. For more information on the FSCI module, see the Connectivity Framework Reference Manual. See References.

The API can have output parameters that are to be received immediately after the status of the request. In such as case, if the status of the request is ‘success’, the polling mechanism continues to receive the whole FSCI packet of the Bluetooth Low Energy event. The output parameters are obtained and the values are filled in the memory space provided by the application. After obtaining the status and optionally the event, the execution of the request is considered completed, the mutex to the serial interface is unlocked, and the execution flow is returned to the user calling context.

Parent topic:Creating a Bluetooth LE application when the Host Stack runs on another processor