i.MX RT bootable image#
Bootable image layout in target flash device#
There are two types of supported boot image:
XIP (Execute-In-Place) boot image: This type of boot image is only applicable to Serial NOR devices connected to QuadSPI or FlexSPI interfaces. The boot device memory is identical to the destination memory. ROM can boot this boot image directly.
Non-XIP boot image: The boot device memory is different from the destination memory. ROM loads the boot image from the boot device memory to the destination memory and then boots from the destination memory.
Bootable image layout

Boot image format#
This section describes the boot image format and data structures. The elftosb utility helps the customers automatically generate the boot image format file. The elftosb utility usage is described later in this document.
The bootable image must have the following data structures:
Image Vector Table (IVT): a list of pointers located at a fixed address that ROM examines to determine the location of other components of the bootable image
Boot Data: a table that indicates the bootable image location, image size in bytes, and the plugin flag
User application and data
CSF (optional): signature block for Secure Boot generated by CST
Each bootable image starts with appropriate IVT. In general, for the external memory devices that support XIP feature, the IVT offset is 0x1000 else it is 0x400.
IVT and boot data#
The IVT is the data structure that the BootROM reads from the boot devices. This data structure supplies the bootable image containing the required data components to perform a successful boot.
See the Program image section in the System Boot chapter of the device reference manual for more details.
IVT data structure
Offset |
Field |
Description |
|---|---|---|
0x00 - 0x03 |
header |
• Byte 0 tag, fixed to 0xD1 |
0x04 - 0x07 |
entry |
Absolute address of the first instruction to execute from the image, or the vector address of the image |
0x08 - 0x0b |
reserved1 |
Reserved for future use, set to 0 |
0x0c - 0x0f |
dcd |
Absolute address of the image, set to NULL as DCDDCD is not supported on RT1010 |
0x10 - 0x13 |
boot_data |
Absolute address of the boot data |
0x14 - 0x17 |
self |
Absolute address of the IVT |
0x18 - 0x1b |
csf |
Absolute address of the Command Sequence File (CSF) used by the HAB library |
0x1c - 0x1f |
reserved2 |
Reserved, set to 0 |
Boot data structure#
Boot Data structure
Offset |
Field |
Description |
|---|---|---|
0x00-0x03 |
start |
Absolute address of the bootable image |
0x04-0x07 |
length |
Size of the bootable image |
0x08-0x0b |
plugin |
Plugin flag, set to 0 because plugin boot is not supported on the RT1010 |
Signed image#
The bootable image can be signed by CST tool. The tool generates the CSF data in the binary file format that consists of command sequences and signatures based on given input command sequence file (csf file). Refer to the documentation in the CST release package for further details.
In this document, a simple method is introduced to generate signed images using the elftosb utility.
Encrypted image#
RT1010 supports only the encrypted XIP image format.
The encrypted XIP image is generated using the AES-CTR algorithm. In different scenarios, the image can be generated on-chip or with an external tool. Upon execution, the hardware engine does the decryption on the programmed image.