Hardware requirements#
Micro USB cable
RD-RW612-BGA board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
DMA memory to memory transfer example begin.
Destination Buffer:
0 0 0 0
DMA memory to memory transfer example finish.
Destination Buffer:
1 2 3 4