Hardware requirements#
Micro USB cable
MIMXRT685-AUD-EVK board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
NOTE: Depending on the toolchain configuration, the benchmark result might be different.
CMSIS DSP benchmark filter test start.
arm_fir_q15Test: xxx
arm_fir_q31Test: xxx
arm_fir_f32Test: xxx
arm_conv_q15Test: xxx
arm_conv_q31Test: xxx
arm_conv_f32Test: xxx
arm_correlate_q15Test: xxx
arm_correlate_q31Test: xxx
arm_correlate_f32Test: xxx
biquad_cascade_f32Test: xxx
CMSIS DSP benchmark filter test succeeded.