MCUXpresso SDK Documentation

Hardware requirements#

  • Type-C USB cable

  • MCXW72-LOC Board

  • Personal Computer

Board settings#

Using instance 0 of LPUART interface to transfer data to itself. TX pin is connected with RX pin.

LPUART0     CONNECTS TO         LPUART0
Pin Name    Board Location      Pin Name  Board Location
RXD         J2-3                TXD       J2-4

Prepare the Demo#

  1. Connect a USB cable between the PC host and the OpenSDA USB port on the board.

  2. Open a serial terminal on PC for OpenSDA serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Reset the SoC and run the project.

Running the demo#

When the demo runs successfully, the log would be seen on the OpenSDA terminal like:

LPUART 9-bit mode example begins
LPUART is configured with address, only data sent to itself after matched address can be received
LPUART will send first piece of data out:

0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f

LPUART will address itself
LPUART will send the other piece of data out:

0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f

LPUART received data:

0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f

All data matches!