Hardware requirements#
USB Type-C cable
MCIMX93-EVK board
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the example runs successfully, you can see the similar information from the terminal as below.
EDMA scatter_gather example begin.
Destination Buffer:
0 0 0 0 0 0 0 0
EDMA scatter_gather example finish.
Destination Buffer:
1 2 3 4 5 6 7 8