Hardware requirements#
2 x Micro USB cable
MC56F81000-EVK board
Personal Computer
Board hardware common setting#
Power setting:
Connect J8 pin2 and pin3 Connect J5 pin1 and pin2 Connect J6 pin1 and pin2
Onboard PnE U-MultiLink debugger setting:
Connet J11 pin2 and pin3 Connect J13 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger PnE U-MultiLink. Note: when use external debugger(connected to J10), leave all J13 pins open.
Board settings#
No special settings are required.
Note: The sample0 works in fully differential mode and the differential pair is selected as ANA6 and ANA7. And the thermistor in MC56F81000-EVK board is connected to ANA6 and ANA7.
Prepare the Demo#
Connect USB cable between the host PC and the USB(J26) port on the target board to setup USB to UART bridge.
Connect USB cable between the host PC and the USB(J12) port on the target baord to setup mulitlink debugger.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board with PnE U-MultiLink debug configuration.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo. Please be noted default FCF(flash configuration field) makes the MCU boot from flash.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
CADC continuous edma conversion.
Press any key to get user channel's ADC value ...
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
User can press any key to get more converter data. The ADC input channel is connected with thermistor, so touching thermistor on board will get the ADC value updated.