Hardware requirements#
Micro USB cable
LPCXpresso54628 board
Personal Computer
RK043FN02H-CT or RK043FN66HS-CT6 LCD board
Board settings#
No special board settings.
Prepare the Demo#
Connect a micro USB cable between the PC host and the LPC-Link USB port (J8) on the board.
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
There is a cursor moves in the panel if the example runs successfully.