Hardware requirements#
FRDMMCXE31B board
FRDM-MC-LVPMSM board
Power supply 24V
Mini/micro USB cable
Low-voltage 3-phase permanent magnet motor
Personal Computer
Overview#
The 3-phase permanent magnet synchronous motor (PMSM) control reference application is intended to provide the example for 3-phase PMSM motor control solutions. The reference design uses a closed-loop field-oriented vector speed (FOC) control mechanism.
More information#
Application web page with the board specific Application User’s guide and other documentation: http://www.nxp.com/sdkmotorcontrol
Board settings#
Follow chapter “Hardware setup” in Application User’s guide.
In this example, the LCU is used as a PWM output, therefore some additional wiring is required. Please connect the FRDM-MC-LVPMSM to the FRDM-MCXE31B, and then connect the LCU outputs on J8 to the Freedom board using wires.
FRDM-MC-LVPMSM FRDM-MCXE31B J3-15 (PWM_AT) with J8-9 (PTB1) J3-13 (PWM_AB) with J8-11 (PTB0) J3-11 (PWM_BT) with J8-6 (PTC9) J3-9 (PWM_BB) with J8-8 (PTC8) J3-7 (PWM_CT) with J8-10 (PTC11) J3-5 (PWM_CB) with J8-12 (PTC10)
Running the demo#
Follow chapter “User interface” in Application User’s guide.