Hardware requirements#
Type-C USB cable
FRDM-MCXC444 board
Personal Computer
Board settings#
No special is needed.
Prepare the Demo#
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
LPUART DMA example
Send back received data
Echo every 8 characters