MCUXpresso SDK Documentation

Hardware requirements#

  • FRDMMCXA266 board

  • FRDM-MC-LVPMSM board

  • Power supply 24V

  • Mini/micro USB cable

  • Low-voltage 3-phase permanent magnet motor

  • Personal Computer

Overview#

The 3-phase permanent magnet synchronous motor (PMSM) control reference application is intended to provide the example for 3-phase PMSM motor control solutions. The reference design uses a closed-loop field-oriented vector speed (FOC) control mechanism.

More information#

Application web page with the board specific Application User’s guide and other documentation: http://www.nxp.com/sdkmotorcontrol

Board settings#

Route the over-current fault signal by connection CMP0_IN1(P1_3, J2-17) with the MC1_CUR_DCB (P2_4, J2-9). Follow chapter “Hardware setup” in Application User’s guide for more information.

Running the demo#

Follow chapter “User interface” in Application User’s guide.