Hardware requirements#
Type-C USB cable
FRDM-MCXA156 Board
Personal Computer
Board settings Positive input channel J2-12(P2_12, OPAMP0_INP0) connects to GND. Negative input channel J2_8(P2_13, OPAMP0_INN) connects to GND. OPAMP output pin: J8-5(P2_15). Note that on the FRDM-MCXA156 board, the resistor R60 is connected as A-type by default, for running this example, the resistor R60 needs to connect as B-type, which enables the OPAMP0_INN to connect to the J2_8. If the user doesn’t want to rework the board, the user also can connect R60-3 to the GND directly.
Prepare the Demo#
Connect a micro USB cable between the PC host and the MCU-Link USB port on the board
Open a serial terminal with the following settings (See Appendix A in the Getting Started guide for the description of how to determine the serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
OPAMP DAC LPADC EXAMPLE. Please input a value (0 - 4095) for DAC, press the entry button to indicate the end of input:400 Input DAC value is 400 The current DAC output is about 322.400 mV Please select OPAMP negative port gain from the following options. Input 0 means select 1x. Input 1 means select 2x. Input 2 means select 4x. Input 3 means select 8x. Input 4 means select 16x. Input 5 means select 33x. Input 6 means select 64x. 3 Input OPAMP negative port gain is 8x Please press any key excluding key (R or r) to get the user channel’s ADC value. Vsw1 ADC value: 1805 Actual voltage on Vsw1: 1.454V Vpref ADC value: 1807 Actual voltage on Vpref: 1.456V
Please input a value (0 - 4095) for DAC, press the entry button to indicate the end of input:500 Input DAC value is 500 The current DAC output is about 403.000 mV Please select OPAMP negative port gain from the following options. Input 0 means select 1x. Input 1 means select 2x. Input 2 means select 4x. Input 3 means select 8x. Input 4 means select 16x. Input 5 means select 33x. Input 6 means select 64x. 1 Input OPAMP negative port gain is 2x Please press any key excluding key (R or r) to get the user channel’s ADC value. Vsw1 ADC value: 752 Actual voltage on Vsw1: 0.606V Vpref ADC value: 751 Actual voltage on Vpref: 0.605V