Hardware requirements#
Mini USB cable
FRDM-K32L2A4S board
Personal Computer
Board settings#
Using instance 2 of LPUART interface to transfer data to itself. TX pin is connected with RX pin.
LPUART2 CONNECTS TO LPUART2
Pin Name Board Location Pin Name Board Location
TXD J4-5 RXD J4-7
Prepare the Demo#
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo#
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
LPUART 9-bit mode example begins
LPUART is configured with address, only data sent to itself after matched address can be received
LPUART will send first piece of data out:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
LPUART will address itself
LPUART will send the other piece of data out:
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
LPUART received data:
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
All data matches!