Hardware requirements#
Micro USB cable
EVK-MIMXRT685 board
Personal Computer
Board settings#
Prepare the Demo#
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
NOTE: Depending on the toolchain configuration, the benchmark result might be different.
CMSIS DSP benchmark matrix test start.
arm_mat_add_q15Test: xxx
arm_mat_add_q31Test: xxx
arm_mat_add_f32Test: xxx
arm_mat_sub_q15Test: xxx
arm_mat_sub_q31Test: xxx
arm_mat_sub_f32Test: xxx
arm_mat_mult_q15Test: xxx
arm_mat_mult_q31Test: xxx
arm_mat_mult_f32Test: xxx
arm_mat_inverse_f32Test: xxx
arm_mat_trans_q15Test: xxx
arm_mat_trans_q31Test: xxx
arm_mat_trans_f32Test: xxx
arm_mat_scale_q15Test: xxx
arm_mat_scale_q31Test: xxx
arm_mat_scale_f32Test: xxx
CMSIS DSP benchmark matrix test succeeded.