MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • EVK-MIMXRT685 board

  • Personal Computer

Board settings#

Prepare the Demo#

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo#

NOTE: Depending on the toolchain configuration, the benchmark result might be different.

CMSIS DSP benchmark filter test start.
arm_fir_q15Test: xxx
arm_fir_q31Test: xxx
arm_fir_f32Test: xxx
arm_conv_q15Test: xxx
arm_conv_q31Test: xxx
arm_conv_f32Test: xxx
arm_correlate_q15Test: xxx
arm_correlate_q31Test: xxx
arm_correlate_f32Test: xxx
biquad_cascade_f32Test: xxx

CMSIS DSP benchmark filter test succeeded.