MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • MIMX8ULP-EVK/EVK9 board

  • J-Link Debug Probe

  • 5V power supply

  • Personal Computer

  • Oscilloscope

Board settings#

CM33: Connect J11-3 and J11-5(GND) to Oscilloscope

Prepare the Demo#

  1. Connect 5V power supply and J-Link Debug Probe to the board, switch SW10 to power on the board.

  2. Connect a micro USB cable between the host PC and the J17 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Running the demo#

When the example runs successfully, the following message is displayed in the terminal:

TPM example to output combined complementary PWM signals on two channels

If an LED is connected to the TPM pin, you will see a change in LED brightness if you enter different values
If no LED is connected to the TPM pin, then probe the signal using an oscilloscope
Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value:5
The duty cycle was successfully updated!

Please enter a value to update the Duty cycle:
Note: The range of value is 1 to 9.
For example: If enter '5', the duty cycle will be set to 50 percent.
Value: