Hardware requirements#
Micro USB cable
EVK-MIMX8M Plus board
J-Link Debug Probe
12V power supply
Personal Computer
Board settings#
No special settings are required.
Prepare the Demo#
Connect 12V power supply and J-Link Debug Probe to the board, switch SW3 to power on the board
Connect a USB cable between the host PC and the J23 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo#
Set any baud rate in your terminal, and send character a or A to board, then
When the demo runs successfully, the log would be seen on the debug terminal like:
UART has detect one character A
Baud rate has been set automatic!
Board will send back received characters