Hardware requirements#
Mini/micro USB cable
MIMXRT1170-EVKB board
Personal Computer
Two SPDIF RCA lines
Soundcacrd support SPDIF interface
Board settings#
1.Make sure J35,J36,J37,J45,J46,T1 and T2 are installed. Weld 10kΩ resistor to R295. 2.Remove R188, R203, R209 and R835.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Connect J46 with SPDIF soundcard output inteface, connect J45 with SPDIF soundcard input interface.
Playback music using the SPDIF soundcard, make the SPDIF signals input to MIMXRT1170 board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
After run the demo, you can hear the music playbacked from SPDIF soundcacrd, the log below shows the output of the example in the terminal window:
SPDIF EDMA example started!
SPDIF EDMA example finished!
Known issues#
==============
When running a flash target of the demo, it gets blocked after printing the “SPDIF EDMA example started!”.