Hardware requirements#
Mini/micro USB cable
MIMXRT1170-EVKB board
Personal Computer
Board settings#
Using instance 7 of LPUART interface to transfer data to itself. TX pin is connected with RX pin.
LPUART7 CONNECTS TO LPUART7
Pin Name Board Location Pin Name Board Location
TXD J9-14 RXD J10-4
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
LPUART 9-bit mode example begins
LPUART is configured with address, only data sent to itself after matched address can be received
LPUART will send first piece of data out:
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
LPUART will address itself
LPUART will send the other piece of data out:
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
LPUART received data:
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
All data matches!