MCUXpresso SDK Documentation

dev_cdc_vnic#

Overview#

The Virtual NIC project is a simple demonstration program based on the MCUXpresso SDK. It is enumerated as a network adapter. Users can access the network by properly configuring this network adapter. The purpose of this demo is to show how to build a device of USB CDC class to implement RNDIS protocol and to provide a simple project for further development.

System Requirement#

Hardware requirements#

  • Mini/micro USB cable

  • USB A to micro AB cable

  • Hardware (Tower module/base board, and so on) for a specific device

  • Personal Computer

Software requirements#

  • The project files are in:
    <MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_cdc_vnic//.
    For lite version, the project files are in:
    <MCUXpresso_SDK_Install>/boards//usb_examples/usb_device_cdc_vnic_lite//.

The is Bare Metal or FreeRTOS OS.

Getting Started#

Hardware Settings#

Set the hardware jumpers (Tower system/base module) to default settings.

Prepare the example#

  1. Download the program to the target board.

  2. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

  3. Plug in the network cable before running this example. (Or you may have to disable and then enable the RNDIS network adapter after you plug in the network cable.)

  4. Connect the USB device port on the board to the host PC and the using a USB cable.

For detailed instructions, see the appropriate board User’s Guide.
Duo to the speed missmatch between usb and enet, some enet frame will be discard when lots of data are received in short time, this issue is obvious, especially on Full speed usb.
The upper layer protocol will handle this issue, such as TCP/IP protocol.
Based on the test on TWR-K65,add the buffer number to receive enet frame data could reduce the discard frame, user may add the buffer number if ram is enough.

Run the example in Windows®#

  1. A network adapter is enumerated in Device Manager.
    Virtual NIC in device manager

On Windows 10, the device would be identified as an virtual com for the first time.
Virtual com in device manager on Windows 10

  1. In Control Panel\Network and Internet\Network Connections, the RNDIS network adapter is listed as below.
    Virtual NIC in Network Connections

  2. Connect the ethernet port to another test PC using a network cable. The IP address of this test PC can be configured as 192.168.1.102.
    Test PC NIC configuration

  3. Then configure the RNDIS adapter in Windows for your host PC. For this testing example, please make sure your PC host and the test PC are in the same network segment. E.g
    Host PC Virtual NIC configuration

  4. Then you are supposed to access the test PC through this USB RNDIS network adapter from your host PC
    Ping to other PC

Note#

  1. The VNIC CIC CLASS code can be changed to be miscellaneous device to implement that there is no need to install inf file by changing the codes for descriptor. Provide the following codes macros for descriptor to change its related codes:
    #define USB_CDC_IFACE_DESCRIPTOR_VNIC_CIC_CLASS (0xEF)
    #define USB_CDC_IFACE_DESCRIPTOR_VNIC_CIC_SUBCLASS (0x04)
    #define USB_CDC_IFACE_DESCRIPTOR_VNIC_CIC_PROTOCOL (0x01)
    Note that the above change is only applied for descriptor, please do not change the codes of class driver. This is not verified under all conditions, so please be cautious to change.

Installing the RNDIS driver for virtual_nic example#

Below are the steps to install the RNDIS driver on Windows 7. Similar steps apply for Windows XP.

Step 1. Click “Update Driver Software…”


Step 2. Choose “Browse…”


Step 3. Select “Let me pick…”


Step 4. Navigate to your RNDIS driver location.

<install_dir>\boards\\usb_examples\usb_device_cdc_vnic\inf

or

<install_dir>\boards\\usb_examples\usb_device_cdc_vnic_lite\inf


Step 5. Press “Next”.


Step 6. Ignore the warning and press “Yes”.


Step 7. Now the RNDIS driver should be installed successfully.


*/

Supported Boards#

MCX-N5XX-EVK
Getting Started
Hardware Settings
  • Connect JP13 2-3. Populate R274 to sync reference clock.

MCX-N9XX-EVK
Getting Started
Hardware Settings
  • Connect JP13 2-3. Populate R274 to sync reference clock.

FRDM-IMXRT1186
Getting Started
Hardware Settings

J12(1-2)/J13(2-3): ETH0 Function Via J56A.

MIMXRT1160-EVK
Getting Started
Hardware Settings
  • Please use the Ethernet RJ45 port(J3).

FRDM-MCXA577
Getting Started
Hardware requirements
  • Type-C USB cable (MCU-Link port, for download)

  • Type-C USB cable (USB device port, for the RNDIS network adapter)

  • RJ45 network cable

  • External USB-to-UART module (for the debug console, see the note below)

  • FRDM-MCXA577 board

  • Personal Computer

Hardware Settings

FRDM-MCXA577 A0 silicon has an ENET RMII receive issue (ERR053383), so this example drives the on-board LAN8741 PHY over MII instead of RMII. MII needs more pins than RMII, so an SCH rev B board requires the following ENET solder-jumper rework before Ethernet works:

Solder jumper

Signal

Setting

SJ13

ENET0_TXD2

disconnect 1-2, short 2-3

SJ14

ENET0_TXD3

disconnect 1-2, short 2-3

SJ16

ENET0_RXD2

disconnect 1-2, short 2-3

SJ17

ENET0_RXD3

disconnect 1-2, short 2-3

SJ18

ENET0_COL

disconnect 1-2, short 2-3

SJ19

ENET0_CRS

disconnect 1-2, short 2-3

SJ15

ENET0_RX_CLK

disconnect both 1-2 and 2-3

SJ44

ENET0_RXER

disconnect both 1-2 and 2-3

The rework applies to the external 100BASE-TX PHY path only. It is not needed for the internal 10BASE-T1S digital PHY.

Note: In this MII configuration the ENET TX bus uses P1_8/P1_9, which are the same pins as the MCU-Link VCOM debug console (LPUART1). This example therefore routes its debug console to LPUART2 on the Arduino header (D1/TX = P2_10, D0/RX = P2_11) instead of the VCOM port. Connect an external USB-to-UART module to those Arduino-header pins (module RX to D1/P2_10, module TX to D0/P2_11, GND to GND) and open the serial terminal on that module’s COM port.

Prepare the example
  1. Rework the board as described above.

  2. Connect an external USB-to-UART module to the Arduino header and open a serial terminal on its COM port with 115200 baud rate, 8 data bits, no parity, one stop bit and no flow control.

  3. Connect a Type-C USB cable between the host PC and the MCU-Link USB port on the target board, then download the program.

  4. Insert an RJ45 network cable into the Ethernet port before running the example.

  5. Connect a Type-C USB cable between the host PC and the USB device port on the target board.

  6. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.