MCUXpresso SDK Release Notes
Overview
The MCUXpresso SDK is a comprehensive software enablement package designed to simplify and accelerate application development with Arm Cortex-M-based devices from NXP, including its general purpose, crossover and Bluetooth-enabled MCUs. MCUXpresso SW and Tools for DSC further extends the SDK support to current 32-bit Digital Signal Controllers. The MCUXpresso SDK includes production-grade software with integrated RTOS (optional), integrated enabling software technologies (stacks and middleware), reference software, and more.
In addition to working seamlessly with the MCUXpresso IDE, the MCUXpresso SDK also supports and provides example projects for various toolchains. The Development tools chapter in the associated Release Notes provides details about toolchain support for your board. Support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.
Underscoring our commitment to high quality, the MCUXpresso SDK is MISRA compliant and checked with Coverity static analysis tools. For details on MCUXpresso SDK, see MCUXpresso-SDK: Software Development Kit for MCUXpresso.
MCUXpresso SDK
As part of the MCUXpresso software and tools, MCUXpresso SDK is the evolution of Kinetis SDK, includes support for LPC, DSC,PN76, and i.MX System-on-Chip (SoC). The same drivers, APIs, and middleware are still available with support for Kinetis, LPC, DSC, and i.MX silicon. The MCUXpresso SDK adds support for the MCUXpresso IDE, an Eclipse-based toolchain that works with all MCUXpresso SDKs. Easily import your SDK into the new toolchain to access to all of the available components, examples, and demos for your target silicon. In addition to the MCUXpresso IDE, support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.
In order to maintain compatibility with legacy Freescale code, the filenames and source code in MCUXpresso SDK containing the legacy Freescale prefix FSL has been left as is. The FSL prefix has been redefined as the NXP Foundation Software Library.
Development tools
The MCUXpresso SDK was tested with following development tools. Same versions or above are recommended.
IAR Embedded Workbench for Arm, version is 9.60.4
MCUXpresso IDE, Rev. 25.06.xx
MCUXpresso for VS Code v25.09
GCC Arm Embedded Toolchain 14.2.x
Supported development systems
This release supports board and devices listed in following table. The board and devices in bold were tested in this release.
Development boards |
MCU devices |
|---|---|
KW47-EVK |
KW47B42Z83AFTA, KW47B42Z96AFTA, KW47B42Z97AFTA, |
MCUXpresso SDK release package
The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.
Device support
The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.
Board support
The boards folder provides the board-specific demo applications, driver examples, and middleware examples.
Demo application and other examples
The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.
RTOS
FreeRTOS
Real-time operating system for microcontrollers from Amazon
Middleware
GenFSK link layer
The Generic FSK protocol enables radio operation using a custom GFSK/GMSK or MSK modulation format.
Main Features supported:
Highly configurable packet structure
Optimized Sequence Command Set
High-precision timebase to maintain network timing
Two timer-compare mechanisms for Interrupt Generation and Sequence Launching
Hardware automation for packet transmit and receive, CRC and Whitening
Up to four network addresses to synchronize to, can be 8-bit, 16-bit or 32-bit
Packet Lengths up to 2047 Bytes
Support complex auto-sequence, like CCA before TX, Auto-ACK, TR.
Many operating modes can support the sending and receiving of multiple protocol packets, such as Bluetooth LE.
Wireless XCVR
The XCVR component provides a base Transceiver Driver for the 2.4 GHz narrowband radio.
Bluetooth LE Controller
Main features supported:
Peripheral Role
Central Role
Multiple PHYs (1 Mbps, 2 Mbps, Coded PHY)
Asymmetric Connections
Public/Random/Static Addresses
Network/Device Privacy Modes
Extended Advertising
Extended Scanning
Passive/Active Scanning
LE Encryption
LE Ping Procedure
HCI Test Interface
UART Test Interface
Randomized Advertising Channel Indexing
Sleep Clock Accuracy Update - Mechanism
ADI Field in Scan Response Data
HCI Support for Debug Keys in LE - Secure Connections
Main capabilities supported:
Simultaneous scanning 1 Mbps and Long Range
Scanning and advertising in parallel
24 connections as a central role
24 connections as a peripheral role
Any combination of central and peripheral roles (24 connections maximum)
8 connections with a 7.5 ms connection interval
Two advertising sets in parallel (\Four adv set as Early Access Release).
26 Accept List entries
36 Resolvable Private Address (RPA) entries
Up to two Chain Packets per Extended Advertising set
Enhanced Notification on end of - Scanning/Advertising/Connection events
Connection event counters associated to Bluetooth LE packet reception
Timestamp associated to Bluetooth LE packet reception
RF channel info associated to Bluetooth LE packet reception
NXP proprietary Bluetooth LE Handover feature
Decision Based Advertising Filtering (DBAF)
Advertising Coding Selection (ACS)
Periodic Advertising with Responses (PAwR) Additional features supported for KW47 and MCX W72 devices:
Channel Sounding Additional features supported as EAR (\Early Access Release) in the experimental builds:
Unified Test Protocol (\UTP).
LL Extended Feature Set.
Monitoring Advertisers.
Note: Project configuration enabling Experimental features on KW45 and MCX W71 requires the Radio Subsystem (NBU) Firmware to be reprogrammed with the firmware provided in the SDK under \middleware\wireless\ble_controller\bin\experimental\. For NBU programming steps, see the EVK Quick Start Guide and Secure Provisioning SDK (SPSDK) documentation.
Project configurations that require usage of the Bluetooth LE controller including all Bluetooth LE examples require the Radio Subsystem (NBU) Firmware to be re-programmed with the firmware provided in the SDK under middleware\wireless\ble_controller\bin.
Wireless Bluetooth LE host stack and applications
The Bluetooth LE Host Stack component provides an implementation for a Bluetooth LE mandatory and some optional, proprietary, and experimental features. The Bluetooth LE Host Stack component provides application examples, services, and profiles.
Main features supported:
Automotive Compliance
MISRA Compliance
HIS CCM <= 20
Advanced Secure Mode
Enhanced ATT
GATT Caching
Bluetooth LE Host GCC Libraries
Bluetooth LE Host IAR Libraries
Bluetooth LE Host Peripheral Libraries
Bluetooth LE Central Libraries
Bluetooth LE Host Full Host Features Libraries
Bluetooth LE Host Optional Features Libraries
Bluetooth LE Host Mandatory Features Libraries
Bare-metal and FreeRTOS Support
Bluetooth LE Privacy Support
CCC Sample Applications
Enhanced Notifications
Dynamic Database
OTA Support - Sample Applications
Decision based Advertising Filtering (DBAF) - Experimental feature
Advertising Coding Selection (ACS) - Experimental feature
Channel Sounding - Experimental feature with controlled access (contact your NXP representative for access)
Bluetooth LE Controller main and experimental features and capabilities described below are supported by the Bluetooth LE Host.
Note: For evaluating DBAF and ACS experimental features, replace the Bluetooth LE Host default example projects libraries with the libraries from the SDK folder ..\middleware\wireless\bluetooth\host\lib_exp and enable the features in the application. The Radio Subsystem (NBU) Firmware with experimental features is required.
Wireless Localization
Localization
Wireless Connectivity Framework
The Connectivity Framework is a software component that provides hardware abstraction modules to the upper layer connectivity stacks and components. It also provides a list of services and APIs, such as, Low power, Over the Air (OTA) Firmware update, File System, Security, Sensors, Serial Connectivity Interface (FSCI), and others. The Connectivity Framework modules are located in the middleware\wireless\framework SDK folder.
CMSIS DSP Library
The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.
TF-M
Trusted Firmware - M Library
PSA Test Suite
Arm Platform Security Architecture Test Suite
NXP PSA CRYPTO DRIVER
PSA crypto driver for crypto library integration via driver wrappers
EdgeLock SE050 Plug and Trust Middleware
Secure subsystem library - SSS APIs
Multicore
Multicore Software Development Kit
mbedTLS
mbedtls SSL/TLS library v3.x
mbedTLS
mbedtls SSL/TLS library v2.x
LittleFS
LittleFS filesystem stack
LIN Stack
LIN Stack middleware
FreeMASTER
FreeMASTER communication driver for 32-bit platforms.
Release contents
Provides an overview of the MCUXpresso SDK release package contents and locations.
Deliverable |
Location |
|---|---|
Boards |
INSTALL_DIR/boards |
Demo Applications |
INSTALL_DIR/boards/<board_name>/demo_apps |
Driver Examples |
INSTALL_DIR/boards/<board_name>/driver_examples |
eIQ examples |
INSTALL_DIR/boards/<board_name>/eiq_examples |
Board Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/boards/<board_name>/project_template |
Driver, SoC header files, extension header files and feature header files, utilities |
INSTALL_DIR/devices/<device_name> |
CMSIS drivers |
INSTALL_DIR/devices/<device_name>/cmsis_drivers |
Peripheral drivers |
INSTALL_DIR/devices/<device_name>/drivers |
Toolchain linker files and startup code |
INSTALL_DIR/devices/<device_name>/<toolchain_name> |
Utilities such as debug console |
INSTALL_DIR/devices/<device_name>/utilities |
Device Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/devices/<device_name>/project_template |
CMSIS Arm Cortex-M header files, DSP library source |
INSTALL_DIR/CMSIS |
Components and board device drivers |
INSTALL_DIR/components |
RTOS |
INSTALL_DIR/rtos |
Release Notes, Getting Started Document and other documents |
INSTALL_DIR/docs |
Tools such as shared cmake files |
INSTALL_DIR/tools |
Middleware |
INSTALL_DIR/middleware |
What is new
The following changes have been implemented compared to the previous SDK release version (25.09.00).
Bluetooth LE Host Stack and Applications
Added
Gap_LoadCustomBondedDeviceInformation API to retrieve custom peer information using NVM index.
Improved
Miscellaneous application updates.
Fixed
Updated privacy timeout mechanism affected by the LE Set Extended Advertising Enable Command.
Changed
Merged Gap_SetPeriodicAdvParameters and Gap_SetPeriodicAdvParametersV2 into Gap_SetPeriodicAdvParameters.
Details can be found in github repository nxp-mcuxpresso/mcuxsdk-middleware-bluetooth-host/CHANGELOG.md.
Bluetooth LE controller
Channel sounding updates:
Fixed the RF-PHY receiver testcases (RF-PHY/RCV-LE/CA/BV-7-C, RF-PHY/RCV-LE/CA/BV-13-C, RF-PHY/RCV-LE/CA/BV-30-C, RF-PHY/RCV-LE/CA/BV-31-C).
Fix provided to set bit in pHadmConn->uiFlags for rxed LL_CS_CAPABILITIES_REQ/RSP, allow multiple LE CS Write Cached Remote Supported Capabilities.
RTT bias compensation : Updated software to align with Chip IFR version 2.5
PAwR/PAST updates:
Fixed multiple responses formatting in the Periodic Advertising Responses report.
Fixed the double message allocation causing a memory leak.
DBAF update:
Fixed case where sometimes AUX_ADV_IND with LE Coded Phy was not scheduled.
Fixed handling of duplicate Connection Request using different Peer RPA (LL/SEC/ADV/BI-01-C & LL/SEC/INI/BI-01-C conformance tests).
Fixed the missing chained packet TX when coded PHY is used on multiple Advertising sets and the Advertising interval is small (LL/DDI/ADV/BV-30-C conformance test).
Fixed issue with packet time restrictions after PHY update (packet payload too long). This fixes the LL/CON/PER/BV-53-C, LL/CON/PER/BV-56-C and LL/CON/PER/BV-59-C conformance tests.
Fixed case where address resolution was stuck.
Transceiver drivers (XCVR)
Added support for Bluetooth LE Channel Sounding.
Added API to control PA ramp type and duration.
Connectivity framework (compared to 25.06.00 release)
Major Changes
[wireless_mcu] Replaced the ICS RX linked list with message queue to eliminate memory allocation in the ISR context and enable user callbacks to run in thread context where memory allocation is permitted.
[wireless_mcu] Added HCI RX workqueue processing support to reduce ISR execution time and system impact. Feature controlled by
gPlatformHciUseWorkqueueRxProcessing_dconfiguration option (enabled by default on kw45_k32w1_mcxw71 and kw47_mcxw72 platforms in freertos applications). When enabled, HCI transport processes received data in system workqueue thread, allowing user callbacks to run in thread context.[wireless_nbu] Introduced
PLATFORM_ConfigureSmuDmemMapping()API to configure SMU and DMEM sharing on NBU for kw47_mcxw72 platform, using linker file symbols for correct configuration.[wireless_mcu][wireless_nbu] Added NBU2Host event manager for status indications to host (Information, Warning, Error) sent over RPMSG.
[wireless_mcu] Added a call to
PLATFORM_IcsRxWorkHandler()withinPLATFORM_NbuApiReq()for baremetal applications to prevent potential deadlocks.[wireless_mcu] Adjusted default value of
BOARD_RADIO_DOMAIN_WAKE_UP_DELAYfrom 0x16 to 0x10 to address stability issues observed with the previous setting. This change enhances system reliability but will reduce low-power performance.[wireless_nbu] Enhanced XTAL32M trimming handling: updates are applied when requested by the application core and the NBU enters low-power mode, ensuring no interference from ongoing radio activity. Introduced new APIs to lock (
PLATFORM_LockXtal32MTrim()) and unlock XTAL32M (PLATFORM_UnlockXtal32MTrim()) trimming updates using a counter-based mechanism. Also added a reset API (PLATFORM_ResetContext()) for platform-specific variables (currently limited to the trimming lock).[wireless_mcu] Introduced a new API,
PLATFORM_SetLdoCoreNormalDriveVoltage(), to enable support for NBU clock frequency at 64 MHz, as required by BLE channel sounding applications.[wireless_mcu][wireless_nbu] Increased delayLpoCycle default from 2 to 3 to address link layer instabilities in low-power NBU use cases. Adjusted
BOARD_RADIO_DOMAIN_WAKE_UP_DELAYfrom 0x10 to 0x16 to balance power consumption and stability. ⚠️ NBU may malfunction if delayLpoCycle (orBOARD_LL_32MHz_WAKEUP_ADVANCE_HSLOT) is set to 2 whileBOARD_RADIO_DOMAIN_WAKE_UP_DELAYis 0x16.
Minor Changes (no impact on application)
[wireless_mcu] Fixed variable underflow issue in
PLATFORM_RemoteActiveRel().[SecLib_RNG] Fixed escaping local HashKeyBuffer address issue and added missing cast in
RNG_GetTrueRandomNumber()function.[Common] Fixed heap memory manager return values and added missing include to fwk_freertos_utils.h.
[rw61x] Prevented array out of bounds in
PLATFORM_RegisterRtcHandle().[FSCI] Fixed memory leak in FSCI module.
[NVM] Enhanced debug facilitation by restricting variable scope, assigning return statuses to variables, and fixing display format in
NV_ShowFlashTable().[wireless_mcu] Added new chip revision A2.1 support in
PLATFORM_SendChipRevision()API.[kw47_mcxw72] Implemented BLE BD address retrieval from IFR memory with fallback to OUI + RNG.
[DBG] Added ThreadX support to fault handlers and reworked fault handler structure with dedicated RTOS files.
[DBG][Common] Added NBU debug support on host side to detect faults and system errors, with debug info extraction capability (limited to MCXW72/KW47).
[Common] Platform CMake rework and Kconfig renaming, removing unneeded checks and renaming PRJSEG platform Kconfigs to COMPONENT.
[wireless_mcu] Cleaned CMakeLists.txt to avoid wrong inclusions of files and folders from incorrect platforms.
[wireless_mcu][wireless_nbu] Added NBU2Host warning when 32MHz crystal is unready on low power exit.
[wireless_mcu][ot] Introduced
gPlatformUseOuiFromIfrto use OUI from IFR for the extended address (disabled by default). When enabled and IFR is not blank, copies first three bytes to OUI field of extended address, otherwise uses static OUI as fallback.[General] Removed useless warning about TSTMR_CLOCK_FREQUENCY_MHZ definition.
[General] Updated framework license and SBOM for 25.09 RFP release.
[wireless_mcu] Fixed unused variable warning when
gPlatformIcsUseWorkqueueRxProcessing_dandgPlatformHciUseWorkqueueRxProcessing_dare disable[Common] Added MDK compatibility for the errno framework header.
[OTA] Enabled calling
OTA_GetImgState()prior toOTA_Initialize().[wireless_mcu] Fixed
PLATFORM_IsExternalFlashSectorBlank()to check the entire sector instead of just one page.[OTA] Removed
gUseInternalStorageLink_dlinker flag definition when external OTA storage is used.[wireless_mcu] Resolved counter wrap issue in
PLATFORM_GetDeltaTimeStamp().[kw47_mcxw72] Updated shared memory allocation for RPMsg adapter.
[kw45_mcxw71][kw47_mcxw72] Moved RAM bank definitions from the connectivity framework to device-specific definitions.
[WorkQ] Increased stack size when RNG use mbedtls port and coverage is enabled.
[FSCI] Resolved an issue where messages remained unprocessed in the queue by ensuring
OSA_EventSet()is triggered when pending messages are detected.[OTA] Fixed a bug in
OTA_PullImageChunk()that prevented retrieval of data previously received viaOTA_PushImageChunk()when still buffered in RAM during posted operations.[OTA] Various MISRA and coverity fixes.
[SFC] Remove obsolete flag
gNbuJtagCapability.[wireless_mcu] Introduced new API
PLATFORM_GetRadioIdleDuration32K(). DeprecatedPLATFORM_CheckNextBleConnectivityActivity()API.[DBG] Cleaned up fwk_fault_handler.c.
Note : Initial support to KW47B42Z83 and KW47B42Z97 KW47 phantoms linker support in connectivity see in README.md Details can be found in CHANGELOG.md
Known issues
This section lists the known issues, limitations, and/or workarounds.
New project wizard compile failure
The following components request the user to manually select other components that they depend upon in order to compile. These components depend on several other components and the New Project Wizard (NPW) is not able to decide which one is needed by the user.
Note: xxx means core variants, such as, cm0plus, cm33, cm4, cm33_nodsp.
Also for low-level adapter components, currently the different types of the same adapter cannot be selected at the same time. For example, if there are two types of timer adapters, gpt_adapter and pit_adapter, only one can be selected as timer adapter in one project at a time. Duplicate implementation of the function results in an error.
Only FreeRTOS is tested for RTOS support
This release only supports the FreeRTOS kernel and a bare-metal non-preemptive task scheduler.
Disabled pairing and bonding for most sensor applications
Most sensor applications have pairing and bonding disabled to allow a faster interaction with mobile applications. These two security features can be enabled in the app_preinclude.h header file.
Bluetooth LE
Most sensor applications have pairing and bonding disabled to allow a faster interaction with mobile applications. These two security features can be enabled in the app_preinclude.h header file.
Bluetooth LE controller:
The maximum Advertising data length is limited to 800 bytes.
Missing chained packets during scanning.
Need to add a dummy nbu request to wake-up NBU core during asynchronous wakeup to avoid low power race condition issue (ie: for NBU ramlog dump from shared memory).
Periodic Advertising with Responses (PAwR):
Periodic Advertising with Response (PAwR) is not supported with the configuration “Subevent Interval = Number of Response Slots * Response Slot Spacing”.
Unoptimized Periodic Advertising placement with Connection events.
KW45/MCXW71: No specific issues.
KW47/MCXW72: Channel Sounding (CS): Limitations:
RTT with Sounding Sequence is not supported.
TX SNR is not supported.
LE 2M 2BT PHY is not supported.
Maximum 6 Channel Sounding procedures are supported in parallel.
Scheduling of activities may be non optimal when multiple Channel Sounding procedures are running in parallel.
Phase measurement bias is within certification range (<1.7x2πns) with KW47 EVK board. However, if different PCB or antenna matching is used, some bias may appear due to increased delay.
Channel Sounding is not supported with internal FRO32. Known issues:
When CS_SYNC=2Mbps, sensitivity drops at –85dBm (vs –95dBm for 1Mbps).
NADM may report false positive attacks when using localization board at 2Mbps.
When CS Subevents are configured very close from each other (<700us), some Subevents may be aborted with reason 0x3.
When CS offset is configured too close from ACL anchor point, the anchor point may not be served (TX on central or RX on peripheral will not happen). Ideally, CS Offset should be configured greater than 1ms.
Wireless_ranging stability issue in test mode 2Mbps with RTT random sequence payload 128 bits.
RTT bias compensation:
For parts not properly configured at production (IFR blank), RTT bias may not be compensated properly. Consequently, an inaccuracy of +/-2m may be observed.
Temperature variation: RTT variation of +/-2m is observed based on temperature.
Other limitations
The following Connectivity Framework configurations are Experimental and not recommended for mass production:
Power down on application power domain.
A hardfault can be encountered when using fsl_component_mem_manager_light.c memory allocator and shutting down some unused RAM banks in low power. It is due to a wrong reinitialization of ECC RAM banks. To be sure not to reproduce the issue,
gPlatformShutdownEccRamInLowPowershould be set to 0.GenFSK
Connectivity_testapplication is not operational with Low Power enabled.Serial manager is only supported on UART (not I2C nor SPI).
The
--no-warn-rwx-segmentscannot been recognized on legacy MCUXpresso IDE versions.The
--no-warn-rwx-segmentsoption in MCUXpresso projects should be manually removed from the project settings if someone needs to use legacy (< 11.8.0) MCUXpresso IDE versionsIf the FRO32K is configured as the clock source of the CM33 Core then the debug session will block in both IAR, MCUX CMSIS-DAP while debugging. Use a lower debug wire speed, for example 1 MHz instead of the default one.
In IAR, the option is in Runtime Checking -> Debugger -> CMSIS DAP -> Interface -> Interface speed.
In MCUXpresso IDE, the option is in LinkServer Debugger -> Advanced Settings -> Wirespeed (Hz).
Low power reference design applications are not supported for the armgcc toolchain from zip archives. Please use MCUXpresso IDE or IAR toolchains for development using these applications.
Latest MCUX IDE 24.9.25 cannot support KW47 multicore compiling
The latest MCUX IDE 24.9.25 cannot support KW47 multicore compiling, users need to upgrade to the Linkserver_24.10.22 or higher version, and change the LinkServer path configuration in the MCUX IDE. Two ways to change the LinkerSever path in the MCUX IDE.
Option 1 (recommended): Using the custom Path

Option 2: Using the command-line to change the settings
Close the MCUXpresso IDE if it is open.
Execute the following command:
<path_to_MCUXpressoIDE_installation_folder>\ide\mcuxpressoide -application com.nxp.mcuxpresso.headless.application -nosplash -run set.config.preference com.nxp.mcuxpresso.core.debug.support.linkserver:linkserver.path.default_path=<path_to_LinkServer_installation_folder>
where:
<path_to_MCUXpressoIDE_installation_folder>is the folder where the MCUXpresso IDE is installed.<path_to_LinkServer_installation_folder>is the folder where the new/custom LinkServer is installed.
Example:
C:\NXP\MCUXpressoIDE_24.9.25\ide\mcuxpressoide -application com.nxp.mcuxpresso.headless.application -nosplash -run set.config.preference com.nxp.mcuxpresso.core.debug.support.linkserver:linkserver.path.default_path=c:\NXP\LinkServer_24.10.15
Examples hello_world_ns, secure_faults_ns, and secure_faults_trdc_ns have incorrect library path in GUI projects
When the affected examples are generated as GUI projects, the library linking the secure and non-secure worlds has an incorrect path set. This causes linking errors during project compilation.
Examples: hello_world_ns, hello_world_s, secure_faults_ns, secure_faults_s, secure_faults_trdc_ns, secure_faults_trdc_s
Affected toolchains: mdk, iar
Workaround: In the IDE project settings for the non-secure (_ns) project, find the linked library (named hello_world_s_CMSE_lib.o, or similar, depending on the example project) and replace the path to the library with <build_directory>/<secure_world_project_folder>/<IDE>/, replacing the subdirectory names with the build directory, the secure world project name, and IDE name.