tsCLD_ZllCommission_ScanRspCommandPayload
This structure is used to hold the payload data for a Touchlink Scan Response command.
typedef struct
{
uint32 u32TransactionId;
uint8 u8RSSICorrection;
uint8 u8ZigbeeInfo;
uint8 u8ZllInfo;
uint16 u16KeyMask;
uint32 u32ResponseId;
uint64 u64ExtPanId;
uint8 u8NwkUpdateId;
uint8 u8LogicalChannel;
uint16 u16PanId;
uint16 u16NwkAddr;
uint8 u8NumberSubDevices;
uint8 u8TotalGroupIds;
uint8 u8Endpoint;
uint16 u16ProfileId;
uint16 u16DeviceId;
uint8 u8Version;
uint8 u8GroupIdCount;
} tsCLD_ZllCommission_ScanRspCommandPayload;
where:
u32TransactionIdis the 32-bit Inter-PAN Transaction Identifier of the response, which must take the same value as the identifier in the corresponding request.u8RSSICorrectionis the 8-bit RSSI correction offset for the node, in the range 0x00 to 0x20.u8ZigbeeInfois an 8-bit field containing the following ZigBee-related information:Bits 1-0: Node type (00 - Co-ordinator, 01 - Router, 10 - End Device)
Bit 2: Rx on when idle (1 - On, 0 - Off)
Bits 7-3: Reserved
u8ZllInfois an 8-bit field containing the following information:Bit 0: Factory new (1 - Yes, 0 - No)
Bit 1: Address assignment capability (1 - Yes, 0 - No)
Bits 3-2: Reserved
Bit 4: Touchlink initiator (1 - Yes, 0 - No)
Bit 5: Touchlink priority request (1 - Yes, 0 - No)
Bits 7-6: Reserved
u16KeyMaskis a 16-bit bitmap indicating which link key is installed on the node - only one bit should be set to ‘1’, corresponding to the key that is in use. The possible values and keys are:0x0001 (bit 0 set): Development key (defined by developer for use during application development)
0x0010 (bit 4 set): Master key (obtained from the ZigBee Alliance after successful certification and agreement with the terms of the ‘ZLL Security Key Licence and Confidentialty Agreement’)
0x8000 (bit 15 set): Certification key (defined in the ZLL Specification for use during development and during certification at test houses)
u``32ResponseIdis a 32-bit random identifier for the response, used during network key transfer.u64ExtPanIdis the 64-bit Extended PAN ID of a network to which the node already belongs, if any (a zero value indicates no network membership).u8NwkUpdateIdis the current value of the Network Update Identifier on the node (see Section 44.4.3).u8LogicalChannelis the number of the IEEE 802.15.4 radio channel used by a network to which the node already belongs, if any (a zero value indicates no network membership and therefore that no particular channel is used).u16PanIdis the 16-bit PAN ID of a network to which the node already belongs, if any (a zero value indicates no network membership).u16NwkAddris the 16-bit network address currently assigned to the node (the value 0xFFFF indicates that the node is ‘factory new’ and has no assigned network address).u8NumberSubDevicesis the number of ZigBee devices on the node.u8TotalGroupIdsis the total number of groups (of lights) supported on the node (across all devices).u8Endpointis number of the endpoint (in the range 1-240) on which the ZigBee device is resident (this field is only used when there is only one ZigBee device on the node).u16ProfileIdis the 16-bit identifier of the ZigBee application profile that is supported by the device (this field is only used when there is only one ZigBee device on the node).u16DeviceIdis the 16-bit Device Identifier supported by the device (this field is only used when there is only one ZigBee device on the node).u8Versionis an 8-bit version number for the device - the four least significant bits are from the Application Device Version field of the appropriate Simple Descriptor and the four most significant bits are zero (this field is only used when there is only one ZigBee device on the node).u8GroupIdCountis the number of groups (of lights) supported by the device (this field is only used when there is only one ZigBee device on the node).
Parent topic:Structures