Price events
The Price cluster has its own events that are handled through the callback mechanism described in Chapter 3. If a device uses the Price cluster then Price event handling must be included in the callback function for the associated endpoint, where this callback function is registered through the relevant endpoint registration function (for example, through eSE_RegisterEspEndPoint() for a standalone ESP). The relevant callback function will then be invoked when a Price event occurs.
For a Price event, the eEventType field of the tsZCL_CallBackEvent structure is set to E_ZCL_CBET_CLUSTER_CUSTOM. This event structure also contains an element sClusterCustomMessage, which is itself a structure containing a field pvCustomData. This field is a pointer to a tsSE_PriceCallBackMessage structure which contains the Price parameters:
typedef struct
{
teSE_PriceCallBackEventType eEventType;
uint32 u32CurrentTime;
union {
tsSE_PriceTableCommand sPriceTableCommand;
tsSE_PriceTableTimeEvent sPriceTableTimeEvent;
teSE_PriceCommandOptions ePriceCommandOptions;
tsSE_PriceAckCmdPayload *psAckCmdPayload;
tsSE_PriceAttrReadInput sReadAttrInfo;
tsSE_BlockPeriodTableTimeEvent sBlockPeriodTableTimeEvent;
tsSE_ConversionFactorTableTimeEvent sConversionFactorTableTimeEvent;
tsSE_CalorificValueTableTimeEvent sCalorificValueTableTimeEvent;
} uMessage;
} tsSE_PriceCallBackMessage;
The eEventType field of the above structure specifies the type of Price event that has been generated - these event types are listed and described below (also refer to Section 40.12.2 for a summary of the Price events).
Note: The field sReadAttrInfo is reserved for future use (for Block mode).
E_SE_PRICE_TABLE_ADD
The E_SE_PRICE_TABLE_ADD event is generated on a Price cluster client when an attempt has been made to add a scheduled price (received in a Publish Price command) to the local price list. In the tsSE_PriceCallBackMessage structure, the u32CurrentTime field is set to the current time from the Publish Price command and the sPriceTableCommand field is used as follows:
typedef struct {
teSE_PriceStatus ePriceStatus;
} tsSE_PriceTableCommand;
ePriceStatus contains E_SE_PRICE_SUCCESS if a new price has been successfully added to the price list. Otherwise, the addition was rejected for the reason specified by ePriceStatus. If the addition was successful but the new price information overlapped (in time) any existing price information in the list, this previous price information may have been deleted from the list according to the rules in the ZigBee SE Profile specification.
E_SE_PRICE_TABLE_ACTIVE
The E_SE_PRICE_TABLE_ACTIVE event is generated when there is a new active price or the active price expires. This event can occur due to a time update or the reception of a Publish Price command from the server. In the tsSE_PriceCallBackMessage structure, the u32CurrentTime field is set to the current ZCL time and the sPriceTableTimeEvent field is used as follows:
typedef struct {
teSE_PriceStatus ePriceStatus;
uint8 u8NumberOfEntriesFree;
} tsSE_PriceTableTimeEvent;
ePriceStatus contains E_SE_PRICE_SUCCESS if there is a new active price or E_SE_PRICE_TABLE_NOT_YET_ACTIVE if the price at the head of the list is scheduled for a time in the future.
u8NumberOfEntriesFree contains the number of free entries in the client’s price list. This number can be used to determine whether the client should issue a new Get Scheduled Prices command, in order to obtain more price entries to fill the free space in the list.
E_SE_PRICE_GET_CURRENT_PRICE_RECEIVED
The E_SE_PRICE_GET_CURRENT_PRICE_RECEIVED event is generated on a Price cluster server when a Get Current Price command is received from a client. In the tsSE_PriceCallBackMessage structure, the ePriceCommandOptions field is used as follows:
typedef enum PACK
{
E_SE_PRICE_REQUESTOR_RX_ON_IDLE = 0x01 // LSB set
} teSE_PriceCommandOptions;
This field indicates whether the client that sent the request has its radio receiver enabled when idle (e.g. sleeping), and is used as described in Section 40.5.1 and Section 40.5.2.
E_SE_PRICE_TIME_UPDATE
The E_SE_PRICE_TIME_UPDATE event is generated on a Price cluster client when a Publish Price command is received from the server. In the tsSE_PriceCallBackMessage structure, the u32CurrentTime field is set to the current time from the Publish Price command. The application may then use this information to time-synchronise the device, as described in Section 40.6.
E_SE_PRICE_ACK_RECEIVED
The E_SE_PRICE_ACK_RECEIVED event is generated on a Price cluster server when a Price Acknowledgment command is received from a client. In the tsSE_PriceCallBackMessage structure, the psAckCmdPayload field is a pointer to the structure tsSE_PriceAckCmdPayload defined as follows:
typedef struct {
uint32 u32ProviderId;
uint32 u32IssuerEventId;
uint32 u32PriceAckTime;
uint8 u8Control;
} tsSE_PriceAckCmdPayload;
This structure contains the Price Acknowledgement command payload.
E_SE_PRICE_NO_PRICE_TABLES
The E_SE_PRICE_NO_PRICE_TABLES event is generated when an active price expires, is deleted from the price list and the price list becomes empty. In the tsSE_PriceCallBackMessage structure the sPriceTableTimeEvent field is used as follows:
typedef struct {
teSE_PriceStatus ePriceStatus;
uint8 u8NumberOfEntriesFree;
} tsSE_PriceTableTimeEvent;
ePriceStatus contains E_SE_PRICE_NO_TABLES.
u8NumberOfEntriesFree contains the number of free entries in the client’s price list. This number can be used to determine whether the client should issue a new Get Scheduled Prices command, in order to obtain more price entries to fill the free space in the list.
E_SE_PRICE_CONVERSION_FACTOR_TABLE_ACTIVE
The E_SE_PRICE_CONVERSION_FACTOR_TABLE_ACTIVE event is generated when a new conversion factor value becomes active - that is, when the start-time of the conversion factor entry becomes less than or equal to the present time. This event can occur due to a time update or the reception of a Publish Conversion Factor command from the server.
In the tsSE_PriceCallBackMessage structure, the u32CurrentTime field is set to the current ZCL time and the field tsSE_PriceConversionFactorTableTimeEvent is used as follows:
typedef struct {
teSE_PriceStatus eConversionFactorStatus;
uint8 u8NumberOfEntriesFree;
} tsSE_ConversionFactorTableTimeEvent;
eConversionFactorStatus takes the value E_ZCL_SUCCESS when a new conversion factor becomes active.
u8NumberOfEntriesFree contains the present number of free entries in the conversion factor list. This value should be checked by the client before issuing a Get Conversion Factor command to obtain a new conversion factor value - the command should be issued only if there is free space in the list for a new entry to be added.
E_SE_PRICE_CONVERSION_FACTOR_ADD
The E_SE_PRICE_CONVERSION_FACTOR_ADD event is generated when a new conversion factor entry is advertised by the ESP to the client application using the Publish Conversion Factor command. Note that the event is generated even when the new entry is not successfully added to the internal conversion factor list maintained by the cluster.
The status of the command is passed back to the user application in the ePriceStatus field of the tsSE_PriceTableCommand structure (see above) within the tsSE_PriceCallBackMessage structure.
E_SE_PRICE_CALORIFIC_VALUE_TABLE_ACTIVE
The E_SE_PRICE_CALORIFIC_VALUE_TABLE_ACTIVE event is generated when a new calorific value becomes active - that is, when the start-time of the calorific value entry becomes less than or equal to the present time. This event can occur due to a time update or the reception of a Publish Calorific Value command from the server.
In the tsSE_PriceCallBackMessage structure, the u32CurrentTime field is set to the current ZCL time and the field tsSE_PriceCalorificValueTableTimeEvent is used as follows:
typedef struct {
teSE_PriceStatus eCalorificValueStatus;
uint8 u8NumberOfEntriesFree;
} tsSE_CalorificValueTableTimeEvent;
eCalorificValueStatus takes the value E_ZCL_SUCCESS when a new calorific value becomes active.
u8NumberOfEntriesFree contains the present number of free entries in the calorific value list. This value should be checked by the client before issuing a Get Calorific Value command to obtain a new calorific value - the command should be issued only if there is free space in the list for a new entry to be added.
E_SE_PRICE_CALORIFIC_VALUE_ADD
The E_SE_PRICE_CALORIFIC_VALUE_ADD event is generated when a new calorific value entry is advertised by the ESP to the client application using the Publish Calorific Value command. Note that this event is generated even when the new entry is not successfully added to the internal calorific value list maintained by the cluster.
The status of the command is passed back to the user application in the ePriceStatus field of the tsSE_PriceTableCommand structure (see above) within the tsSE_PriceCallBackMessage structure.
Parent topic:Price Cluster