tsCLD_Commissioning_RestartDevicePayload
The following structure contains the payload of a Restart Device command.
typedef struct
{
zbmap8 u8Options;
uint8 u8Delay;
uint8 u8Jitter;
} tsCLD_Commissioning_RestartDevicePayload;
where:
u8Options is a 8-bit bitmap specifying the required start-up options:
Bits |
Option |
Description |
|---|---|---|
0-2 |
Start-up Mode |
Determines the starting state of the device restart: |
0b000: Restart with current Start-up Parameter values
0b001: Restart from existing stack state
All other values are reserved.
| |3|Immediate|Determines how quickly the start-up procedure will begin follow-ing receipt of the command or the specified delay/jitter:
1: Immediately
0: At a convenient moment (e.g. following any pending actions)
| |4-7|-|Reserved|
u8Delay specifies the time-delay, in seconds, before the start-up procedure should be executed.
u8Jitter is a value which determines the possible range of values of the jitter that is added to the delay u8Delay - the jitter, in milliseconds, is a random value in the range 0 to u8Jitter x 80.
Parent topic:Structures