tsCLD_Commissioning_ModifyStartupParametersPayload
The following structure contains the payload of the following commands: Save Start-up Parameters, Restore Start-up Parameters and Reset Start-up Parameters.
typedef struct
{
zbmap8 u8Options;
uint8 u8Index;
} tsCLD_Commissioning_ModifyStartupParametersPayload;
where:
u8Options is an 8-bit bitmap specifying the required reset options for the Reset Start-up Parameters command (it is not used by the other commands):
Bits |
Option |
Description |
|---|---|---|
0 |
Reset Current |
Determines whether the current Start-up Parameters will be reset to their default values: |
1: Reset to default values
0: Do not reset (remain unchanged)
| |1|Reset All|Determines whether all stored Start-up Parameter sets will be reset to their default values:
1: Reset all stored Start-up Parameter sets
0: Reset the stored Start-up Parameter set with specified index
| |2|Erase Index|Determines whether the stored Start-up Parameter set with speci-fied index will be erased:
1: Erase Start-up Parameter set with specified index
0: Do not erase Start-up Parameter set with specified index
| |3-7|-|Reserved|
u8Index is the index of the saved Start-up Parameter set to which actions specified in u8Options relate (this index is ignored if no actions are specified).
Parent topic:Structures