Commissioning Events
The Commissioning cluster has its own events that are handled through the callback mechanism outlined in Chapter 3. If a device uses this cluster then application-specific Commissioning event handling must be included in the user-defined callback function for the associated endpoint, where this callback function is registered through the relevant endpoint registration function. This callback function will then be invoked when a Commissioning event occurs and needs the attention of the application.
For a Commissioning event, the eEventType field of the tsZCL_CallBackEvent structure is set to E_ZCL_CBET_CLUSTER_CUSTOM. This event structure also contains an element sClusterCustomMessage, which is itself a structure containing a field pvCustomData. This field is a pointer to the following tsCLD_CommissioningCallBackMessage structure (fully detailed in Section43.9.6).
typedef struct
{
uint8 u8CommandId;
union
{
tsCLD_Commissioning_RestartDevicePayload
*psRestartDevicePayload;
tsCLD_Commissioning_ModifyStartupParametersPayload
*psModifyStartupParamsPayload;
} uReqMessage;
union
{
tsCLD_Commissioning_ResponsePayload
*psCommissioningResponsePayload;
} uRespMessage;
} tsCLD_CommissioningCallBackMessage;
When a Commissioning event occurs, one of a number of command types could have been received. The relevant command type is specified through the u8CommandId field of the tsCLD_CommissioningCallBackMessage structure. The possible command types are detailed below.
The table below details the command types that can be received by the cluster server.
u8CommandId Enumeration |
Description |
|---|---|
E_CLD_COMMISSIONING_CMD_RESTART_DEVICE |
A Restart Device command has been received |
E_CLD_COMMISSIONING_CMD_SAVE_STARTUP_PARAMS |
A Save Start-up Parameters command has been received |
E_CLD_COMMISSIONING_CMD_RESTORE_STARTUP_PARAMS |
A Restore Start-up Parameters command has been received |
E_CLD_COMMISSIONING_CMD_RESET_STARTUP_PARAMS |
A Reset Start-up Parameters command has been received |
The table below details the command types that can be received by the cluster client.
u8CommandId Enumeration |
Description |
|---|---|
E_CLD_COMMISSIONING_CMD_RESTART_DEVICE |
A Restart Device response has been received |
E_CLD_COMMISSIONING_CMD_SAVE_STARTUP_PARAMS |
A Save Start-up Parameters response has been received |
E_CLD_COMMISSIONING_CMD_RESTORE_STARTUP_PARAMS |
A Restore Start-up Parameters response has been received |
E_CLD_COMMISSIONING_CMD_RESET_STARTUP_PARAMS |
A Reset Start-up Parameters response has been received |
Parent topic:Commissioning Cluster