Custom Response Payloads
This section contains the structures for the payloads of the Alarms cluster custom responses.
Get Alarm Response Payload
typedef struct
{
uint8 u8Status;
uint8 u8AlarmCode;
uint16 u16ClusterId;
uint32 u32TimeStamp;
} tsCLD_AlarmsGetAlarmResponsePayload;
where:
u8Statusindicates the result of the Get Alarm operation as follows:SUCCESS (0x01): An alarm entry is successfully retrieved from the Alarms table and its details are reported in the remaining fields (below)
NOT_FOUND (0x00): There were no alarm entries to be retrieved from the Alarms table and the remaining fields (below) are empty
u8AlarmCodeis the code which identifies the type of alarm reported - these codes are cluster-specificu16ClusterIdis the Cluster ID of the cluster which generated the alarmu32TimeStampis a timestamp representing the time (UTC) at which the alarm was generated (a value of 0XFFFFFFFF indicates that no timestamp is available for the alarm)
Parent topic:Custom Response Payloads
Parent topic:Structures