BDB_tsOobWriteDataToCommission
The following structure contains the data values used to initialize a node at the start of out-of-band commissioning of the node.
typedef struct{
uint64 u64PanId;
uint64 u64TrustCenterAddress;
uint8* pu8NwkKey;
uint8* pu8InstallCode;
uint16 u16PanId;
uint16 u16ShortAddress;
bool_t bRejoin;
uint8 u8ActiveKeySqNum;
uint8 u8DeviceType;
uint8 u8RxOnWhenIdle;
uint8 u8Channel;
uint8 u8NwkUpdateId;
}BDB_tsOobWriteDataToCommission;
where:
u64PanIdis the Extended PAN ID of the network to be joined.u64TrustCenterAddressis the IEEE/MAC address of the Trust Centre in the centralized network to be joined.pu8NwkKeyis a pointer to the network key.pu8InstallCodeis a pointer to an initial link key derived from an install code (see Section 2.3.1).u16PanIdis the PAN ID of the network to be joined.u16ShortAddressis the network address assigned to the node.bRejoinis the ‘rejoin flag’ which indicates whether the node should attempt to rejoin the network if it leaves (TRUE: rejoin, FALSE: do not rejoin).u8ActiveKeySqNumis the key sequence number associated with the active network key.u8DeviceTypeis a value indicating the type of ZigBee node:0: Coordinator
1: Router
2: End Device All other values are reserved.
u8RxOnWhenIdleis a value indicating whether the receiver of the node is enabled during idle periods:0: Receiver off when idle (sleeping device)
1: Receiver on when idle (non-sleeping device) All other values are reserved.
u8Channelis the radio channel number on which the network operates.u8NwkUpdateIdis a unique byte value which is incremented when the network parameters are updated (and is therefore used to determine whether a receiving node has missed an update).
Parent topic:Structures