ZPS_tsNwkNetworkDescr
This structure is used in an array element in the structure ZPS_tsAfNwkDiscoveryEvent, which is created as part of the ZPS_EVENT_NWK_DISCOVERY_COMPLETE event. This event reports the networks detected during a network discovery (see Section 8.2.2.9).
The ZPS_tsNwkNetworkDescrstructure contains information on a detected network and is detailed below.
typedef struct
{
uint64 u64ExtPanId;
uint8 u8LogicalChan;
uint8 u8StackProfile;
uint8 u8ZigBeeVersion;
uint8 u8PermitJoining;
uint8 u8RouterCapacity;
uint8 u8EndDeviceCapacity;
} ZPS_tsNwkNetworkDescr;
where:
u64ExtPanIdis the Extended PAN ID of the discovered network.u8LogicalChanis the 2400-MHz channel on which the network was found.u8StackProfileis the Stack Profile of the discovered network:0 - manufacturer-specific
1 - ZigBee
2 - ZigBee PRO
other values reserved, and is fixed at 2 for the NXP stack
u8ZigBeeVersionis the ZigBee version of the discovered network.u8PermitJoiningindicates the number of detected nodes with ‘permit joining’ enabled (and therefore allowing nodes to join the network through them).u8RouterCapacityindicates the number of detected nodes that are allowing Routers to join the network through them.u8EndDeviceCapacityindicates the number of detected nodes that are allowing End Devices to join the network through them.
Parent topic:Other structures