ZPS_tsAplZdpStoreBkupBindEntryRsp
This structure is used to store Store_Bkup_Bind_Entry_rsp message data - a response to a call to the function ZPS_eAplZdpStoreBkupBindEntryRequest(). This response indicates the status of the back-up request.
The ZPS_tsAplZdpStoreBkupBindEntryRspstructure is detailed below.
typedef struct {
uint8 u8Status;
} ZPS_tsAplZdpStoreBkupBindEntryRsp;
where u8Statusis the return status for the function ZPS_eAplZdpStoreBkupBindEntryRequest().
Parent topic:ZDP response structures