ZPS_tsAplZdpRemoveNodeCacheReq
This structure is used by the function ZPS_eAplZdpActiveEpStoreRequest(). It represents a request to a remote node to remove from its Primary Discovery Cache all ‘discovery information’ relating to a particular End Device.
The ZPS_tsAplZdpRemoveNodeCacheReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
} ZPS_tsAplZdpRemoveNodeCacheReq;
where:
u16NwkAddris the network address of the End Device of interestu64IeeeAddris the IEEE address of the End Device of interest
Parent topic:ZDP Request structures