ZPS_tsAplZdpMgmtNwkUpdateNotify
This structure is used to store Mgmt_NWK_Update_notify message data - a notification which can be sent in response to a call to the function ZPS_eAplZdpMgmtNwkUpdateRequest(). This notification reports the results of an energy scan on the wireless network radio channels.
The ZPS_tsAplZdpMgmtNwkUpdateNotifystructure is detailed below.
Sample Codeblock:
typedef struct {
uint8 u8Status;
uint32 u32ScannedChannels;
uint16 u16TotalTransmissions;
uint16 u16TransmissionFailures;
uint8 u8ScannedChannelListCount;
/* Rest of the message is variable Length */
uint8* u8EnergyValuesList;
} ZPS_tsAplZdpMgmtNwkUpdateNotify;
where:
u8Statusis the return status for ZPS_eAplZdpMgmtNwkUpdateRequest()u32ScannedChannelsis a bitmask of the set of scanned radio channels (‘1’ means scanned, ‘0’ means not scanned):Bits 0 to 26 respectively represent channels 0 to 26 (only bits 11 to 26 are relevant to the 2400-MHz band)
Bits 27 to 31 are reserved
u16TotalTransmissionsis the total number of transmissions (from other networks) detected during the scanu16TransmissionFailuresis the number of failed transmissions detected during the scanu8ScannedChannelListCountis the number of energy-level measurements (one per scanned channel) reported in this notification (throughu8EnergyValuesList)u8EnergyValuesListis a pointer to the first in the set of reported energy-level measurements (the value 0xFF indicates there is too much interference on the channel)
Parent topic:ZDP response structures