ZPS_tsAplZdpMgmtNwkDiscReq
This structure is used by the function ZPS_eAplZdpMgmtNwkDiscRequest(). It represents a request to a remote node to discover any other wireless networks that are operating in the neighborhood.
The ZPS_tsAplZdpMgmtNwkDiscReqstructure is detailed below.
typedef struct {
uint32 u32ScanChannels;
uint8 u8ScanDuration;
uint8 u8StartIndex;
} ZPS_tsAplZdpMgmtNwkDiscReq;
where:
u32ScanChannelsis a bitmask of the radio channels to scan (‘1’ means scan, ‘0’ means do not scan):Bits 0 to 26 respectively represent channels 0 to 26 (only bits 11 to 26 are relevant to the 2400-MHz band)
Bits 27 to 31 are reserved
u8ScanDurationis a value in the range 0x00 to 0x0E that determines the time spent scanning each channel - this time is proportional to 2u8ScanDuration+1u8StartIndexis the index of the first result from the results list to include in the response to this request
Parent topic:ZDP Request structures