ZPS_tsAplZdpMgmtDirectJoinRsp
This structure is used to store Mgmt_Direct_Join_rsp message data - a response to a call to the function ZPS_eAplZdpMgmtDirectJoinRequest(). This response is issued by a remote node (Router or Coordinator) that has been requested to allow a particular device to join the network as a child of the node.
The ZPS_tsAplZdpMgmtDirectJoinRspstructure is detailed below.
typedef struct {
uint8 u8Status;
} ZPS_tsAplZdpMgmtDirectJoinRsp;
where u8Statusis the return status for ZPS_eAplZdpMgmtDirectJoinRequest().
Parent topic:ZDP response structures