ZPS_tsAfNwkLeaveConfEvent
This structure is used in the event ZPS_EVENT_NWK_LEAVE_CONFIRM, which reports the results of a node leave request issued by the local node.
The ZPS_tsAfNwkLeaveConfEventstructure is detailed below.
typedef struct {
uint64 u64ExtAddr;
uint8 eStatus;
} ZPS_tsAfNwkLeaveConfEvent;
where:
u64ExtAddris the 64-bit IEEE (MAC) address of the leaving node. This value is zero if the local node itself is leaving.eStatusis the leave status returned by the lower layers - ZPS_NWK_ENUM_SUCCESS, if the leave request has been successful.
Parent topic:Event structures