ZPS_tsAfInterPanDataIndEvent
This structure is used in the ZPS_EVENT_APS_INTERPAN_DATA_INDICATION event, which indicates that an inter-PAN data packet has arrived.
The ZPS_tsAfInterPanDataIndEventstructure is detailed below.
typedef struct
{
ZPS_tsInterPanAddress sDstAddr;
uint8 u8SrcAddrMode;
uint16 u16SrcPan;
uint64 u64SrcAddress;
uint16 u16ProfileId;
uint16 u16ClusterId;
PDUM_thAPduInstance hAPduInst;
uint8 eStatus;
uint8 u8DstEndpoint;
uint8 u8LinkQuality;
} ZPS_tsAfInterPanDataIndEvent;
where
sDstAddris a structure of the typeZPS_tsInterPanAddress(see Section8.2.3.3) which contains the PAN ID and address for the destination node(s) of the inter-PAN data packet.u8SrcAddrModeindicates the type of address specified through the elementu64SrcAddress(see Table).u16SrcPanis the PAN ID of the network from which the data packet originates.u64SrcAddressis the address of the node which sent the data packet (the type of address is specified using the elementu8SrcAddrModeabove).u16ProfileIdis the identifier of the application profile for which the data packet is intended.u16ClusterIdis the identifier of the cluster for which the data packet is intended.hAPduInstis the handle of the APDU instance for the data packet.eStatusis one of the status codes from the lower stack layers, detailed in Section 11.2.u8DstEndpointis the number of the destination endpoint for the data packet (in range 1-240).u8LinkQualityis an LQI value indicating the perceived strength of the radio signal which carried the received data packet.
Parent topic:Event structures