Changelog RPMSG-Lite

All notable changes to this project will be documented in this file.

The format is based on Keep a Changelog, and this project adheres to Semantic Versioning.

v5.2.1

Added

  • Doc added RPMSG-Lite VirtIO Overview

  • Doc added RPSMG-Lite Design Consi​derations

  • Added frdmimxrt1186 unit testing

Fixed

  • Fixed CERT-C INT31-C violation in platform_notify function in rpmsg_platform.c for imxrt700_m33, imxrt700_hifi4, imxrt700_hifi1 platforms

v5.2.0

Added

  • Add MCXL20 porting layer and unit testing

  • New utility macro RL_CALCULATE_BUFFER_COUNT_DOWN_SAFE to safely determine maximum buffer count within shared memory while preventing integer underflow.

  • RT700 platform add support for MCMGR in DSPs

Changed

  • Change rpmsg_platform.c to support new MCMGR API

  • Improved input validation in initialization functions to properly handle insufficient memory size conditions.

  • Refactored repeated buffer count calculation pattern for better code maintainability.

  • To make sure that remote has already registered IRQ there is required App level IPC mechanism to notify master about it

Fixed

  • Fixed env_wait_for_link_up function to handle timeout in link state checks for baremetal and qnx environment, RL_BLOCK mode can be used to wait indefinitely.

  • Fixed CERT-C INT31-C violation by adding compile-time check to ensure RL_PLATFORM_HIGHEST_LINK_ID remains within safe range for 16-bit casting in virtqueue ID creation.

  • Fixed CERT-C INT30-C violations by adding protection against unsigned integer underflow in shared memory calculations, specifically in shmem_length - (uint32_t)RL_VRING_OVERHEAD and shmem_length - 2U * shmem_config.vring_size expressions.

  • Fixed CERT INT31-C violation in platform_interrupt_disable() and similar functions by replacing unsafe cast from uint32_t to int32_t with a return of 0 constant.

  • Fixed unsigned integer underflow in rpmsg_lite_alloc_tx_buffer() where subtracting header size from buffer size could wrap around if buffer was too small, potentially leading to incorrect buffer sizing.

  • Fixed CERT-C INT31-C violation in rpmsg_lite.c where size parameter was cast from uint32_t to uint16_t without proper validation.

    • Applied consistent masking approach to both size and flags parameters: (uint16_t)(value & 0xFFFFU).

    • This fix prevents potential data loss when size values exceed 65535.

  • Fixed CERT INT31-C violation in env_memset functions by explicitly converting int32_t values to unsigned char using bit masking. This prevents potential data loss or misinterpretation when passing values outside the unsigned char range (0-255) to the standard memset() function.

  • Fixed CERT-C INT31-C violations in RPMsg-Lite environment porting: Added validation checks for signed-to-unsigned integer conversions to prevent data loss and misinterpretation.

    • rpmsg_env_freertos.c: Added validation before converting int32_t to UBaseType_t.

    • rpmsg_env_qnx.c: Fixed format string and added validation before assigning to mqstat fields.

    • rpmsg_env_threadx.c: Added validation to prevent integer overflow and negative values.

    • rpmsg_env_xos.c: Added range checking before casting to uint16_t.

    • rpmsg_env_zephyr.c: Added validation before passing values to k_msgq_init.

  • Fixed a CERT INT31-C compliance issue in env_get_current_queue_size() function where an unsigned queue count was cast to a signed int32_t without proper validation, which could lead to lost or misinterpreted data if queue size exceeded INT32_MAX.

  • Fixed CERT INT31-C violation in rpmsg_platform.c where memcmp() return value (signed int) was compared with unsigned constant without proper type handling.

  • Fixed CERT INT31-C violation in rpmsg_platform.c where casting from uint32_t to uint16_t could potentially result in data loss. Changed length variable type from uint16_t to uint32_t to properly handle memory address differences without truncation.

  • Fixed potential integer overflow in env_sleep_msec() function in ThreadX environment implementation by rearranging calculation order in the sleep duration formula.

  • Fixed CERT-C INT31-C violation in RPMsg-Lite where bitwise NOT operations on integer constants were performed in signed integer context before being cast to unsigned. This could potentially lead to misinterpreted data on imx943 platform.

  • Added RL_MAX_BUFFER_COUNT (32768U) and RL_MAX_VRING_ALIGN (65536U) limit to ensure alignment values cannot contribute to integer overflow

  • Fixed CERT INT31-C violation in vring_need_event(), added cast to uint16_t for each operand.

v5.1.4 - 27-Mar-2025

Added

  • Add KW43B43 porting layer

Changed

  • Doxygen bump to version 1.9.6

v5.1.3 - 13-Jan-2025

Added

  • Memory cache management of shared memory. Enable with #define RL_USE_DCACHE (1) in rpmsg_config.h in case of data cache is used.

  • Cmake/Kconfig support added.

  • Porting layers for imx95, imxrt700, mcmxw71x, mcmxw72x, kw47b42 added.

v5.1.2 - 08-Jul-2024

Changed

  • Zephyr-related changes.

  • Minor Misra corrections.

v5.1.1 - 19-Jan-2024

Added

  • Test suite provided.

  • Zephyr support added.

Changed

  • Minor changes in platform and env. layers, minor test code updates.

v5.1.0 - 02-Aug-2023

Added

  • RPMsg-Lite: Added aarch64 support.

Changed

  • RPMsg-Lite: Increased the queue size to (2 * RL_BUFFER_COUNT) to cover zero copy cases.

  • Code formatting using LLVM16.

Fixed

  • Resolved issues in ThreadX env. layer implementation.

v5.0.0 - 19-Jan-2023

Added

  • Timeout parameter added to rpmsg_lite_wait_for_link_up API function.

Changed

  • Improved debug check buffers implementation - instead of checking the pointer fits into shared memory check the presence in the VirtIO ring descriptors list.

  • VRING_SIZE is set based on number of used buffers now (as calculated in vring_init) - updated for all platforms that are not communicating to Linux rpmsg counterpart.

Fixed

  • Fixed wrong RL_VRING_OVERHEAD macro comment in platform.h files

  • Misra corrections.

v4.0.0 - 20-Jun-2022

Added

  • Added support for custom shared memory arrangement per the RPMsg_Lite instance.

  • Introduced new rpmsg_lite_wait_for_link_up() API function - this allows to avoid using busy loops in rtos environments, GitHub PR #21.

Changed

  • Adjusted rpmsg_lite_is_link_up() to return RL_TRUE/RL_FALSE.

v3.2.0 - 17-Jan-2022

Added

  • Added support for i.MX8 MP multicore platform.

Changed

  • Improved static allocations - allow OS-specific objects being allocated statically, GitHub PR #14.

  • Aligned rpmsg_env_xos.c and some platform layers to latest static allocation support.

Fixed

  • Minor Misra and typo corrections, GitHub PR #19, #20.

v3.1.2 - 16-Jul-2021

Added

  • Addressed MISRA 21.6 rule violation in rpmsg_env.h (use SDK’s PRINTF in MCUXpressoSDK examples, otherwise stdio printf is used).

  • Added environment layers for XOS.

  • Added support for i.MX RT500, i.MX RT1160 and i.MX RT1170 multicore platforms.

Fixed

  • Fixed incorrect description of the rpmsg_lite_get_endpoint_from_addr function.

Changed

  • Updated RL_BUFFER_COUNT documentation (issue #10).

  • Updated imxrt600_hifi4 platform layer.

v3.1.1 - 15-Jan-2021

Added

  • Introduced RL_ALLOW_CONSUMED_BUFFERS_NOTIFICATION config option to allow opposite side notification sending each time received buffers are consumed and put into the queue of available buffers.

  • Added environment layers for Threadx.

  • Added support for i.MX8QM multicore platform.

Changed

  • Several MISRA C-2012 violations addressed.

v3.1.0 - 22-Jul-2020

Added

  • Added support for several new multicore platforms.

Fixed

  • MISRA C-2012 violations fixed (7.4).

  • Fixed missing lock in rpmsg_lite_rx_callback() for QNX env.

  • Correction of rpmsg_lite_instance structure members description.

  • Address -Waddress-of-packed-member warnings in GCC9.

Changed

  • Clang update to v10.0.0, code re-formatted.

v3.0.0 - 20-Dec-2019

Added

  • Added support for several new multicore platforms.

Fixed

  • MISRA C-2012 violations fixed, incl. data types consolidation.

  • Code formatted.

v2.2.0 - 20-Mar-2019

Added

  • Added configuration macro RL_DEBUG_CHECK_BUFFERS.

  • Several MISRA violations fixed.

  • Added environment layers for QNX and Zephyr.

  • Allow environment context required for some environment (controlled by the RL_USE_ENVIRONMENT_CONTEXT configuration macro).

  • Data types consolidation.

v1.1.0 - 28-Apr-2017

Added

  • Supporting i.MX6SX and i.MX7D MPU platforms.

  • Supporting LPC5411x MCU platform.

  • Baremental and FreeRTOS support.

  • Support of copy and zero-copy transfer.

  • Support of static API (without dynamic allocations).