Hardware requirements

  • Type-C USB cable

  • FRDM-MCXA266 board

  • Personal Computer

Overview

This application demonstrates use of certified NXP Safety Library 5.0 which meets the IEC60730 class B standard.

More information

More information about the Safety Library with the board specific Library/Example User’s guide, release note, certificate and other documentation: http://www.nxp.com/iec60730

Board settings

Follow chapter “Hardware setup” in Example User’s guide.

Running the demo

Follow chapter “Running example” in Example User’s guide.