MCUXpresso SDK Release Notes
Overview
The MCUXpresso SDK is a comprehensive software enablement package designed to simplify and accelerate application development with Arm Cortex-M-based devices from NXP, including its general purpose, crossover and Bluetooth-enabled MCUs. MCUXpresso SW and Tools for DSC further extends the SDK support to current 32-bit Digital Signal Controllers. The MCUXpresso SDK includes production-grade software with integrated RTOS (optional), integrated enabling software technologies (stacks and middleware), reference software, and more.
In addition to working seamlessly with the MCUXpresso IDE, the MCUXpresso SDK also supports and provides example projects for various toolchains. The Development tools chapter in the associated Release Notes provides details about toolchain support for your board. Support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.
Underscoring our commitment to high quality, the MCUXpresso SDK is MISRA compliant and checked with Coverity static analysis tools. For details on MCUXpresso SDK, see MCUXpresso-SDK: Software Development Kit for MCUXpresso.
MCUXpresso SDK
As part of the MCUXpresso software and tools, MCUXpresso SDK is the evolution of Kinetis SDK, includes support for LPC, DSC,PN76, and i.MX System-on-Chip (SoC). The same drivers, APIs, and middleware are still available with support for Kinetis, LPC, DSC, and i.MX silicon. The MCUXpresso SDK adds support for the MCUXpresso IDE, an Eclipse-based toolchain that works with all MCUXpresso SDKs. Easily import your SDK into the new toolchain to access to all of the available components, examples, and demos for your target silicon. In addition to the MCUXpresso IDE, support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.
In order to maintain compatibility with legacy Freescale code, the filenames and source code in MCUXpresso SDK containing the legacy Freescale prefix FSL has been left as is. The FSL prefix has been redefined as the NXP Foundation Software Library.
Development tools
The MCUXpresso SDK was tested with following development tools. Same versions or above are recommended.
IAR Embedded Workbench for Arm, version is 9.60.4
MCUXpresso IDE, Rev. 25.06.xx
MCUXpresso for VS Code v25.09
GCC Arm Embedded Toolchain 14.2.x
Supported development systems
This release supports board and devices listed in following table. The board and devices in bold were tested in this release.
Development boards |
MCU devices |
|---|---|
KW47-LOC |
KW47B42ZB7AFTA |
MCUXpresso SDK release package
The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.
Device support
The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.
Board support
The boards folder provides the board-specific demo applications, driver examples, and middleware examples.
Demo application and other examples
The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.
RTOS
FreeRTOS
Real-time operating system for microcontrollers from Amazon
Middleware
GenFSK link layer
The Generic FSK protocol enables radio operation using a custom GFSK/GMSK or MSK modulation format.
Main Features supported:
Highly configurable packet structure
Optimized Sequence Command Set
High-precision timebase to maintain network timing
Two timer-compare mechanisms for Interrupt Generation and Sequence Launching
Hardware automation for packet transmit and receive, CRC and Whitening
Up to four network addresses to synchronize to, can be 8-bit, 16-bit or 32-bit
Packet Lengths up to 2047 Bytes
Support complex auto-sequence, like CCA before TX, Auto-ACK, TR.
Many operating modes can support the sending and receiving of multiple protocol packets, such as Bluetooth LE.
Wireless XCVR
The XCVR component provides a base Transceiver Driver for the 2.4 GHz narrowband radio.
Bluetooth LE Controller
Main features supported:
Peripheral Role
Central Role
Multiple PHYs (1 Mbps, 2 Mbps, Coded PHY)
Asymmetric Connections
Public/Random/Static Addresses
Network/Device Privacy Modes
Extended Advertising
Extended Scanning
Passive/Active Scanning
LE Encryption
LE Ping Procedure
HCI Test Interface
UART Test Interface
Randomized Advertising Channel Indexing
Sleep Clock Accuracy Update - Mechanism
ADI Field in Scan Response Data
HCI Support for Debug Keys in LE - Secure Connections
Main capabilities supported:
Simultaneous scanning 1 Mbps and Long Range
Scanning and advertising in parallel
24 connections as a central role
24 connections as a peripheral role
Any combination of central and peripheral roles (24 connections maximum)
8 connections with a 7.5 ms connection interval
Two advertising sets in parallel (\Four adv set as Early Access Release).
26 Accept List entries
36 Resolvable Private Address (RPA) entries
Up to two Chain Packets per Extended Advertising set
Enhanced Notification on end of - Scanning/Advertising/Connection events
Connection event counters associated to Bluetooth LE packet reception
Timestamp associated to Bluetooth LE packet reception
RF channel info associated to Bluetooth LE packet reception
NXP proprietary Bluetooth LE Handover feature
Decision Based Advertising Filtering (DBAF)
Advertising Coding Selection (ACS)
Periodic Advertising with Responses (PAwR) Additional features supported for KW47 and MCX W72 devices:
Channel Sounding
Note: Project configuration enabling Experimental features on KW45 and MCX W71 requires the Radio Subsystem (NBU) Firmware to be reprogrammed with the firmware provided in the SDK under \middleware\wireless\ble_controller\bin\experimental\. For NBU programming steps, see the EVK Quick Start Guide and Secure Provisioning SDK (SPSDK) documentation.
Project configurations that require usage of the Bluetooth LE controller including all Bluetooth LE examples require the Radio Subsystem (NBU) Firmware to be re-programmed with the firmware provided in the SDK under middleware\wireless\ble_controller\bin.
Wireless Bluetooth LE host stack and applications
The Bluetooth LE Host Stack component provides an implementation for a Bluetooth LE mandatory and some optional, proprietary, and experimental features. The Bluetooth LE Host Stack component provides application examples, services, and profiles.
Main features supported:
Automotive Compliance
MISRA Compliance
HIS CCM <= 20
Advanced Secure Mode
Enhanced ATT
GATT Caching
Bluetooth LE Host GCC Libraries
Bluetooth LE Host IAR Libraries
Bluetooth LE Host Peripheral Libraries
Bluetooth LE Central Libraries
Bluetooth LE Host Full Host Features Libraries
Bluetooth LE Host Optional Features Libraries
Bluetooth LE Host Mandatory Features Libraries
Bare-metal and FreeRTOS Support
Bluetooth LE Privacy Support
CCC Sample Applications
Enhanced Notifications
Dynamic Database
OTA Support - Sample Applications
Decision based Advertising Filtering (DBAF) - Experimental feature
Advertising Coding Selection (ACS) - Experimental feature
Channel Sounding - Experimental feature with controlled access (contact your NXP representative for access)
Bluetooth LE Controller main and experimental features and capabilities described below are supported by the Bluetooth LE Host.
Note: For evaluating DBAF and ACS experimental features, replace the Bluetooth LE Host default example projects libraries with the libraries from the SDK folder ..\middleware\wireless\bluetooth\host\lib_exp and enable the features in the application. The Radio Subsystem (NBU) Firmware with experimental features is required.
Wireless Localization
Localization
Wireless Connectivity Framework
The Connectivity Framework is a software component that provides hardware abstraction modules to the upper layer connectivity stacks and components. It also provides a list of services and APIs, such as, Low power, Over the Air (OTA) Firmware update, File System, Security, Sensors, Serial Connectivity Interface (FSCI), and others. The Connectivity Framework modules are located in the middleware\wireless\framework SDK folder.
CMSIS DSP Library
The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.
NXP PSA CRYPTO DRIVER
PSA crypto driver for crypto library integration via driver wrappers
EdgeLock SE050 Plug and Trust Middleware
Secure subsystem library - SSS APIs
Multicore
Multicore Software Development Kit
mbedTLS
mbedtls SSL/TLS library v3.x
mbedTLS
mbedtls SSL/TLS library v2.x
LittleFS
LittleFS filesystem stack
LIN Stack
LIN Stack middleware
FreeMASTER
FreeMASTER communication driver for 32-bit platforms.
Release contents
Provides an overview of the MCUXpresso SDK release package contents and locations.
Deliverable |
Location |
|---|---|
Boards |
INSTALL_DIR/boards |
Demo Applications |
INSTALL_DIR/boards/<board_name>/demo_apps |
Driver Examples |
INSTALL_DIR/boards/<board_name>/driver_examples |
eIQ examples |
INSTALL_DIR/boards/<board_name>/eiq_examples |
Board Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/boards/<board_name>/project_template |
Driver, SoC header files, extension header files and feature header files, utilities |
INSTALL_DIR/devices/<device_name> |
CMSIS drivers |
INSTALL_DIR/devices/<device_name>/cmsis_drivers |
Peripheral drivers |
INSTALL_DIR/devices/<device_name>/drivers |
Toolchain linker files and startup code |
INSTALL_DIR/devices/<device_name>/<toolchain_name> |
Utilities such as debug console |
INSTALL_DIR/devices/<device_name>/utilities |
Device Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/devices/<device_name>/project_template |
CMSIS Arm Cortex-M header files, DSP library source |
INSTALL_DIR/CMSIS |
Components and board device drivers |
INSTALL_DIR/components |
RTOS |
INSTALL_DIR/rtos |
Release Notes, Getting Started Document and other documents |
INSTALL_DIR/docs |
Tools such as shared cmake files |
INSTALL_DIR/tools |
Middleware |
INSTALL_DIR/middleware |
What is new
The following changes have been implemented compared to the previous SDK release version (25.09.00-pvw2).
Bluetooth LE Host Stack and Applications
Added
CCC sample applications updated to CCC Digital Key v4.0.0 Specification.
RAS/RAP PTS 8.7.4 test support added in Localization Sample applications.
Support for CS start procedure while the previous procedure is not completed; old procedure replaced with the new one.
Improved
Localization Sample Applications Ram partition.
RAS/RAP profile and service.
Various sample applications have been updated.
Fixed
Always set the Advertising Legacy Set handle if the legacy API was used.
PAWR parameters in PeriodicSyncTransferReceived are now parsed correctly.
Ensure an RPA/NRPA is properly set from the application to enable a central using Controller Privacy to connect to unbonded peripherals.
CS algorithm buffer overwrite issue during Connection Handover application.
Various sample applications bug fixes applied.
Pass correct Codded PHY (S2) to Channel Sounding Set Procedure Parameters.
Changed
Merged Gap_SetExtAdvertisingParameters and Gap_SetExtAdvertisingParametersV2 into Gap_SetExtAdvertisingParameters.
ce_status_buffer type changed to int32_t.
Details can be found in github repository nxp-mcuxpresso/mcuxsdk-middleware-bluetooth-host/CHANGELOG.md.
Bluetooth LE controller
Channel sounding updates:
Handle Procedure collision between LLCP CS Procedure and non-CS Procedure and between two LLCP CS procedures.
Start Feature Exchange autonomously if needed prior initiating the CS Capability Exchange Procedure.
Fix CS Procedure aborted with CS_SYNC=2Mbps and T_PM=40.
Fix phase accuracy bias when CFO is high [-50ppm, +50ppm].
Fix RTT bias due to chip sample RC Calibration imprecision. Chip IFR now contains appropriate calibration value used by software to compensate associated delay.
Fix wrong PRBS payload coding in HADM test mode.
Fix testmode generating more than one subevent with subevt_int=0 and more than 160 steps.
Fix CS handover regression due to MISRA fix.
Use precompiled libraries for CS support.
PAwR/PAST updates:
Window widening for PAwR responses supports the worst clock accuracy (500ppm) to avoid interoperability issues.
Autonomous Feature Exchange is done prior PAST Procedure.
Fix Connection Update state machine on peripheral side after Connection Update rejection.
Fix to handle correctly concurrent Connection Update procedures initiated by peer and local devices on different connections.
Support 4 Advertising set with optimized Advertising placement when Advertising intervals are multiple of each other.
Transceiver drivers (XCVR)
Added support for Bluetooth LE Channel Sounding.
Added API to control PA ramp type and duration.
Connectivity framework
Major Changes
[wireless_mcu][wireless_nbu] Introduced PLATFORM_Get32KTimeStamp() API, available on platforms that support it.
[RNG] Switched to using a workqueue for scheduling seed generation tasks.
[Sensors] Integrated workqueue to trigger temperature readings on periodic timer expirations.
[wireless_nbu] Removed outdated configuration files from wireless_nbu/configs.
[SecLib_RNG][PSA] Added a PSA-compliant implementation for SecLib_RNG. ⚠️ This is an experimental feature and should be used with caution.
[wireless_mcu][wireless_nbu] Implemented PLATFORM_SendNBUXtal32MTrim() API to transmit XTAL32M trimming values to the NBU.
Minor Changes (no impact on application)
[MWS] Migrated the Mobile Wireless Standard (MWS) service to the public repository. This service manages coexistence between connectivity protocols such as BLE, 802.15.4, and GenFSK.
[HWParameter][NVM][SecLib_RNG][Sensors] Addressed various MISRA compliance issues across multiple modules.
[Sensors] Applied a filtering mechanism to temperature data measured by the application core before forwarding it to the NBU, improving data reliability.
[Common] Relocated the GetPowerOfTwoShift() function to a shared module for broader accessibility across components.
[RNG] Resolved inconsistencies in RNG behavior when using the fsl_adapter_rng HAL by aligning it with other API implementations.
[SecLib] Updated the AES CMAC block counter in AES_128_CMAC() and AES_128_CMAC_LsbFirstInput() to support data segments larger than 4KB.
[SecLib] Utilized sss_sscp_key_object_free() with kSSS_keyObjFree_KeysStoreDefragment to avoid key allocation failures.
[WorkQ] Increased workqueue stack size to accommodate RNG usage with mbedtls.
[wireless_mcu][ot] Suppressed chip revision transmission when operating with nbu_15_4.
[platform][mflash] Ensured proper address alignment for external flash reads in PLATFORM_ReadExternalFlash() when required by platform constraints.
[RNG] Corrected reseed flag behavior in RNG_GetPseudoRandomData() after reaching gRngMaxRequests_d threshold.
[platform][mflash] Fixed uninitialized variable issue in PLATFORM_ReadExternalFlash().
[platform][wireless_nbu] Fixed an issue on KW47 where PLATFORM_InitFro192M incorrectly reads IFR1 from a hardcoded flash address (0x48000), leading to unstable FRO192M trimming. The function is now conditionally compiled for KW45 only.
Details can be found in CHANGELOG.md
Known issues
This section lists the known issues, limitations, and/or workarounds.
Maximum file path length in Windows 7 operating system
The Windows 7 operating system imposes a 260-character maximum length for file paths. When installing the MCUXpresso SDK, place it in a directory close to the root to prevent file paths from exceeding the maximum character length specified by the Windows operating system. The recommended location is the C:\nxp folder.
Only FreeRTOS is tested for RTOS support
This release only supports the FreeRTOS kernel and a bare-metal non-preemptive task scheduler.
Bluetooth LE
Most sensor applications have pairing and bonding disabled to allow a faster interaction with mobile applications. These two security features can be enabled in the app_preinclude.h header file.
Bluetooth LE controller:
The maximum Advertising data length is limited to 800 bytes.
Missing chained packet TX when coded phy is used on multiple Advertising sets and Advertising interval is small.
Issue with packet time restrictions after phy update (packet payload too long).
Missing chained packets during scanning.
Need to add a dummy nbu request to wake-up NBU core during asynchronous wakeup to avoid low power race condition issue (ie: for NBU ramlog dump from shared memory).
Need to stop/restart scan before RPA timeout when controller privacy is enabled, else address resolution may not work properly.
Periodic Advertising with Responses (PAwR):
Periodic Advertising with Response (PAwR) is not supported with the configuration “Subevent Interval = Number of Response Slots * Response Slot Spacing”.
Unoptimized Periodic Advertising placement with Connection events.
PAwR Advertiser is not able to report multiple periodic Advertising responses in a same subevent.
KW45/MCXW71: No specific issues.
KW47/MCXW72: Channel Sounding (CS): Limitations:
RTT with Sounding Sequence is not supported.
TX SNR is not supported.
LE 2M 2BT PHY is not supported.
Maximum 6 Channel Sounding procedures are supported in parallel.
Scheduling of activities may be non optimal when multiple Channel Sounding procedures are running in parallel.
Phase measurement bias is within certification range (<1.7x2πns) with KW47 EVK board. However, if different PCB or antenna matching is used, some bias may appear due to increased delay.
Channel Sounding is not supported with internal FRO32. Known issues:
When CS_SYNC=2Mbps, sensitivity drops at –85dBm (vs –95dBm for 1Mbps).
NADM may report false positive attacks when using localization board at 2Mbps.
When CS Subevents are configured very close from each other (<700us), some Subevents may be aborted with reason 0x3.
When CS offset is configured too close from ACL anchor point, the anchor point may not be served (TX on central or RX on peripheral will not happen). Ideally, CS Offset should be configured greater than 1ms.
Wireless_ranging stability issue in test mode 2Mbps with RTT random sequence payload 128 bits.
RF-PHY receiver testcases failing: RF-PHY/RCV-LE/CA/BV-7-C, RF-PHY/RCV-LE/CA/BV-13-C, RF-PHY/RCV-LE/CA/BV-30-C, RF-PHY/RCV-LE/CA/BV-31-C.
RTT bias compensation:
For parts not properly configured at production (IFR blank), RTT bias may not be compensated properly. Consequently, an inaccuracy of +/-2m may be observed.
Temperature variation: RTT variation of +/-2m is observed based on temperature.
Other limitations
The following Connectivity Framework configurations are Experimental and not recommended for mass production:
Power down on application power domain.
A hardfault can be encountered when using fsl_component_mem_manager_light.c memory allocator and shutting down some unused RAM banks in low power. It is due to a wrong reinitialization of ECC RAM banks. To be sure not to reproduce the issue,
gPlatformShutdownEccRamInLowPowershould be set to 0.GenFSK
Connectivity_testapplication is not operational with Low Power enabled.Serial manager is only supported on UART (not I2C nor SPI).
The
--no-warn-rwx-segmentscannot been recognized on legacy MCUXpresso IDE versions.The
--no-warn-rwx-segmentsoption in MCUXpresso projects should be manually removed from the project settings if someone needs to use legacy (< 11.8.0) MCUXpresso IDE versionsIf the FRO32K is configured as the clock source of the CM33 Core then the debug session will block in both IAR, MCUX CMSIS-DAP while debugging. Use a lower debug wire speed, for example 1 MHz instead of the default one.
In IAR, the option is in Runtime Checking -> Debugger -> CMSIS DAP -> Interface -> Interface speed.
In MCUXpresso IDE, the option is in LinkServer Debugger -> Advanced Settings -> Wirespeed (Hz).
Low power reference design applications are not supported for the armgcc toolchain from zip archives. Please use MCUXpresso IDE or IAR toolchains for development using these applications.
Latest MCUX IDE 24.9.25 cannot support KW47 multicore compiling
The latest MCUX IDE 24.9.25 cannot support KW47 multicore compiling, users need to upgrade to the Linkserver_24.10.22 or higher version, and change the LinkServer path configuration in the MCUX IDE. Two ways to change the LinkerSever path in the MCUX IDE.
Option 1 (recommended): Using the custom Path

Option 2: Using the command-line to change the settings
Close the MCUXpresso IDE if it is open.
Execute the following command:
<path_to_MCUXpressoIDE_installation_folder>\ide\mcuxpressoide -application com.nxp.mcuxpresso.headless.application -nosplash -run set.config.preference com.nxp.mcuxpresso.core.debug.support.linkserver:linkserver.path.default_path=<path_to_LinkServer_installation_folder>
where:
<path_to_MCUXpressoIDE_installation_folder>is the folder where the MCUXpresso IDE is installed.<path_to_LinkServer_installation_folder>is the folder where the new/custom LinkServer is installed.
Example:
C:\NXP\MCUXpressoIDE_24.9.25\ide\mcuxpressoide -application com.nxp.mcuxpresso.headless.application -nosplash -run set.config.preference com.nxp.mcuxpresso.core.debug.support.linkserver:linkserver.path.default_path=c:\NXP\LinkServer_24.10.15