Hardware requirements
Micro USB cable
MCX-N5XX-EVK board
Personal Computer
Board settings
Default layout setup - bootloader located in IFR region
Region |
From |
To |
Size |
|---|---|---|---|
Primary slot |
0x00000000 |
0x000FFFFF |
1024kB |
Secondary slot |
0x00100000 |
0x001FFFFF |
1024kB |
—————- |
———— |
———— |
——– |
MCUboot code |
0x01008000 |
0x0100FFFF |
32kB |
MCUBoot resides in the
Bank_1 IFR_0region to utilize flash remap featureMCUBoot header size is set to 1024 bytes
Signing algorithm is ECDSA-P256 (TinyCrypt)
Write alignment is 16 bytes
MCUBoot is configured to use its
DIRECT_XIPimage handling strategyFlash swapping HW feature is used for zero-overhead image swapping
Image signing example:
imgtool sign --key sign-ecdsa-p256-priv.pem
--align 16
--version 1.1
--slot-size 0x100000
--header-size 0x400
--pad-header
ota_mcuboot_basic.bin
ota_mcuboot_basic.SIGNED.bin
Note that for the first image flashed manually together with the bootloader
additional imgtool options --pad and --confirm must be used. Otherwise
the bootloader would reject the image for missing data in the trailer area.
If the toolchain used for build has problems with writing the bootloader to the IFR flash region, an alternative can be to use NXP blhost utility or MCUXpresso Secure Provisioning Tool.
IMPORTANT:
The CMPA region must be configured so that ROM loader boots from the IFR
region. This is done by setting the BOOT_CFG.BOOT_SRC field to 0b10. This
value directs the ROM loader to start execution from the IFR region where
MCUboot is located. Default CMPA setup with this particular field set is
attached to this example in cmpa.bin binary file.
To flash this configuration together with MCUboot binary the following blhost
commands can be used. Note that the board must be in the ISP mode to use
the following commands:
#Erase IFR0 Bank 1 region
blhost -u 0x1FC9,0x014F -- flash-erase-region 0x01008000 32768 0
#Flash MCUboot
blhost -u 0x1FC9,0x014F -- write-memory 0x01008000 mcuboot_opensource.bin
#Flash CMPA
blhost -u 0x1FC9,0x014F -- write-memory 0x01004000 cmpa.bin
Custom layout setup - bootloader located in main flash
Default layout setup using the IFR region limits usage of some features such as hardware accelerated mbedTLS (due size of IFR region) or encrypted XIP using NPX module. This custom configuration moves the bootloader to main flash array.
Region |
From |
To |
Size |
|---|---|---|---|
MCUboot code |
0x00000000 |
0x0003FFFF |
256kB |
Primary slot |
0x00040000 |
0x0011FFFF |
896kB |
Secondary slot |
0x00120000 |
0x001FFFFF |
896kB |
MCUBoot header size is set to 1024 bytes
Signing algorithm is ECDSA-P256 (mbedTLS)
Write alignment is 16 bytes
MCUBoot is configured to use its
SWAP_USING_MOVEimage update strategy
Image signing example:
imgtool sign --key sign-ecdsa-p256-priv.pem
--align 16
--version 1.1
--slot-size 0xE0000
--header-size 0x400
--max-sectors 111
--pad-header
ota_mcuboot_basic.bin
ota_mcuboot_basic.SIGNED.bin
The custom build can be generated using west build and supports only IAR and GCC toolchain.
Example:
Bootloader:
west build -p always examples/ota_examples/mcuboot_opensource -b mcxn5xxevk --config debug --toolchain armgcc -Dcore_id=cm33_core0 -DCONF_FILE="examples/ota_examples/_custom_cfg/mcxn_mcuboot_in_main_flash/mcuboot_opensource.conf"
OTA application:
west build -p always examples/ota_examples/ota_mcuboot_basic -b mcxn5xxevk --config debug --toolchain armgcc -Dcore_id=cm33_core0 -DCONF_FILE="examples/ota_examples/_custom_cfg/mcxn_mcuboot_in_main_flash/ota_mcuboot_basic.conf"