Logo
25.09.00-pvw1
MCUXpresso SDK Project v: latest
Document Release Versions
25.09.00-pvw1
25.06.00
25.06.00-pvw2
25.06.00-pvw1
25.03.00
latest

Introduction

  • MCUXPresso SDK

Getting Started

  • Github Repository
  • Zip Package

User Guide

  • Drivers
  • Examples
  • Middleware
    • Boot
    • Cloud
    • Connectivity
    • eIQ
    • File System
    • Motor Control
    • MultiCore
    • Multimedia
    • Wireless
      • NXP Wireless Framework and Stacks
        • Wi-Fi, Bluetooth, 802.15.4
        • Wireless Zigbee
          • ZigBee Demo Applications User's Guide (UG10194)
          • ZigBee 3.0 Stack User Guide (JN-UG-3130)
          • ZigBee 3.0 Devices User Guide (JN-UG-3131)
          • ZigBee 3.0 Cluster Library (JN-UG-3132)
          • ZigBee NCP Host Coordinator Example
          • ZigBee NCP Host Router Example
          • Zigbee Coordinator and Bluetooth LE Example
          • Zigbee Router and Bluetooth LE Example
        • NXP Bluetooth LE Host and Sample Applications
        • Wireless Framework
        • Wireless IEEE
      • Wi-Fi
      • EdgeFast Bluetooth
    • Sensors
  • RTOS
  • Boards

Development

  • Build And Configuration System
  • Developing with MCUXpresso SDK

Releases

  • Release Notes
mcuxsdk
  • Docs »
  • Middleware »
  • Wireless »
  • NXP Wireless Framework and Stacks »
  • Wireless Zigbee »
  • MCXW71/MCXW72/RW612 ZigBee Demo Applications User Guide
  • Open on Repo Report an issue

MCXW71/MCXW72/RW612 ZigBee Demo Applications User Guide

Table of Contents

  • Overview
    • Related documentation
  • Introduction
  • Development environment
    • Software
    • Hardware
  • Examples
    • FRDM-MCXW7x board
    • FRDM-MCXW71 / FRDM-MCXW72 board
    • RD-RW612-BGA board
    • FRDM-RW612 board
    • MCX-W71-EVK / MCX-W72-EVK board
  • Running the demonstration examples
    • Loading the applications
    • Loading the application for RW612 platform
    • Coordinator functionality
      • Forming a network
      • Allowing other nodes to join (Network Steering)
      • Operating the device (Coordinator)
      • Rejoining a network (Coordinator)
      • Performing a factory reset (Coordinator)
      • Summary of serial interface commands
    • Router functionality
      • Forming or joining a network (router)
      • Joining an existing network using network steering (Router)
      • Allowing other devices to join the network (Router)
      • Operating the device (router)
      • Rejoining a network (router)
      • Performing a factory reset (router)
    • End Device functionality
      • Joining an existing network using network steering (ED)
      • Operating the device (ED)
      • Rejoining a network (ED)
      • Performing a factory reset (ED)
    • Binding devices
  • ZigBee over-the-air upgrade
    • OTA for RW612 platform
    • Overview
    • OTA upgrade operation
    • Image credentials
    • Upgrade and downgrade
  • LED indication table
    • Coordinator
    • Router
    • End Device RX On
    • End Device RX Off (sleepy device)
  • Note about the source code in the document
  • Revision history

Copyright 2025, NXP. Last generated on Jul 17, 2025 16:25+0200; branch release/25.09.00-pvw1, revision b64f8fe5049b66fd3bf22464fb88e71ddf73d6ec.